<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックRe: Kenitis KL05 DMA channel source</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kenitis-KL05-DMA-channel-source/m-p/1783900#M65886</link>
    <description>&lt;P&gt;Having used DMA in a small number of experimental configurations, and found the documentation "lacking".&lt;/P&gt;&lt;P&gt;I think naming this field as "SOURCE" is confusing.&lt;/P&gt;&lt;P&gt;DMA transfers are triggered by some event, which can include a ALWAYS trigger.&lt;/P&gt;&lt;P&gt;The SOURCE is the source of the TRIGGER.&lt;/P&gt;&lt;P&gt;For some reason the PIT timer gets a special feature in that the TRIG selects the PIT timer overflow as the trigger, but with limitations that you can only use DMA0 with PIT0, DMA1 with PIT1, etc.&lt;/P&gt;&lt;P&gt;While some of the trigger "sources" are obvious, there are a few which I couldn't figure out from the reference manual.&lt;/P&gt;</description>
    <pubDate>Sat, 06 Jan 2024 16:52:38 GMT</pubDate>
    <dc:creator>migry</dc:creator>
    <dc:date>2024-01-06T16:52:38Z</dc:date>
    <item>
      <title>Kenitis KL05 DMA channel source</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kenitis-KL05-DMA-channel-source/m-p/1780663#M65842</link>
      <description>&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="1.png" style="width: 999px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/256087i5A4801ED27BB8D4A/image-size/large?v=v2&amp;amp;px=999" role="button" title="1.png" alt="1.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;1.png&lt;/span&gt;&lt;/span&gt;Hi,i am recently use Kenitis family MCU KL05Z32 , but i conldn't find the dma channel source's details ,neither datasheet nor RM document,where could i find the dma request source of KL05? Could somebody help me?&lt;/P&gt;</description>
      <pubDate>Thu, 28 Dec 2023 02:03:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kenitis-KL05-DMA-channel-source/m-p/1780663#M65842</guid>
      <dc:creator>cfk</dc:creator>
      <dc:date>2023-12-28T02:03:25Z</dc:date>
    </item>
    <item>
      <title>Re: Kenitis KL05 DMA channel source</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kenitis-KL05-DMA-channel-source/m-p/1781951#M65861</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;Pls refer to section 3.4.8.1 DMA MUX Request Sources in reference manual of KL05.&lt;/P&gt;
&lt;P&gt;Hope it can help you&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;XiangJun Rong&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="xiangjun_rong_0-1704253019366.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/256432i0A92E627D5ADE885/image-size/medium?v=v2&amp;amp;px=400" role="button" title="xiangjun_rong_0-1704253019366.png" alt="xiangjun_rong_0-1704253019366.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;xiangjun_rong_0-1704253019366.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 03 Jan 2024 03:37:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kenitis-KL05-DMA-channel-source/m-p/1781951#M65861</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2024-01-03T03:37:54Z</dc:date>
    </item>
    <item>
      <title>Re: Kenitis KL05 DMA channel source</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kenitis-KL05-DMA-channel-source/m-p/1783900#M65886</link>
      <description>&lt;P&gt;Having used DMA in a small number of experimental configurations, and found the documentation "lacking".&lt;/P&gt;&lt;P&gt;I think naming this field as "SOURCE" is confusing.&lt;/P&gt;&lt;P&gt;DMA transfers are triggered by some event, which can include a ALWAYS trigger.&lt;/P&gt;&lt;P&gt;The SOURCE is the source of the TRIGGER.&lt;/P&gt;&lt;P&gt;For some reason the PIT timer gets a special feature in that the TRIG selects the PIT timer overflow as the trigger, but with limitations that you can only use DMA0 with PIT0, DMA1 with PIT1, etc.&lt;/P&gt;&lt;P&gt;While some of the trigger "sources" are obvious, there are a few which I couldn't figure out from the reference manual.&lt;/P&gt;</description>
      <pubDate>Sat, 06 Jan 2024 16:52:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kenitis-KL05-DMA-channel-source/m-p/1783900#M65886</guid>
      <dc:creator>migry</dc:creator>
      <dc:date>2024-01-06T16:52:38Z</dc:date>
    </item>
    <item>
      <title>Re: Kenitis KL05 DMA channel source</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kenitis-KL05-DMA-channel-source/m-p/1784295#M65900</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;As the section 3.4.8.1 DMA MUX request sources, the source number in Table&amp;nbsp; 20 define the DMA request source.&lt;/P&gt;
&lt;P&gt;The DMA triggering source can only be PITx channel, this is a special case, it can manipulate GPIO with PIT cycle.&lt;/P&gt;
&lt;P&gt;Hope it can help you&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;XiangJun Rong&lt;/P&gt;</description>
      <pubDate>Mon, 08 Jan 2024 09:20:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kenitis-KL05-DMA-channel-source/m-p/1784295#M65900</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2024-01-08T09:20:02Z</dc:date>
    </item>
  </channel>
</rss>