<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックMK12DX256VLK5 POR problem</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/MK12DX256VLK5-POR-problem/m-p/1783815#M65881</link>
    <description>&lt;P&gt;I'm using the above micro and it doesn't seem to come out of reset on a power up. I can load and debug code using JTAG (JTAG reset works). But when I power cycle the board the micro seems stuck in reset.&amp;nbsp;The board has a reset button connected to RESET_b and this will reset the micro and everything is fine. What would cause the micro to not come out of POR on power up?&lt;/P&gt;&lt;P&gt;I've been using other Kinetis micros for many (many) years and never had this problem. I'm stumped!&lt;/P&gt;&lt;P&gt;Vcc = 2.9V so should be high enough.&lt;/P&gt;</description>
    <pubDate>Fri, 05 Jan 2024 21:31:17 GMT</pubDate>
    <dc:creator>larrydemuth</dc:creator>
    <dc:date>2024-01-05T21:31:17Z</dc:date>
    <item>
      <title>MK12DX256VLK5 POR problem</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/MK12DX256VLK5-POR-problem/m-p/1783815#M65881</link>
      <description>&lt;P&gt;I'm using the above micro and it doesn't seem to come out of reset on a power up. I can load and debug code using JTAG (JTAG reset works). But when I power cycle the board the micro seems stuck in reset.&amp;nbsp;The board has a reset button connected to RESET_b and this will reset the micro and everything is fine. What would cause the micro to not come out of POR on power up?&lt;/P&gt;&lt;P&gt;I've been using other Kinetis micros for many (many) years and never had this problem. I'm stumped!&lt;/P&gt;&lt;P&gt;Vcc = 2.9V so should be high enough.&lt;/P&gt;</description>
      <pubDate>Fri, 05 Jan 2024 21:31:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/MK12DX256VLK5-POR-problem/m-p/1783815#M65881</guid>
      <dc:creator>larrydemuth</dc:creator>
      <dc:date>2024-01-05T21:31:17Z</dc:date>
    </item>
    <item>
      <title>Re: MK12DX256VLK5 POR problem</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/MK12DX256VLK5-POR-problem/m-p/1783983#M65894</link>
      <description>&lt;P&gt;Never mind, I found the problem. PTA4 (NMI) was being used as an input from another IC, and the pin was low on power up, causing an NMI interrupt. I set last word in the CFM PROT to&amp;nbsp;0xfffff9fe to disable NMI and EZPORT, it was&amp;nbsp;0xfffffffe.&lt;/P&gt;&lt;P&gt;The board now boots on power up.&lt;/P&gt;</description>
      <pubDate>Mon, 08 Jan 2024 00:56:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/MK12DX256VLK5-POR-problem/m-p/1783983#M65894</guid>
      <dc:creator>larrydemuth</dc:creator>
      <dc:date>2024-01-08T00:56:54Z</dc:date>
    </item>
  </channel>
</rss>