<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックRe: LWIP TCP receiving</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/LWIP-TCP-receiving/m-p/1783252#M65876</link>
    <description>&lt;P&gt;Hello&lt;/P&gt;
&lt;P&gt;I hope you are well.&lt;/P&gt;
&lt;P&gt;Increasing the buffer size might be helpful.&lt;BR /&gt;What causes the TCP window to 0?&amp;nbsp; Usually, it comes down to performance, simple as that.&amp;nbsp;The TCP receive buffer is full and it cannot receive any more data.&lt;/P&gt;
&lt;P&gt;Best regards,&lt;BR /&gt;Omar&lt;/P&gt;</description>
    <pubDate>Fri, 05 Jan 2024 00:25:37 GMT</pubDate>
    <dc:creator>Omar_Anguiano</dc:creator>
    <dc:date>2024-01-05T00:25:37Z</dc:date>
    <item>
      <title>LWIP TCP receiving</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/LWIP-TCP-receiving/m-p/1773404#M65778</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I am using FRDM-K66 with LWIP stack. I have the following problems:&lt;/P&gt;&lt;P&gt;When I use sample TCP sever, everything works fine except the following:&lt;/P&gt;&lt;P&gt;If PC send TCP packet evrery 100ms, my server get zero window size in TCP. Can anyone tells me how to avoid this. Like RESET window size when detect it or speed up TCP coming process, or increasing buffer, nd etc...&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Christie&lt;/P&gt;</description>
      <pubDate>Tue, 12 Dec 2023 22:06:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/LWIP-TCP-receiving/m-p/1773404#M65778</guid>
      <dc:creator>a8Chcx</dc:creator>
      <dc:date>2023-12-12T22:06:35Z</dc:date>
    </item>
    <item>
      <title>Re: LWIP TCP receiving</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/LWIP-TCP-receiving/m-p/1783252#M65876</link>
      <description>&lt;P&gt;Hello&lt;/P&gt;
&lt;P&gt;I hope you are well.&lt;/P&gt;
&lt;P&gt;Increasing the buffer size might be helpful.&lt;BR /&gt;What causes the TCP window to 0?&amp;nbsp; Usually, it comes down to performance, simple as that.&amp;nbsp;The TCP receive buffer is full and it cannot receive any more data.&lt;/P&gt;
&lt;P&gt;Best regards,&lt;BR /&gt;Omar&lt;/P&gt;</description>
      <pubDate>Fri, 05 Jan 2024 00:25:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/LWIP-TCP-receiving/m-p/1783252#M65876</guid>
      <dc:creator>Omar_Anguiano</dc:creator>
      <dc:date>2024-01-05T00:25:37Z</dc:date>
    </item>
  </channel>
</rss>