<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: KEA128 FTM2 in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KEA128-FTM2/m-p/1778442#M65823</link>
    <description>&lt;P&gt;如图可以看到FTM2的中断已经定义在中断向量表中，实际使用当我改变UART的波特率是会影响的，若是波特率大约等于9600，此时使用FTM2输出PWM，系统会不间断复位，若波特率不是9600，那么系统运行正常，FTM2也正常&lt;/P&gt;</description>
    <pubDate>Thu, 21 Dec 2023 07:05:20 GMT</pubDate>
    <dc:creator>primaryleaf</dc:creator>
    <dc:date>2023-12-21T07:05:20Z</dc:date>
    <item>
      <title>KEA128 FTM2</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KEA128-FTM2/m-p/1776763#M65811</link>
      <description>&lt;P&gt;时钟选用内部时钟，当PTC3属性配置成FTM2通道3时，频率100hz，占空比50%，UART的初始化会导致系统不间断复位，屏蔽UART初始化则正常。&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="FTM2初始化" style="width: 969px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/254944i0BB5F60B37B67EF4/image-size/large?v=v2&amp;amp;px=999" role="button" title="FTM2初始化.jpeg" alt="FTM2初始化" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;FTM2初始化&lt;/span&gt;&lt;/span&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="UART初始化" style="width: 977px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/254945i4155AD068D14B9D8/image-size/large?v=v2&amp;amp;px=999" role="button" title="UART初始化.jpeg" alt="UART初始化" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;UART初始化&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 19 Dec 2023 03:37:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KEA128-FTM2/m-p/1776763#M65811</guid>
      <dc:creator>primaryleaf</dc:creator>
      <dc:date>2023-12-19T03:37:39Z</dc:date>
    </item>
    <item>
      <title>Re: KEA128 FTM2</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KEA128-FTM2/m-p/1777566#M65819</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;我认为FTM2和Uart1没有任何关系， 关于你的问题，你已经允许FTM2和Uart1的中断，请检查是否有相应的中断服务程序。&lt;/P&gt;
&lt;P&gt;你必须将中断服务程序添加到vectors.c 中。&lt;/P&gt;
&lt;P&gt;谢谢&lt;/P&gt;
&lt;P&gt;XiangJuneRong&lt;/P&gt;</description>
      <pubDate>Wed, 20 Dec 2023 03:38:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KEA128-FTM2/m-p/1777566#M65819</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2023-12-20T03:38:05Z</dc:date>
    </item>
    <item>
      <title>Re: KEA128 FTM2</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KEA128-FTM2/m-p/1778442#M65823</link>
      <description>&lt;P&gt;如图可以看到FTM2的中断已经定义在中断向量表中，实际使用当我改变UART的波特率是会影响的，若是波特率大约等于9600，此时使用FTM2输出PWM，系统会不间断复位，若波特率不是9600，那么系统运行正常，FTM2也正常&lt;/P&gt;</description>
      <pubDate>Thu, 21 Dec 2023 07:05:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KEA128-FTM2/m-p/1778442#M65823</guid>
      <dc:creator>primaryleaf</dc:creator>
      <dc:date>2023-12-21T07:05:20Z</dc:date>
    </item>
    <item>
      <title>Re: KEA128 FTM2</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KEA128-FTM2/m-p/1778570#M65824</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;The uart of Kea128 supports Irda, it is possible that it take effects on the uart?&lt;/P&gt;
&lt;P&gt;Pls refer to section 3.2.5 UART0/1/2_RX capture in UM of KEA128.&lt;/P&gt;
&lt;P&gt;Hope it can provide a clue for you&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;XiangJun Rong&lt;/P&gt;</description>
      <pubDate>Thu, 21 Dec 2023 08:52:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KEA128-FTM2/m-p/1778570#M65824</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2023-12-21T08:52:50Z</dc:date>
    </item>
  </channel>
</rss>