<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic GPIO Interrupt not triggering for FRDM-KL25z in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/GPIO-Interrupt-not-triggering-for-FRDM-KL25z/m-p/1758617#M65709</link>
    <description>&lt;P&gt;&lt;STRONG&gt;IMPORTANT: Updates at bottom of post&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;I'm trying to set up interrupts for pins 0,5, and 2 of Port D of my FRDM-KL25z. I want the interrupts to trigger on a falling edge. For testing purposes, I have written the ISR to turn on the Red LED, using code that wrote for a previous project (LED.c). Below is my main code file.&lt;/P&gt;&lt;P&gt;I've tried to execute the following steps to set up interrupts:&lt;/P&gt;&lt;OL&gt;&lt;LI&gt;Use the NVIC_EnableIRQ function to enable interrupts from Port D&lt;/LI&gt;&lt;LI&gt;Configure pins 0,2,5 as GPIO inputs and to request interrupts on the falling edge&lt;/LI&gt;&lt;LI&gt;Write the PORTD_IRQHandler function to do something (in this case, turn on the red LED).&lt;/LI&gt;&lt;/OL&gt;&lt;P&gt;Unfortunately, the red LED is not turning on when I transition any of the pins from logical 1 to 0. I've confirmed that the pins are functioning as inputs through some code that I haven't included in this post, so I must conclude that I have done something incorrectly or that I have missed a step.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Main code file:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;LI-SPOILER&gt;&lt;LI-CODE lang="c"&gt;#include &amp;lt;stdio.h&amp;gt;
#include "board.h"
#include "peripherals.h"
#include "pin_mux.h"
#include "clock_config.h"
#include "MKL25Z4.h"
#include "fsl_debug_console.h"
/* TODO: insert other include files here. */
#include "LED.h"
/* TODO: insert other definitions and declarations here. */

/*
 * @brief   Application entry point.
 */

const uint32_t INPUT_CONFIG =   PORT_PCR_IRQC(1010) | // IRQ Falling Edge
                                PORT_PCR_MUX(001)   | // Pin set to GPIO
                                PORT_PCR_DSE(0)     | // Low drive strength
                                PORT_PCR_PFE(0)     | // TODO: Passive filter disabled, try enabling if noisy
                                PORT_PCR_SRE(0)     | // TODO: Fast slew rate, look up what slow would mean
                                PORT_PCR_PE(0)      | // Pull resistor is disabled
                                PORT_PCR_PS(0);       // Pull resistor is set to pulldown (but is still disabled)

int main(void) {

  	/* Init board hardware. */
    BOARD_InitBootPins();
    BOARD_InitBootClocks();
    BOARD_InitBootPeripherals();
#ifndef BOARD_INIT_DEBUG_CONSOLE_PERIPHERAL
    /* Init FSL debug console. */
    BOARD_InitDebugConsole();
#endif

    NVIC_EnableIRQ(PORTD_IRQn);

    // LED Initialization
    LED_Initialize();
    LED_Off();

    // Enable and setup 3 pins in PORTA
    SIM-&amp;gt;SCGC5 |= SIM_SCGC5_PORTD_MASK;    //Enable the clock to port D

    PORTD-&amp;gt;PCR[5] = INPUT_CONFIG;     //Setup PTD5
    PORTD-&amp;gt;PCR[0] = INPUT_CONFIG;     //Setup PTD0
    PORTD-&amp;gt;PCR[2] = INPUT_CONFIG;     //Setup PTD2

    /* Force the counter to be placed into memory. */
    volatile static int i = 0 ;
    /* Enter an infinite loop, just incrementing a counter. */
    while(1) {
        i++ ;
        /* 'Dummy' NOP to allow source level single stepping of
            tight while() loop */
        __asm volatile ("nop");
    }
    return 0 ;
}

void PORTD_IRQHandler(void){
    //TODO: USE ISFR to see which pin triggered the interrupt

    LEDRed_On();

    //CLEAR INTERRUPT FLAG
    PORTD-&amp;gt;ISFR = 0xFFFFFFFF;
}&lt;/LI-CODE&gt;&lt;/LI-SPOILER&gt;&lt;P&gt;LED Utility Functions&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;LI-SPOILER&gt;&lt;LI-CODE lang="c"&gt;#include &amp;lt;MKL25Z4.h&amp;gt;
#include &amp;lt;LED.h&amp;gt;
/*----------------------------------------------------------------------------
  Function that initializes LEDs

  Note: You need to perform the following steps
  1. Turn on the clock gating to the appropriate ports
  2. Set the pin MUX to GPIO
  3. Set the pin to output
 ----------------------------------------------------------------------------*/
void LED_Initialize(void){
	//ENABLE RED LED
	SIM-&amp;gt;SCGC5 |= (1 &amp;lt;&amp;lt; 10);            //Enable the clock to port B
	PORTB-&amp;gt;PCR[18] = PORT_PCR_MUX(001); //Set up PTB18 as GPIO
	PTB-&amp;gt;PDDR |= (1 &amp;lt;&amp;lt; 18);             //Set bit 18 of PDDR for Port B to 1 (Port data direction register)

	//ENABLE GREEN LED
	//clock is already enabled to port B, don't need to do it again
	PORTB-&amp;gt;PCR[19] = PORT_PCR_MUX(001); //Set up PTB19 as GPIO
	PTB-&amp;gt;PDDR |= (1 &amp;lt;&amp;lt; 19);             //Set bit 19 of PDDR for Port B to 1 (Port data direction register)

	//Enable Blue LED
	SIM-&amp;gt;SCGC5 |= (1 &amp;lt;&amp;lt; 12);            //Enable the clock to port D
	PORTD-&amp;gt;PCR[1] = PORT_PCR_MUX(001);  //Set up PTD1 as GPIO
	PTD-&amp;gt;PDDR |= (1 &amp;lt;&amp;lt; 1);              //Set bit 1 of PDDR for Port D to 1 (Port data direction register)
}



/*---------------------------------------------------------------------------
 Three functions for toggling the current state of each LED individually
 ----------------------------------------------------------------------------*/
void LEDRed_Toggle(void){
	if(((PTB-&amp;gt;PDOR &amp;gt;&amp;gt; 18) &amp;amp; 0b1) == 1){ //If pin 18 of port B is 1, the LED is off
		LEDRed_On(); //so turn it on
	}else{
		LEDRed_Off(); //else turn it off
	}
}
void LEDGreen_Toggle(void){
	if(((PTB-&amp;gt;PDOR &amp;gt;&amp;gt; 19) &amp;amp; 0b1) == 1){ //If pin 19 of port B is 1, the LED is off
		LEDGreen_On(); //so turn it on
	}else{
		LEDGreen_Off(); //else turn it off
	}
}
void LEDBlue_Toggle(void){
	if(((PTD-&amp;gt;PDOR &amp;gt;&amp;gt; 1) &amp;amp; 0b1) == 1){ //If pin 1 of port D is 1, the LED is off
		LEDBlue_On(); //so turn it on
	}else{
		LEDBlue_Off(); //else turn it off
	}
}



/*---------------------------------------------------------------------------
 Three functions for toggling the turning ON LEDs individually
 ----------------------------------------------------------------------------*/
void LEDRed_On(void){
	PTB-&amp;gt;PCOR |= (1 &amp;lt;&amp;lt; 18);         	//Turn on the red LED (Using PCOR because LED is active-low)
}
void LEDGreen_On(void){
	PTB-&amp;gt;PCOR |= (1 &amp;lt;&amp;lt; 19);             //Turn on the green LED (Using PCOR because LED is active-low)
}
void LEDBlue_On(void){
	PTD-&amp;gt;PCOR |= (1 &amp;lt;&amp;lt; 1);             //Turn on the blue LED (Using PCOR because LED is active-low)
}



/*---------------------------------------------------------------------------
 Three functions for toggling the turning OFF LEDs individually
 ----------------------------------------------------------------------------*/
void LEDRed_Off(void){
	PTB-&amp;gt;PSOR |= (1 &amp;lt;&amp;lt; 18);         	//Turn off the red LED (Using PSOR because LED is active-low)
}
void LEDGreen_Off(void){
	PTB-&amp;gt;PSOR |= (1 &amp;lt;&amp;lt; 19);         	//Turn off the green LED (Using PSOR because LED is active-low)
}
void LEDBlue_Off(void){
	PTD-&amp;gt;PSOR |= (1 &amp;lt;&amp;lt; 1);             //Turn on the blue LED (Using PSOR because LED is active-low)
}



/*---------------------------------------------------------------------------
 One function turning OFF all 3 LEDs
 ----------------------------------------------------------------------------*/
void LED_Off(void){
	LEDRed_Off();
	LEDGreen_Off();
	LEDBlue_Off();
}&lt;/LI-CODE&gt;&lt;/LI-SPOILER&gt;&lt;P&gt;&lt;STRONG&gt;UPDATE: &lt;/STRONG&gt;I have confirmed that bits in Port D's&amp;nbsp;ISFR are being set when pins 0,5, and 2 experience a falling edge. This makes me think that the problem lies how I have enabled Port D interrupts rather than how I have configured the pins. The program continues running as normal despite the interrupt flags not being cleared. It seems that PORTD_IRQHandler is never being called.&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;UPDATE 2:&lt;/STRONG&gt; The interrupts do not seem to be reaching&amp;nbsp;NVIC-&amp;gt;ISPR register. Attached is a console screenshot showing this behavior.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Interrupts Registers.png" style="width: 819px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/250356i68CC476EB490FB61/image-size/large?v=v2&amp;amp;px=999" role="button" title="Interrupts Registers.png" alt="Interrupts Registers.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Fri, 17 Nov 2023 07:00:58 GMT</pubDate>
    <dc:creator>MelonM</dc:creator>
    <dc:date>2023-11-17T07:00:58Z</dc:date>
    <item>
      <title>GPIO Interrupt not triggering for FRDM-KL25z</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/GPIO-Interrupt-not-triggering-for-FRDM-KL25z/m-p/1758617#M65709</link>
      <description>&lt;P&gt;&lt;STRONG&gt;IMPORTANT: Updates at bottom of post&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;I'm trying to set up interrupts for pins 0,5, and 2 of Port D of my FRDM-KL25z. I want the interrupts to trigger on a falling edge. For testing purposes, I have written the ISR to turn on the Red LED, using code that wrote for a previous project (LED.c). Below is my main code file.&lt;/P&gt;&lt;P&gt;I've tried to execute the following steps to set up interrupts:&lt;/P&gt;&lt;OL&gt;&lt;LI&gt;Use the NVIC_EnableIRQ function to enable interrupts from Port D&lt;/LI&gt;&lt;LI&gt;Configure pins 0,2,5 as GPIO inputs and to request interrupts on the falling edge&lt;/LI&gt;&lt;LI&gt;Write the PORTD_IRQHandler function to do something (in this case, turn on the red LED).&lt;/LI&gt;&lt;/OL&gt;&lt;P&gt;Unfortunately, the red LED is not turning on when I transition any of the pins from logical 1 to 0. I've confirmed that the pins are functioning as inputs through some code that I haven't included in this post, so I must conclude that I have done something incorrectly or that I have missed a step.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Main code file:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;LI-SPOILER&gt;&lt;LI-CODE lang="c"&gt;#include &amp;lt;stdio.h&amp;gt;
#include "board.h"
#include "peripherals.h"
#include "pin_mux.h"
#include "clock_config.h"
#include "MKL25Z4.h"
#include "fsl_debug_console.h"
/* TODO: insert other include files here. */
#include "LED.h"
/* TODO: insert other definitions and declarations here. */

/*
 * @brief   Application entry point.
 */

const uint32_t INPUT_CONFIG =   PORT_PCR_IRQC(1010) | // IRQ Falling Edge
                                PORT_PCR_MUX(001)   | // Pin set to GPIO
                                PORT_PCR_DSE(0)     | // Low drive strength
                                PORT_PCR_PFE(0)     | // TODO: Passive filter disabled, try enabling if noisy
                                PORT_PCR_SRE(0)     | // TODO: Fast slew rate, look up what slow would mean
                                PORT_PCR_PE(0)      | // Pull resistor is disabled
                                PORT_PCR_PS(0);       // Pull resistor is set to pulldown (but is still disabled)

int main(void) {

  	/* Init board hardware. */
    BOARD_InitBootPins();
    BOARD_InitBootClocks();
    BOARD_InitBootPeripherals();
#ifndef BOARD_INIT_DEBUG_CONSOLE_PERIPHERAL
    /* Init FSL debug console. */
    BOARD_InitDebugConsole();
#endif

    NVIC_EnableIRQ(PORTD_IRQn);

    // LED Initialization
    LED_Initialize();
    LED_Off();

    // Enable and setup 3 pins in PORTA
    SIM-&amp;gt;SCGC5 |= SIM_SCGC5_PORTD_MASK;    //Enable the clock to port D

    PORTD-&amp;gt;PCR[5] = INPUT_CONFIG;     //Setup PTD5
    PORTD-&amp;gt;PCR[0] = INPUT_CONFIG;     //Setup PTD0
    PORTD-&amp;gt;PCR[2] = INPUT_CONFIG;     //Setup PTD2

    /* Force the counter to be placed into memory. */
    volatile static int i = 0 ;
    /* Enter an infinite loop, just incrementing a counter. */
    while(1) {
        i++ ;
        /* 'Dummy' NOP to allow source level single stepping of
            tight while() loop */
        __asm volatile ("nop");
    }
    return 0 ;
}

void PORTD_IRQHandler(void){
    //TODO: USE ISFR to see which pin triggered the interrupt

    LEDRed_On();

    //CLEAR INTERRUPT FLAG
    PORTD-&amp;gt;ISFR = 0xFFFFFFFF;
}&lt;/LI-CODE&gt;&lt;/LI-SPOILER&gt;&lt;P&gt;LED Utility Functions&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;LI-SPOILER&gt;&lt;LI-CODE lang="c"&gt;#include &amp;lt;MKL25Z4.h&amp;gt;
#include &amp;lt;LED.h&amp;gt;
/*----------------------------------------------------------------------------
  Function that initializes LEDs

  Note: You need to perform the following steps
  1. Turn on the clock gating to the appropriate ports
  2. Set the pin MUX to GPIO
  3. Set the pin to output
 ----------------------------------------------------------------------------*/
void LED_Initialize(void){
	//ENABLE RED LED
	SIM-&amp;gt;SCGC5 |= (1 &amp;lt;&amp;lt; 10);            //Enable the clock to port B
	PORTB-&amp;gt;PCR[18] = PORT_PCR_MUX(001); //Set up PTB18 as GPIO
	PTB-&amp;gt;PDDR |= (1 &amp;lt;&amp;lt; 18);             //Set bit 18 of PDDR for Port B to 1 (Port data direction register)

	//ENABLE GREEN LED
	//clock is already enabled to port B, don't need to do it again
	PORTB-&amp;gt;PCR[19] = PORT_PCR_MUX(001); //Set up PTB19 as GPIO
	PTB-&amp;gt;PDDR |= (1 &amp;lt;&amp;lt; 19);             //Set bit 19 of PDDR for Port B to 1 (Port data direction register)

	//Enable Blue LED
	SIM-&amp;gt;SCGC5 |= (1 &amp;lt;&amp;lt; 12);            //Enable the clock to port D
	PORTD-&amp;gt;PCR[1] = PORT_PCR_MUX(001);  //Set up PTD1 as GPIO
	PTD-&amp;gt;PDDR |= (1 &amp;lt;&amp;lt; 1);              //Set bit 1 of PDDR for Port D to 1 (Port data direction register)
}



/*---------------------------------------------------------------------------
 Three functions for toggling the current state of each LED individually
 ----------------------------------------------------------------------------*/
void LEDRed_Toggle(void){
	if(((PTB-&amp;gt;PDOR &amp;gt;&amp;gt; 18) &amp;amp; 0b1) == 1){ //If pin 18 of port B is 1, the LED is off
		LEDRed_On(); //so turn it on
	}else{
		LEDRed_Off(); //else turn it off
	}
}
void LEDGreen_Toggle(void){
	if(((PTB-&amp;gt;PDOR &amp;gt;&amp;gt; 19) &amp;amp; 0b1) == 1){ //If pin 19 of port B is 1, the LED is off
		LEDGreen_On(); //so turn it on
	}else{
		LEDGreen_Off(); //else turn it off
	}
}
void LEDBlue_Toggle(void){
	if(((PTD-&amp;gt;PDOR &amp;gt;&amp;gt; 1) &amp;amp; 0b1) == 1){ //If pin 1 of port D is 1, the LED is off
		LEDBlue_On(); //so turn it on
	}else{
		LEDBlue_Off(); //else turn it off
	}
}



/*---------------------------------------------------------------------------
 Three functions for toggling the turning ON LEDs individually
 ----------------------------------------------------------------------------*/
void LEDRed_On(void){
	PTB-&amp;gt;PCOR |= (1 &amp;lt;&amp;lt; 18);         	//Turn on the red LED (Using PCOR because LED is active-low)
}
void LEDGreen_On(void){
	PTB-&amp;gt;PCOR |= (1 &amp;lt;&amp;lt; 19);             //Turn on the green LED (Using PCOR because LED is active-low)
}
void LEDBlue_On(void){
	PTD-&amp;gt;PCOR |= (1 &amp;lt;&amp;lt; 1);             //Turn on the blue LED (Using PCOR because LED is active-low)
}



/*---------------------------------------------------------------------------
 Three functions for toggling the turning OFF LEDs individually
 ----------------------------------------------------------------------------*/
void LEDRed_Off(void){
	PTB-&amp;gt;PSOR |= (1 &amp;lt;&amp;lt; 18);         	//Turn off the red LED (Using PSOR because LED is active-low)
}
void LEDGreen_Off(void){
	PTB-&amp;gt;PSOR |= (1 &amp;lt;&amp;lt; 19);         	//Turn off the green LED (Using PSOR because LED is active-low)
}
void LEDBlue_Off(void){
	PTD-&amp;gt;PSOR |= (1 &amp;lt;&amp;lt; 1);             //Turn on the blue LED (Using PSOR because LED is active-low)
}



/*---------------------------------------------------------------------------
 One function turning OFF all 3 LEDs
 ----------------------------------------------------------------------------*/
void LED_Off(void){
	LEDRed_Off();
	LEDGreen_Off();
	LEDBlue_Off();
}&lt;/LI-CODE&gt;&lt;/LI-SPOILER&gt;&lt;P&gt;&lt;STRONG&gt;UPDATE: &lt;/STRONG&gt;I have confirmed that bits in Port D's&amp;nbsp;ISFR are being set when pins 0,5, and 2 experience a falling edge. This makes me think that the problem lies how I have enabled Port D interrupts rather than how I have configured the pins. The program continues running as normal despite the interrupt flags not being cleared. It seems that PORTD_IRQHandler is never being called.&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;UPDATE 2:&lt;/STRONG&gt; The interrupts do not seem to be reaching&amp;nbsp;NVIC-&amp;gt;ISPR register. Attached is a console screenshot showing this behavior.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Interrupts Registers.png" style="width: 819px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/250356i68CC476EB490FB61/image-size/large?v=v2&amp;amp;px=999" role="button" title="Interrupts Registers.png" alt="Interrupts Registers.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 17 Nov 2023 07:00:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/GPIO-Interrupt-not-triggering-for-FRDM-KL25z/m-p/1758617#M65709</guid>
      <dc:creator>MelonM</dc:creator>
      <dc:date>2023-11-17T07:00:58Z</dc:date>
    </item>
    <item>
      <title>Re: GPIO Interrupt not triggering for FRDM-KL25z</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/GPIO-Interrupt-not-triggering-for-FRDM-KL25z/m-p/1759458#M65715</link>
      <description>&lt;P&gt;I discovered the problem. In my declaration of the INPUT_CONFIG const, I wrote.&lt;/P&gt;&lt;LI-CODE lang="c"&gt;PORT_PCR_IRQC(1010)&lt;/LI-CODE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I intended to have this value be binary, but I forgot to write indicate it as such. Replacing it with the below line fixed the issue.&lt;/P&gt;&lt;LI-CODE lang="c"&gt;PORT_PCR_IRQC(0b1010)&lt;/LI-CODE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 20 Nov 2023 02:10:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/GPIO-Interrupt-not-triggering-for-FRDM-KL25z/m-p/1759458#M65715</guid>
      <dc:creator>MelonM</dc:creator>
      <dc:date>2023-11-20T02:10:54Z</dc:date>
    </item>
  </channel>
</rss>