<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Microcontrollers中的主题 Re: FRDM-K66F Bricked on Windows10</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-K66F-Bricked-on-Windows10/m-p/1730062#M65578</link>
    <description>&lt;P&gt;I'm trying to put the bin files inside of the bootloader, however, as soon as I drag and drop the file I get this error, I've attached a screenshot.&amp;nbsp;&lt;BR /&gt;When I try to drag and drop the 0224_k20dx_bl_0x8000.bin file the board gets ejected automatically.&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Wed, 27 Sep 2023 02:52:00 GMT</pubDate>
    <dc:creator>AerafKhan</dc:creator>
    <dc:date>2023-09-27T02:52:00Z</dc:date>
    <item>
      <title>FRDM-K66F Bricked on Windows10</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-K66F-Bricked-on-Windows10/m-p/846590#M50944</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am not new to microcontrollers, but very new to mbed controllers - new as in, blinky_led sample code bricked my controller 10 minutes after plugging it in for the first time.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For a few minutes, after loading blinky_led and trying to move to the next example, I was stuck with the controller mounting and showing up as bootloader.&amp;nbsp; It would periodically reboot and remount every minute or so.&amp;nbsp; So I tried updating the firmware by dragging-and-dropping the .bin file from&amp;nbsp; &lt;A class="link-titled" href="https://os.mbed.com/platforms/FRDM-K66F/" title="https://os.mbed.com/platforms/FRDM-K66F/"&gt;FRDM-K66F | Mbed&lt;/A&gt; .&amp;nbsp; Now the board doesn't even light up when plugged into USB and Windows doesn't recognize any device being plugged in.&amp;nbsp; If I plug into the power port, blinky_led will run.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have a second board but I'm afraid to use it.&amp;nbsp; I plugged it in hoping that I could use it to install the Windows ARM serial driver, as I was receiving "no microcontroller found" with the bricked one - nope still get error despite this being the very first instruction on the aforementioned mbed website.&amp;nbsp; So I tried to do this right, and held down reset to go into bootloader mode, and at the beginning of a remounting cycle, tried to copy over the firmware.&amp;nbsp; NOPE!&amp;nbsp; firmware is 95kB and I only have 92kB of freespace on the board!&amp;nbsp; Also, the article says DAPLink needs to be upgraded if it mounts as "bootloader" - ok, but of course, there is no FRDM-K66F listed in the table: &lt;A class="link-titled" href="https://os.mbed.com/blog/entry/DAPLink-bootloader-update/" title="https://os.mbed.com/blog/entry/DAPLink-bootloader-update/"&gt;DAPLink bootloader update | Mbed&lt;/A&gt;&amp;nbsp; .&amp;nbsp; I would use the K64F, but its such a fragile piece of equipment, that I'm afraid to.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;None of the instructions to keep this delicate thing from dying seem to work.&amp;nbsp; My second board is now stuck in bootloader mode, probably soon to be bricked as well.&amp;nbsp; Please help.&amp;nbsp; I want to use this board, but I'm frustrated by how out-of-the-box instructions don't work and can actually kill the board.&amp;nbsp; I haven't even tried anything unique yet.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;EDIT:&lt;/P&gt;&lt;P&gt;Got board #2 working ok.&amp;nbsp; For some reason I showed 98kB of free space when loaded into Linux and could copy the firmware, which made the device appear as a drive called FRDM-K66FD.&amp;nbsp; And then the serial driver would install correctly.&amp;nbsp; I'm still stuck short of having a probe to allow debugging.&amp;nbsp; I checked my downloads, I believe I dropped blinkyled.bin onto the BootLoader drive which killed the first board - I did not drop firmware.&amp;nbsp; Hopefully there is a repair for this mistake.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 16 Nov 2018 16:15:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-K66F-Bricked-on-Windows10/m-p/846590#M50944</guid>
      <dc:creator>eflament</dc:creator>
      <dc:date>2018-11-16T16:15:58Z</dc:date>
    </item>
    <item>
      <title>Re: FRDM-K66F Bricked on Windows10</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-K66F-Bricked-on-Windows10/m-p/846591#M50945</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&amp;nbsp;E F,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please refer the answer in&amp;nbsp; &lt;A _jive_internal="true" href="https://community.nxp.com/thread/487624"&gt;Really Hard Bricked FRDM-K22F Boards&lt;/A&gt;.&lt;/P&gt;&lt;P&gt;&lt;EM&gt;In any case, you need a separate/external device to re-program the bootloader.&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;there is no FRDM-K66F listed in the table&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;You can download the&amp;nbsp;&lt;A href="https://www.nxp.com/support/developer-resources/run-time-software/kinetis-developer-resources/ides-for-kinetis-mcus/opensda-serial-and-debug-adapter:OPENSDA#FRDM-K66F"&gt;latest bootloader and firmware application&lt;/A&gt; of DAPLink rev0244. I have also attached these two files here.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Robin&lt;/P&gt;&lt;P style="min- padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 21 Nov 2018 03:13:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-K66F-Bricked-on-Windows10/m-p/846591#M50945</guid>
      <dc:creator>Robin_Shen</dc:creator>
      <dc:date>2018-11-21T03:13:28Z</dc:date>
    </item>
    <item>
      <title>Re: FRDM-K66F Bricked on Windows10</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-K66F-Bricked-on-Windows10/m-p/1730062#M65578</link>
      <description>&lt;P&gt;I'm trying to put the bin files inside of the bootloader, however, as soon as I drag and drop the file I get this error, I've attached a screenshot.&amp;nbsp;&lt;BR /&gt;When I try to drag and drop the 0224_k20dx_bl_0x8000.bin file the board gets ejected automatically.&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 27 Sep 2023 02:52:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-K66F-Bricked-on-Windows10/m-p/1730062#M65578</guid>
      <dc:creator>AerafKhan</dc:creator>
      <dc:date>2023-09-27T02:52:00Z</dc:date>
    </item>
    <item>
      <title>Re: FRDM-K66F Bricked on Windows10</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-K66F-Bricked-on-Windows10/m-p/1730089#M65581</link>
      <description>&lt;P&gt;Have you already updated the bootloader itself to a version working with your machine? See &lt;A href="https://mcuoneclipse.com/2016/08/01/bricking_and_recovering_opensda_boards_in_windows_8_and_10/" target="_blank"&gt;https://mcuoneclipse.com/2016/08/01/bricking_and_recovering_opensda_boards_in_windows_8_and_10/&lt;/A&gt;&lt;/P&gt;</description>
      <pubDate>Wed, 27 Sep 2023 03:49:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-K66F-Bricked-on-Windows10/m-p/1730089#M65581</guid>
      <dc:creator>ErichStyger</dc:creator>
      <dc:date>2023-09-27T03:49:16Z</dc:date>
    </item>
  </channel>
</rss>