<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックRe: GoMCUxpresso conflict</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/GoMCUxpresso-conflict/m-p/1723676#M65547</link>
    <description>&lt;P&gt;Good morning&lt;/P&gt;&lt;P&gt;I am using Windows 10 x64, MCUXpresso v11.7.1_9221.&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;P&gt;In the VBOX I use the same operating system. The project is using the K64, and it is a huge development not imported from any example.&amp;nbsp;&lt;BR /&gt;The project has worked for years on KDS. Possibly after the installation of the Embarcadero CBuilder new release the problem started. The KDS does not find the JTAG without any consistent message other than a generic error. The MCUxpresso does not want to build at all because is trying to use the make of Embarcadero.&lt;BR /&gt;I tried to test the MCUxpresso with an example project&amp;nbsp; and it works.&amp;nbsp;&lt;/P&gt;&lt;P&gt;That's all.&lt;BR /&gt;It seems something went wrong during the export. But I would prefer to use the KDS still.&lt;BR /&gt;Thank You&lt;/P&gt;&lt;P&gt;Pietro&lt;/P&gt;</description>
    <pubDate>Fri, 15 Sep 2023 06:55:35 GMT</pubDate>
    <dc:creator>pietrodicastri</dc:creator>
    <dc:date>2023-09-15T06:55:35Z</dc:date>
    <item>
      <title>GoMCUxpresso conflict</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/GoMCUxpresso-conflict/m-p/1722076#M65537</link>
      <description>&lt;P&gt;Good morning&lt;/P&gt;&lt;P&gt;I have a project imported from the KDS. Whe I try to build it gives this message&lt;/P&gt;&lt;P&gt;14:45:13 **** Clean-only build of configuration Debug2 for project Capas2p0_008 ****&lt;BR /&gt;make clean&lt;BR /&gt;MAKE Version 5.41 Copyright (c) 1987, 2014 Embarcadero Technologies, Inc.&lt;BR /&gt;Error makefile 6: Command syntax error&lt;BR /&gt;Error makefile 11: Command syntax error&lt;BR /&gt;Error makefile 12: Command syntax error&lt;BR /&gt;Error makefile 13: Command syntax error&lt;BR /&gt;Error makefile 14: Command syntax error&lt;BR /&gt;Error makefile 15: Command syntax error&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;and more of.&lt;BR /&gt;It seems it is conflicting with the Embarcadero make.&amp;nbsp;&lt;BR /&gt;What to do?&lt;/P&gt;&lt;P&gt;Thank You&lt;/P&gt;&lt;P&gt;Pietro&lt;/P&gt;</description>
      <pubDate>Wed, 13 Sep 2023 12:49:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/GoMCUxpresso-conflict/m-p/1722076#M65537</guid>
      <dc:creator>pietrodicastri</dc:creator>
      <dc:date>2023-09-13T12:49:06Z</dc:date>
    </item>
    <item>
      <title>Re: GoMCUxpresso conflict</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/GoMCUxpresso-conflict/m-p/1722080#M65538</link>
      <description>I specify the tool works with other projects. Something related to the importing is producing the error&lt;BR /&gt;</description>
      <pubDate>Wed, 13 Sep 2023 12:52:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/GoMCUxpresso-conflict/m-p/1722080#M65538</guid>
      <dc:creator>pietrodicastri</dc:creator>
      <dc:date>2023-09-13T12:52:41Z</dc:date>
    </item>
    <item>
      <title>Re: GoMCUxpresso conflict</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/GoMCUxpresso-conflict/m-p/1722787#M65542</link>
      <description>If I install on a VBox on the same PC it works.&lt;BR /&gt;Please suggest something. It is difficult to work on the VBox...&lt;BR /&gt;Thank You</description>
      <pubDate>Thu, 14 Sep 2023 06:18:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/GoMCUxpresso-conflict/m-p/1722787#M65542</guid>
      <dc:creator>pietrodicastri</dc:creator>
      <dc:date>2023-09-14T06:18:32Z</dc:date>
    </item>
    <item>
      <title>Re: GoMCUxpresso conflict</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/GoMCUxpresso-conflict/m-p/1723352#M65544</link>
      <description>&lt;P class="lia-align-justify"&gt;Hello &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/20031"&gt;@pietrodicastri&lt;/a&gt;,&lt;/P&gt;
&lt;P class="lia-align-justify"&gt;Could you please give us more details about what you are doing? Which MCUXpresso IDE version are you using? Which OS do you have both in VBox and your computer? From which microcontroller are you importing the project? Is the project an example code or your own development?&lt;/P&gt;
&lt;P class="lia-align-justify"&gt;At the meantime, could you please take a look at the following information?&lt;/P&gt;
&lt;UL class="lia-align-justify" type="disc"&gt;
&lt;LI&gt;&lt;A href="https://community.nxp.com/t5/MCUXpresso-IDE-Knowledge-Base/Moving-to-MCUXpresso-IDE-from-Kinetis-Design-Studio/ta-p/1104459#:~:text=There%20is%20no%20automatic%20tool%20to%20take%20a,in%20the%20custom%20source%20code%20and%20other%20modifications." target="_blank"&gt;Moving to MCUXpresso IDE from Kinetis Design Studi... - NXP Community&lt;/A&gt;&lt;/LI&gt;
&lt;LI&gt;&lt;A href="https://mcuoneclipse.com/2017/04/02/mcuxpresso-ide-importing-kinetis-design-studio-projects/" target="_blank"&gt;MCUXpresso IDE: Importing Kinetis Design Studio Projects | MCU on Eclipse&lt;/A&gt;&lt;/LI&gt;
&lt;/UL&gt;
&lt;P class="lia-align-justify"&gt;Kind regards, Raul.&lt;/P&gt;</description>
      <pubDate>Thu, 14 Sep 2023 18:39:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/GoMCUxpresso-conflict/m-p/1723352#M65544</guid>
      <dc:creator>RaRo</dc:creator>
      <dc:date>2023-09-14T18:39:51Z</dc:date>
    </item>
    <item>
      <title>Re: GoMCUxpresso conflict</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/GoMCUxpresso-conflict/m-p/1723676#M65547</link>
      <description>&lt;P&gt;Good morning&lt;/P&gt;&lt;P&gt;I am using Windows 10 x64, MCUXpresso v11.7.1_9221.&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;P&gt;In the VBOX I use the same operating system. The project is using the K64, and it is a huge development not imported from any example.&amp;nbsp;&lt;BR /&gt;The project has worked for years on KDS. Possibly after the installation of the Embarcadero CBuilder new release the problem started. The KDS does not find the JTAG without any consistent message other than a generic error. The MCUxpresso does not want to build at all because is trying to use the make of Embarcadero.&lt;BR /&gt;I tried to test the MCUxpresso with an example project&amp;nbsp; and it works.&amp;nbsp;&lt;/P&gt;&lt;P&gt;That's all.&lt;BR /&gt;It seems something went wrong during the export. But I would prefer to use the KDS still.&lt;BR /&gt;Thank You&lt;/P&gt;&lt;P&gt;Pietro&lt;/P&gt;</description>
      <pubDate>Fri, 15 Sep 2023 06:55:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/GoMCUxpresso-conflict/m-p/1723676#M65547</guid>
      <dc:creator>pietrodicastri</dc:creator>
      <dc:date>2023-09-15T06:55:35Z</dc:date>
    </item>
    <item>
      <title>Re: GoMCUxpresso conflict</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/GoMCUxpresso-conflict/m-p/1723707#M65548</link>
      <description>I reinstalled the KDS and it is working..&lt;BR /&gt;Thank You</description>
      <pubDate>Fri, 15 Sep 2023 07:40:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/GoMCUxpresso-conflict/m-p/1723707#M65548</guid>
      <dc:creator>pietrodicastri</dc:creator>
      <dc:date>2023-09-15T07:40:43Z</dc:date>
    </item>
  </channel>
</rss>