<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックMK66 usb_device_hid_generic sometimes fails when going through a usb hub</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/MK66-usb-device-hid-generic-sometimes-fails-when-going-through-a/m-p/1698689#M65393</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&amp;nbsp;I have a project based on the usb_device_hid_generic example for an MK66. Using SDK_2.6.0_FRDM_K66F. When communicating with my device through a PC, I typically don't have an issue. When my device is connected via a USB hub, sometimes a HID communication will fail. This has happened with multiple hubs. Has anyone seen this issue and have any suggestions? Thank you&lt;/P&gt;</description>
    <pubDate>Thu, 03 Aug 2023 14:14:04 GMT</pubDate>
    <dc:creator>ryan_pearson</dc:creator>
    <dc:date>2023-08-03T14:14:04Z</dc:date>
    <item>
      <title>MK66 usb_device_hid_generic sometimes fails when going through a usb hub</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/MK66-usb-device-hid-generic-sometimes-fails-when-going-through-a/m-p/1698689#M65393</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&amp;nbsp;I have a project based on the usb_device_hid_generic example for an MK66. Using SDK_2.6.0_FRDM_K66F. When communicating with my device through a PC, I typically don't have an issue. When my device is connected via a USB hub, sometimes a HID communication will fail. This has happened with multiple hubs. Has anyone seen this issue and have any suggestions? Thank you&lt;/P&gt;</description>
      <pubDate>Thu, 03 Aug 2023 14:14:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/MK66-usb-device-hid-generic-sometimes-fails-when-going-through-a/m-p/1698689#M65393</guid>
      <dc:creator>ryan_pearson</dc:creator>
      <dc:date>2023-08-03T14:14:04Z</dc:date>
    </item>
    <item>
      <title>Re: MK66 usb_device_hid_generic sometimes fails when going through a usb hub</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/MK66-usb-device-hid-generic-sometimes-fails-when-going-through-a/m-p/1698829#M65395</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/134913"&gt;@ryan_pearson&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;USB hubs have disadvantages and could be the cause of your issue.&lt;/P&gt;
&lt;P&gt;Not enough power supplied to the MCU, add latency to the usb port in PC and could affect performance in data transfer speed.&lt;/P&gt;
&lt;P&gt;I highly recommend you to connect the MCU directly to the pc instead of the hub or while debuging disconnect other unused devices on the hub.&lt;/P&gt;
&lt;P&gt;Best Regards,Miguel.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 03 Aug 2023 18:03:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/MK66-usb-device-hid-generic-sometimes-fails-when-going-through-a/m-p/1698829#M65395</guid>
      <dc:creator>Miguel04</dc:creator>
      <dc:date>2023-08-03T18:03:54Z</dc:date>
    </item>
  </channel>
</rss>