<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Microcontrollers中的主题 Re: Fail to connect MKM34Z256</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Fail-to-connect-MKM34Z256/m-p/1693044#M65324</link>
    <description>&lt;P&gt;Hi Pavel,&lt;/P&gt;&lt;P&gt;I am getting below error in MCUXpresso IDE -&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Executing flash operation 'Resurrect locked Kinetis device' (Resurrect locked Kinetis device) - Wed Jul 26 16:57:28 IST 2023&lt;BR /&gt;Checking MCU info...&lt;BR /&gt;Scanning for targets...&lt;BR /&gt;Executing flash action...&lt;BR /&gt;SEGGER J-Link Commander V7.86 (Compiled Feb 15 2023 17:16:22)&lt;BR /&gt;DLL version V7.86, compiled Feb 15 2023 17:14:56&lt;BR /&gt;J-Link Command File read successfully.&lt;BR /&gt;Processing script file...&lt;BR /&gt;J-Link&amp;gt;ExitOnError 1&lt;BR /&gt;J-Link Commander will now exit on Error&lt;BR /&gt;J-Link&amp;gt;unlock kinetis&lt;BR /&gt;J-Link connection not established yet but required for command.&lt;BR /&gt;Connecting to J-Link via USB...O.K.&lt;BR /&gt;Firmware: J-Link WiFi-V1 compiled Mar 15 2023 11:22:42&lt;BR /&gt;Hardware version: V1.00&lt;BR /&gt;J-Link uptime (since boot): 0d 00h 06m 31s&lt;BR /&gt;S/N: 941000092&lt;BR /&gt;License(s): RDI, FlashBP, FlashDL, JFlash, GDB&lt;BR /&gt;USB speed mode: High speed (480 MBit/s)&lt;BR /&gt;IP-Addr: DHCP (no addr. received yet)&lt;BR /&gt;VTref=3.277V&lt;BR /&gt;Found SWD-DP with ID 0x0BC11477&lt;BR /&gt;Unlocking device...Unlock via debug port is disabled. Unlock failed.&lt;BR /&gt;Timeout while unlocking device.&lt;BR /&gt;Script processing completed.&lt;BR /&gt;Unable to perform operation!&lt;BR /&gt;Command failed with exit code 1&lt;/P&gt;&lt;P&gt;Thanks,&lt;BR /&gt;Rahul&lt;/P&gt;</description>
    <pubDate>Wed, 26 Jul 2023 11:29:59 GMT</pubDate>
    <dc:creator>rahul_4</dc:creator>
    <dc:date>2023-07-26T11:29:59Z</dc:date>
    <item>
      <title>Fail to connect MKM34Z256</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Fail-to-connect-MKM34Z256/m-p/1692188#M65314</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;During programming, I am getting below error -&amp;nbsp;&lt;/P&gt;&lt;P&gt;Connecting ...&lt;BR /&gt;- Connecting via USB to probe/ programmer device 0&lt;BR /&gt;- Probe/ Programmer firmware: J-Link WiFi-V1 compiled Mar 15 2023 11:22:42&lt;BR /&gt;- Device "MKM34Z256XXX7" selected.&lt;BR /&gt;- Target interface speed: 4000 kHz (Fixed)&lt;BR /&gt;- VTarget = 3.290V&lt;BR /&gt;- InitTarget()&lt;BR /&gt;- Readout protection is set and mass erase is disabled. J-Link cannot unprotect the device.&lt;BR /&gt;- Found SW-DP with ID 0x0BC11477&lt;BR /&gt;- DPIDR: 0x0BC11477&lt;BR /&gt;- CoreSight SoC-400 or earlier&lt;BR /&gt;- Scanning AP map to find all available APs&lt;BR /&gt;- AP[2]: Stopped AP scan as end of AP map has been reached&lt;BR /&gt;- AP[0]: AHB-AP (IDR: 0x04770031)&lt;BR /&gt;- AP[1]: JTAG-AP (IDR: 0x001C0020)&lt;BR /&gt;- Iterating through AP map to find AHB-AP to use&lt;BR /&gt;- AP[0]: Skipped. Could not read CPUID register&lt;BR /&gt;- AP[1]: Skipped. Not an AHB-AP&lt;BR /&gt;- Attach to CPU failed. Executing connect under reset.&lt;BR /&gt;- DPIDR: 0x0BC11477&lt;BR /&gt;- CoreSight SoC-400 or earlier&lt;BR /&gt;- Scanning AP map to find all available APs&lt;BR /&gt;- AP[2]: Stopped AP scan as end of AP map has been reached&lt;BR /&gt;- AP[0]: AHB-AP (IDR: 0x04770031)&lt;BR /&gt;- AP[1]: JTAG-AP (IDR: 0x001C0020)&lt;BR /&gt;- Iterating through AP map to find AHB-AP to use&lt;BR /&gt;- AP[0]: Skipped. Could not read CPUID register&lt;BR /&gt;- AP[1]: Skipped. Not an AHB-AP&lt;BR /&gt;- Could not find core in Coresight setup&lt;BR /&gt;- InitTarget()&lt;BR /&gt;- Readout protection is set and mass erase is disabled. J-Link cannot unprotect the device.&lt;BR /&gt;- Found SW-DP with ID 0x0BC11477&lt;BR /&gt;- DPIDR: 0x0BC11477&lt;BR /&gt;- CoreSight SoC-400 or earlier&lt;BR /&gt;- Scanning AP map to find all available APs&lt;BR /&gt;- AP[2]: Stopped AP scan as end of AP map has been reached&lt;BR /&gt;- AP[0]: AHB-AP (IDR: 0x04770031)&lt;BR /&gt;- AP[1]: JTAG-AP (IDR: 0x001C0020)&lt;BR /&gt;- Iterating through AP map to find AHB-AP to use&lt;BR /&gt;- AP[0]: Skipped. Could not read CPUID register&lt;BR /&gt;- AP[1]: Skipped. Not an AHB-AP&lt;BR /&gt;- Attach to CPU failed. Executing connect under reset.&lt;BR /&gt;- DPIDR: 0x0BC11477&lt;BR /&gt;- CoreSight SoC-400 or earlier&lt;BR /&gt;- Scanning AP map to find all available APs&lt;BR /&gt;- AP[2]: Stopped AP scan as end of AP map has been reached&lt;BR /&gt;- AP[0]: AHB-AP (IDR: 0x04770031)&lt;BR /&gt;- AP[1]: JTAG-AP (IDR: 0x001C0020)&lt;BR /&gt;- Iterating through AP map to find AHB-AP to use&lt;BR /&gt;- AP[0]: Skipped. Could not read CPUID register&lt;BR /&gt;- AP[1]: Skipped. Not an AHB-AP&lt;BR /&gt;- Could not find core in Coresight setup&lt;BR /&gt;- ERROR: Failed to connect.&lt;BR /&gt;Could not establish a connection to target.&lt;/P&gt;&lt;P&gt;Can you please guide me how to solve this issue?&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Rahul&lt;/P&gt;</description>
      <pubDate>Tue, 25 Jul 2023 10:07:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Fail-to-connect-MKM34Z256/m-p/1692188#M65314</guid>
      <dc:creator>rahul_4</dc:creator>
      <dc:date>2023-07-25T10:07:35Z</dc:date>
    </item>
    <item>
      <title>Re: Fail to connect MKM34Z256</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Fail-to-connect-MKM34Z256/m-p/1692453#M65318</link>
      <description>&lt;P&gt;Hello, my name is Pavel, and I will be supporting your case, I reviewed your information, but could you tell me if you have an EVK board or if this is a custom?&lt;/P&gt;&lt;P&gt;If your board is custom trying to do a mass erase. In case you have an EVK try to follow the steps on the next page.&lt;/P&gt;&lt;P&gt;&lt;A href="https://mcuoneclipse.com/2022/06/16/resurrecting-bricked-nxp-kinetis-devices/" target="_blank"&gt;Resurrecting ‘bricked’ NXP Kinetis Devices | MCU on Eclipse&lt;/A&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;BR /&gt;Pavel&lt;/P&gt;</description>
      <pubDate>Tue, 25 Jul 2023 19:10:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Fail-to-connect-MKM34Z256/m-p/1692453#M65318</guid>
      <dc:creator>Pavel_Hernandez</dc:creator>
      <dc:date>2023-07-25T19:10:02Z</dc:date>
    </item>
    <item>
      <title>Re: Fail to connect MKM34Z256</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Fail-to-connect-MKM34Z256/m-p/1692830#M65321</link>
      <description>&lt;P&gt;Hi Pavel,&lt;/P&gt;&lt;P&gt;I am using custom board.&lt;/P&gt;&lt;P&gt;Thanks,&lt;BR /&gt;Rahul&lt;/P&gt;</description>
      <pubDate>Wed, 26 Jul 2023 07:56:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Fail-to-connect-MKM34Z256/m-p/1692830#M65321</guid>
      <dc:creator>rahul_4</dc:creator>
      <dc:date>2023-07-26T07:56:06Z</dc:date>
    </item>
    <item>
      <title>Re: Fail to connect MKM34Z256</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Fail-to-connect-MKM34Z256/m-p/1693044#M65324</link>
      <description>&lt;P&gt;Hi Pavel,&lt;/P&gt;&lt;P&gt;I am getting below error in MCUXpresso IDE -&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Executing flash operation 'Resurrect locked Kinetis device' (Resurrect locked Kinetis device) - Wed Jul 26 16:57:28 IST 2023&lt;BR /&gt;Checking MCU info...&lt;BR /&gt;Scanning for targets...&lt;BR /&gt;Executing flash action...&lt;BR /&gt;SEGGER J-Link Commander V7.86 (Compiled Feb 15 2023 17:16:22)&lt;BR /&gt;DLL version V7.86, compiled Feb 15 2023 17:14:56&lt;BR /&gt;J-Link Command File read successfully.&lt;BR /&gt;Processing script file...&lt;BR /&gt;J-Link&amp;gt;ExitOnError 1&lt;BR /&gt;J-Link Commander will now exit on Error&lt;BR /&gt;J-Link&amp;gt;unlock kinetis&lt;BR /&gt;J-Link connection not established yet but required for command.&lt;BR /&gt;Connecting to J-Link via USB...O.K.&lt;BR /&gt;Firmware: J-Link WiFi-V1 compiled Mar 15 2023 11:22:42&lt;BR /&gt;Hardware version: V1.00&lt;BR /&gt;J-Link uptime (since boot): 0d 00h 06m 31s&lt;BR /&gt;S/N: 941000092&lt;BR /&gt;License(s): RDI, FlashBP, FlashDL, JFlash, GDB&lt;BR /&gt;USB speed mode: High speed (480 MBit/s)&lt;BR /&gt;IP-Addr: DHCP (no addr. received yet)&lt;BR /&gt;VTref=3.277V&lt;BR /&gt;Found SWD-DP with ID 0x0BC11477&lt;BR /&gt;Unlocking device...Unlock via debug port is disabled. Unlock failed.&lt;BR /&gt;Timeout while unlocking device.&lt;BR /&gt;Script processing completed.&lt;BR /&gt;Unable to perform operation!&lt;BR /&gt;Command failed with exit code 1&lt;/P&gt;&lt;P&gt;Thanks,&lt;BR /&gt;Rahul&lt;/P&gt;</description>
      <pubDate>Wed, 26 Jul 2023 11:29:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Fail-to-connect-MKM34Z256/m-p/1693044#M65324</guid>
      <dc:creator>rahul_4</dc:creator>
      <dc:date>2023-07-26T11:29:59Z</dc:date>
    </item>
    <item>
      <title>Re: Fail to connect MKM34Z256</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Fail-to-connect-MKM34Z256/m-p/1693593#M65328</link>
      <description>&lt;P&gt;Hello, have you ever this available to program the MCU in the past? It seems like the MCU is blocking.&lt;/P&gt;
&lt;P&gt;Could you read the FSEC? and share the result.&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com/docs/en/application-note/AN4835.pdf?_gl=1*1hlhhqa*_ga*MjAwNDQ2NjI3My4xNjkwNDEzNzA5*_ga_WM5LE0KMSH*MTY5MDQxMzcwOC4xLjEuMTY5MDQxMzkxMC4wLjAuMA.." target="_blank"&gt;Production Flash programming best practices for Kinetis K and L MCUs (nxp.com)&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;This app note shows different methods to do a mass erase.&lt;/P&gt;
&lt;P&gt;Best regards,&lt;BR /&gt;Pavel&lt;/P&gt;</description>
      <pubDate>Wed, 26 Jul 2023 23:27:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Fail-to-connect-MKM34Z256/m-p/1693593#M65328</guid>
      <dc:creator>Pavel_Hernandez</dc:creator>
      <dc:date>2023-07-26T23:27:01Z</dc:date>
    </item>
  </channel>
</rss>