<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic LoRa SX1278 and KL25Z in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/LoRa-SX1278-and-KL25Z/m-p/1690718#M65307</link>
    <description>&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;I am trying to use a LoRa module based on the SX1278 RF transceiver with the KL25Z MCU. The two devices are meant to communicate through SPI so I have developed a library to implement this, and then another library specifically for the LoRa SPI communication. The problem is that I am not receiving appropriate messages from the LoRa module in response to the commands I am sending.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Some key points...&lt;/P&gt;&lt;P&gt;-&amp;gt; I have tested the SPI library with Arduino and confirmed it's working;&lt;/P&gt;&lt;P&gt;-&amp;gt; I have developed a LoRa library to implement SPI communication specifically to address the SX1278 module based on the same library implemented in Arduino projects (I have simply translated from C++ to C);&lt;/P&gt;&lt;P&gt;-&amp;gt; I know the KL25Z is sending commands to the LoRa module as I observed with a logic analyser, but the RF module is not responding at all.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Does anyone know how to fix this?&lt;/P&gt;</description>
    <pubDate>Sat, 22 Jul 2023 11:21:37 GMT</pubDate>
    <dc:creator>gnps44</dc:creator>
    <dc:date>2023-07-22T11:21:37Z</dc:date>
    <item>
      <title>LoRa SX1278 and KL25Z</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/LoRa-SX1278-and-KL25Z/m-p/1690718#M65307</link>
      <description>&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;I am trying to use a LoRa module based on the SX1278 RF transceiver with the KL25Z MCU. The two devices are meant to communicate through SPI so I have developed a library to implement this, and then another library specifically for the LoRa SPI communication. The problem is that I am not receiving appropriate messages from the LoRa module in response to the commands I am sending.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Some key points...&lt;/P&gt;&lt;P&gt;-&amp;gt; I have tested the SPI library with Arduino and confirmed it's working;&lt;/P&gt;&lt;P&gt;-&amp;gt; I have developed a LoRa library to implement SPI communication specifically to address the SX1278 module based on the same library implemented in Arduino projects (I have simply translated from C++ to C);&lt;/P&gt;&lt;P&gt;-&amp;gt; I know the KL25Z is sending commands to the LoRa module as I observed with a logic analyser, but the RF module is not responding at all.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Does anyone know how to fix this?&lt;/P&gt;</description>
      <pubDate>Sat, 22 Jul 2023 11:21:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/LoRa-SX1278-and-KL25Z/m-p/1690718#M65307</guid>
      <dc:creator>gnps44</dc:creator>
      <dc:date>2023-07-22T11:21:37Z</dc:date>
    </item>
  </channel>
</rss>