<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Unused pins of KS22 Microcontroller in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Unused-pins-of-KS22-Microcontroller/m-p/1686328#M65283</link>
    <description>&lt;P&gt;Hi Erich&lt;/P&gt;&lt;P&gt;The part number of MCU is&amp;nbsp;&lt;SPAN&gt;MKS22FN256VLH12 and the data sheet is attached here.&lt;/SPAN&gt;&lt;/P&gt;</description>
    <pubDate>Wed, 12 Jul 2023 07:20:31 GMT</pubDate>
    <dc:creator>vishnuvariyath_2</dc:creator>
    <dc:date>2023-07-12T07:20:31Z</dc:date>
    <item>
      <title>Unused pins of KS22 Microcontroller</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Unused-pins-of-KS22-Microcontroller/m-p/1686282#M65281</link>
      <description>&lt;P&gt;I am using&amp;nbsp;&lt;SPAN&gt;MKS22FN256VLH12 in my application. Many pins not used in application.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;I don't know exactly what to do with these pins. Can they float, do they have to go to GND or VDD.&lt;/P&gt;&lt;P&gt;In KS22 there is two CAN modules and only one module is using in application, what to do with unused CAN module pins.&lt;BR /&gt;&lt;BR /&gt;I referred in the "Data sheet and Kinetis Ks22 Sub-Family Reference Manual " there is no correct answer for this.&lt;/P&gt;&lt;P&gt;Can someone give me a hint or help me with this?&lt;/P&gt;</description>
      <pubDate>Wed, 12 Jul 2023 06:23:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Unused-pins-of-KS22-Microcontroller/m-p/1686282#M65281</guid>
      <dc:creator>vishnuvariyath_2</dc:creator>
      <dc:date>2023-07-12T06:23:30Z</dc:date>
    </item>
    <item>
      <title>Re: Unused pins of KS22 Microcontroller</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Unused-pins-of-KS22-Microcontroller/m-p/1686297#M65282</link>
      <description>&lt;P&gt;I think you mean the MK22 and not a MKS22?&lt;/P&gt;&lt;P&gt;You can keep unused pins floating, see &lt;A href="https://community.nxp.com/t5/Wireless-Connectivity-Knowledge/Configuration-for-Unused-Pins-GPIOs-on-Kinetis/ta-p/1107797" target="_blank"&gt;https://community.nxp.com/t5/Wireless-Connectivity-Knowledge/Configuration-for-Unused-Pins-GPIOs-on-Kinetis/ta-p/1107797&lt;/A&gt;&lt;/P&gt;</description>
      <pubDate>Wed, 12 Jul 2023 06:40:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Unused-pins-of-KS22-Microcontroller/m-p/1686297#M65282</guid>
      <dc:creator>ErichStyger</dc:creator>
      <dc:date>2023-07-12T06:40:39Z</dc:date>
    </item>
    <item>
      <title>Re: Unused pins of KS22 Microcontroller</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Unused-pins-of-KS22-Microcontroller/m-p/1686328#M65283</link>
      <description>&lt;P&gt;Hi Erich&lt;/P&gt;&lt;P&gt;The part number of MCU is&amp;nbsp;&lt;SPAN&gt;MKS22FN256VLH12 and the data sheet is attached here.&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Wed, 12 Jul 2023 07:20:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Unused-pins-of-KS22-Microcontroller/m-p/1686328#M65283</guid>
      <dc:creator>vishnuvariyath_2</dc:creator>
      <dc:date>2023-07-12T07:20:31Z</dc:date>
    </item>
    <item>
      <title>Re: Unused pins of KS22 Microcontroller</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Unused-pins-of-KS22-Microcontroller/m-p/1686838#M65287</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/220129"&gt;@vishnuvariyath_2&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;This information is from the datasheet:&lt;/P&gt;
&lt;P&gt;&lt;EM&gt;Unused GPIO pins must be left floating (no electrical connections) with the MUX&amp;nbsp;&lt;/EM&gt;&lt;EM&gt;field of the pin’s PORTx_PCRn register equal to 0:0:0. This disables the digital&amp;nbsp;&lt;/EM&gt;&lt;EM&gt;input path to the MCU.&lt;/EM&gt;&lt;/P&gt;
&lt;P&gt;This refer to chapter&amp;nbsp;&lt;STRONG&gt;12.6.1 Pin Control Register n (PORTx_PCRn)&amp;nbsp;&lt;/STRONG&gt;from your reference manual. On this register you select the alternative for the pin you want to use. f.e.&amp;nbsp; CAN0_TX pin is assigned to&amp;nbsp;PTA12 as Alternative 2 (ALT2) and by setting MUX pins as 0:0:0 this will be disabled.&lt;/P&gt;
&lt;P&gt;Best Regards, Miguel.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 12 Jul 2023 18:52:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Unused-pins-of-KS22-Microcontroller/m-p/1686838#M65287</guid>
      <dc:creator>Miguel04</dc:creator>
      <dc:date>2023-07-12T18:52:14Z</dc:date>
    </item>
    <item>
      <title>Re: Unused pins of KS22 Microcontroller</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Unused-pins-of-KS22-Microcontroller/m-p/1687103#M65288</link>
      <description>Hi Miguel&lt;BR /&gt;Here only mentioned about the GPIO Pins, And I have doubt regarding the connection of CMP pins and DAC pins.And also about the JTAG connection</description>
      <pubDate>Thu, 13 Jul 2023 05:15:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Unused-pins-of-KS22-Microcontroller/m-p/1687103#M65288</guid>
      <dc:creator>vishnuvariyath_2</dc:creator>
      <dc:date>2023-07-13T05:15:40Z</dc:date>
    </item>
  </channel>
</rss>