<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: FlexCAN messaging on KEAZ64 Board in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/FlexCAN-messaging-on-KEAZ64-Board/m-p/1682163#M65249</link>
    <description>&lt;P&gt;&lt;SPAN&gt;Hi Raul, thank you for the support. Is there any sample code for MSCAN that is able to show it sending and receiving multiple CAN messages? I can only find the Test_Case code for the driver that allows for either 1 message to be sent or 1 message to be received. Any sample code to polling for messages and the sending of multiple messages would be highly appreciated.&lt;/SPAN&gt;&lt;/P&gt;</description>
    <pubDate>Wed, 05 Jul 2023 17:20:22 GMT</pubDate>
    <dc:creator>GarrettMJ</dc:creator>
    <dc:date>2023-07-05T17:20:22Z</dc:date>
    <item>
      <title>FlexCAN messaging on KEAZ64 Board</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/FlexCAN-messaging-on-KEAZ64-Board/m-p/1681392#M65246</link>
      <description>&lt;P&gt;I am wondering if there is a way to get FlexCAN working on the a KEAZ64 board as I am trying to port over some J1939 CAN code that is setup for a FlexCAN module to a KEAZ board. I am unfortunately not able to get this to work and can't find anything saying this is even possible. Any advice would be extremely helpful.&lt;/P&gt;</description>
      <pubDate>Tue, 04 Jul 2023 16:54:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/FlexCAN-messaging-on-KEAZ64-Board/m-p/1681392#M65246</guid>
      <dc:creator>GarrettMJ</dc:creator>
      <dc:date>2023-07-04T16:54:02Z</dc:date>
    </item>
    <item>
      <title>Re: FlexCAN messaging on KEAZ64 Board</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/FlexCAN-messaging-on-KEAZ64-Board/m-p/1681442#M65247</link>
      <description>&lt;P class="lia-align-justify"&gt;Hello &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/217136"&gt;@GarrettMJ&lt;/a&gt;,&lt;/P&gt;
&lt;P class="lia-align-justify"&gt;Unfortunately, there is not an example about the KEAZ64 board and compatibility with J1939. Nevertheless, it could be useful to take a look to the following information:&lt;/P&gt;
&lt;UL class="lia-align-justify" type="disc"&gt;
&lt;LI&gt;&lt;A href="https://community.nxp.com/t5/Kinetis-Microcontrollers/CAN-2-0-vs-SAE-J1939/m-p/619469" target="_blank"&gt;CAN 2.0 vs SAE J1939 - NXP Community&lt;/A&gt;&lt;/LI&gt;
&lt;LI&gt;&lt;A href="https://community.nxp.com/t5/S32-Design-Studio/S32-KEAZ-SDK-PEX-MSCAN-Missing-Help/m-p/660826" target="_blank"&gt;S32 KEAZ-SDK &amp;amp; PEX, MSCAN Missing --Help! - NXP Community&lt;/A&gt;&lt;/LI&gt;
&lt;LI&gt;&lt;A href="http://Hello%20__name__,  Unfortunately, there is not an example for the KEAZ64 board to work with J1939. Nevertheless, it could be useful to take a look to the following information: 	• CAN 2.0 vs SAE J1939 - NXP Community 	• S32 KEAZ-SDK &amp;amp; PEX, MSCAN Missing --Help! - NXP Community 	• KEA General Purpose Evaluation Board | NXP Semiconductors 	• KEA128 Sub-Family Reference Manual. Chapter 32 Freescale's Scalable Controller Area Network (MSCAN).  Best regards, Raul." target="_self"&gt;KEA128 Sub-Family Reference Manual. Chapter 32 Freescale's Scalable Controller Area Network (MSCAN).&lt;/A&gt;&lt;/LI&gt;
&lt;LI&gt;&lt;A href="https://www.nxp.com/design/development-boards/automotive-development-platforms/s32k-mcu-platforms/kea-general-purpose-evaluation-board:FRDM-KEAZ128" target="_blank"&gt;KEA General Purpose Evaluation Board | NXP Semiconductors&lt;/A&gt;, you could download the MSCAN driver here which could be helpful.&lt;/LI&gt;
&lt;/UL&gt;
&lt;P class="lia-align-justify"&gt;Best regards, Raul.&lt;/P&gt;</description>
      <pubDate>Tue, 04 Jul 2023 20:54:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/FlexCAN-messaging-on-KEAZ64-Board/m-p/1681442#M65247</guid>
      <dc:creator>RaRo</dc:creator>
      <dc:date>2023-07-04T20:54:28Z</dc:date>
    </item>
    <item>
      <title>Re: FlexCAN messaging on KEAZ64 Board</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/FlexCAN-messaging-on-KEAZ64-Board/m-p/1682163#M65249</link>
      <description>&lt;P&gt;&lt;SPAN&gt;Hi Raul, thank you for the support. Is there any sample code for MSCAN that is able to show it sending and receiving multiple CAN messages? I can only find the Test_Case code for the driver that allows for either 1 message to be sent or 1 message to be received. Any sample code to polling for messages and the sending of multiple messages would be highly appreciated.&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Wed, 05 Jul 2023 17:20:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/FlexCAN-messaging-on-KEAZ64-Board/m-p/1682163#M65249</guid>
      <dc:creator>GarrettMJ</dc:creator>
      <dc:date>2023-07-05T17:20:22Z</dc:date>
    </item>
    <item>
      <title>Re: FlexCAN messaging on KEAZ64 Board</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/FlexCAN-messaging-on-KEAZ64-Board/m-p/1684122#M65268</link>
      <description>&lt;P class="lia-align-justify"&gt;Hello &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/217136"&gt;@GarrettMJ&lt;/a&gt;,&lt;/P&gt;
&lt;P class="lia-align-justify"&gt;Sadly, the only example of KEA's MSCAN is the Test_Case you mention. Nonetheless, might be helpful to check the following information:&lt;/P&gt;
&lt;UL class="lia-align-justify" type="disc"&gt;
&lt;LI&gt;&lt;A href="https://www.nxp.com/docs/en/application-note/AN12355.pdf" target="_blank"&gt;Using MSCAN on KE16Z MCU&lt;/A&gt;&lt;/LI&gt;
&lt;LI&gt;&lt;A href="https://community.nxp.com/t5/Kinetis-Microcontrollers/regarding-CAN-Tx-and-Rx-in-KEA128/m-p/432535" target="_blank"&gt;regarding CAN Tx and Rx in KEA128 - NXP Community&lt;/A&gt;&lt;/LI&gt;
&lt;LI&gt;&lt;A href="https://community.nxp.com/t5/MCUXpresso-IDE/Questions-about-sending-and-receiving-multiple-CAN-messages/m-p/970346" target="_blank"&gt;Questions about sending and receiving multiple CAN... - NXP Community&lt;/A&gt;&lt;/LI&gt;
&lt;LI&gt;&lt;A href="https://www.nxp.com/docs/en/application-note/AN2283.pdf" target="_blank"&gt;AN2283/D: Motorola Scalable Controller Area Network (MSCAN) Interrupts&lt;/A&gt;&lt;/LI&gt;
&lt;/UL&gt;
&lt;P class="lia-align-justify"&gt;Sorry for any inconvenient this may cause you.&lt;/P&gt;
&lt;P class="lia-align-justify"&gt;Best regards, Raul.&lt;/P&gt;</description>
      <pubDate>Fri, 07 Jul 2023 21:24:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/FlexCAN-messaging-on-KEAZ64-Board/m-p/1684122#M65268</guid>
      <dc:creator>RaRo</dc:creator>
      <dc:date>2023-07-07T21:24:14Z</dc:date>
    </item>
  </channel>
</rss>