<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックRe: MKM34 and MKM35 code compaitbility, one code for both controllers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/MKM34-and-MKM35-code-compaitbility-one-code-for-both-controllers/m-p/1675096#M65217</link>
    <description>&lt;P class="lia-align-justify"&gt;Hello &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/219291"&gt;@Chris_P&lt;/a&gt;,&lt;/P&gt;
&lt;BLOCKQUOTE&gt;
&lt;P class="lia-align-justify"&gt;&lt;EM&gt;Is it possible to compile the code only for the MKM35 and run it on both controllers without any risk?&lt;/EM&gt;&lt;/P&gt;
&lt;/BLOCKQUOTE&gt;
&lt;P class="lia-align-justify"&gt;As you mention, both microcontrollers share some characteristics and functionalities.&lt;/P&gt;
&lt;P class="lia-align-justify"&gt;Nonetheless, you should be careful with those that are not, for example: SRAM. Specially if you intend to program or compile from MKM35Z256 to MKM34Z256.&lt;/P&gt;
&lt;P class="lia-align-justify"&gt;You could continue working as you mention, but it might be a better practice to use the corresponding microcontroller SDK.&lt;/P&gt;
&lt;P class="lia-align-justify"&gt;Best regards, Raul.&lt;/P&gt;</description>
    <pubDate>Fri, 23 Jun 2023 18:53:08 GMT</pubDate>
    <dc:creator>RaRo</dc:creator>
    <dc:date>2023-06-23T18:53:08Z</dc:date>
    <item>
      <title>MKM34 and MKM35 code compaitbility, one code for both controllers</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/MKM34-and-MKM35-code-compaitbility-one-code-for-both-controllers/m-p/1674283#M65206</link>
      <description>&lt;P&gt;Hello *,&lt;/P&gt;&lt;P&gt;I have the case that I want to replace the MKM34Z256 with the MKM35Z256 and I only use those internal modules and features that both of them have inside.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Is it possible to compile the code only for the MKM35 and run it on both controllers without any risk? (watchdog is active) I have already run code compiled for 34 on the 35 without any obvious problems...&lt;/P&gt;&lt;P&gt;As I read in the docu and migration guide there are only small additions in the MKM35, they have the same pinning, registers, adcs etc and even the SDK drivers I use in Keil are nearly the same, only minor differences.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks in advance !!&lt;/P&gt;&lt;P&gt;Christian&lt;/P&gt;</description>
      <pubDate>Thu, 22 Jun 2023 07:57:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/MKM34-and-MKM35-code-compaitbility-one-code-for-both-controllers/m-p/1674283#M65206</guid>
      <dc:creator>Chris_P</dc:creator>
      <dc:date>2023-06-22T07:57:43Z</dc:date>
    </item>
    <item>
      <title>Re: MKM34 and MKM35 code compaitbility, one code for both controllers</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/MKM34-and-MKM35-code-compaitbility-one-code-for-both-controllers/m-p/1675096#M65217</link>
      <description>&lt;P class="lia-align-justify"&gt;Hello &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/219291"&gt;@Chris_P&lt;/a&gt;,&lt;/P&gt;
&lt;BLOCKQUOTE&gt;
&lt;P class="lia-align-justify"&gt;&lt;EM&gt;Is it possible to compile the code only for the MKM35 and run it on both controllers without any risk?&lt;/EM&gt;&lt;/P&gt;
&lt;/BLOCKQUOTE&gt;
&lt;P class="lia-align-justify"&gt;As you mention, both microcontrollers share some characteristics and functionalities.&lt;/P&gt;
&lt;P class="lia-align-justify"&gt;Nonetheless, you should be careful with those that are not, for example: SRAM. Specially if you intend to program or compile from MKM35Z256 to MKM34Z256.&lt;/P&gt;
&lt;P class="lia-align-justify"&gt;You could continue working as you mention, but it might be a better practice to use the corresponding microcontroller SDK.&lt;/P&gt;
&lt;P class="lia-align-justify"&gt;Best regards, Raul.&lt;/P&gt;</description>
      <pubDate>Fri, 23 Jun 2023 18:53:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/MKM34-and-MKM35-code-compaitbility-one-code-for-both-controllers/m-p/1675096#M65217</guid>
      <dc:creator>RaRo</dc:creator>
      <dc:date>2023-06-23T18:53:08Z</dc:date>
    </item>
    <item>
      <title>Re: MKM34 and MKM35 code compaitbility, one code for both controllers</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/MKM34-and-MKM35-code-compaitbility-one-code-for-both-controllers/m-p/1675751#M65221</link>
      <description>&lt;P&gt;Hi Raul,&lt;/P&gt;&lt;P&gt;thank you for your reply and your hint regarding the SRAM, to be honest I didn't recognize the different address ranges in MKM34 and 35.&lt;/P&gt;&lt;P&gt;I will reconsider the one-compile-for-all strategy &lt;LI-EMOJI id="lia_winking-face" title=":winking_face:"&gt;&lt;/LI-EMOJI&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Christian&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 26 Jun 2023 07:28:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/MKM34-and-MKM35-code-compaitbility-one-code-for-both-controllers/m-p/1675751#M65221</guid>
      <dc:creator>Chris_P</dc:creator>
      <dc:date>2023-06-26T07:28:30Z</dc:date>
    </item>
    <item>
      <title>Re: MKM34 and MKM35 code compaitbility, one code for both controllers</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/MKM34-and-MKM35-code-compaitbility-one-code-for-both-controllers/m-p/1841795#M66262</link>
      <description>&lt;P&gt;Hi Chris_P,&lt;/P&gt;&lt;P&gt;Can you tell which compiler are you using for code?&lt;/P&gt;&lt;P&gt;If it is IAR, which version?&lt;/P&gt;&lt;P&gt;Are you able to build output file for both&amp;nbsp;&lt;SPAN&gt;MKM34Z256 and MKM35Z256 using IARv9.10.2?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;I'm facing a issue while compiling the code for&amp;nbsp;MKM34Z256 with iarv9.10.2. I think some linker issues.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;The error shown is:&lt;STRONG&gt; Fatal Error[Lp049]: there was no reference to __iar_data_init3, but it is needed to initialize section .bss (irtc.o #8) on iar v9.10&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;can you please help me if you have any idea regarding this error, I'm new in this field:(&lt;/P&gt;&lt;P&gt;Thanks and regards&lt;/P&gt;</description>
      <pubDate>Sun, 07 Apr 2024 14:38:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/MKM34-and-MKM35-code-compaitbility-one-code-for-both-controllers/m-p/1841795#M66262</guid>
      <dc:creator>amal_s</dc:creator>
      <dc:date>2024-04-07T14:38:11Z</dc:date>
    </item>
  </channel>
</rss>