<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Clock deviation in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Clock-deviation/m-p/1664596#M65149</link>
    <description>&lt;P&gt;Hi, anybody knows what is&amp;nbsp;IRC48 sensitivity to the MCU rail voltage VCC?&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Tue, 06 Jun 2023 20:23:58 GMT</pubDate>
    <dc:creator>marktverskoy</dc:creator>
    <dc:date>2023-06-06T20:23:58Z</dc:date>
    <item>
      <title>Clock deviation</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Clock-deviation/m-p/980051#M55437</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;BLOCKQUOTE class="jive_macro_quote jive-quote jive_text_macro"&gt;&lt;P&gt;Hi NXP community,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I had a few questions regarding the clock deviation using the 48MIRC on the K24.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Firstly, I understand the from the datasheet that the open loop deviation from 0 to 85 degress is 1%.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/101121iBD29349F6F260BD7/image-size/large?v=v2&amp;amp;px=999" title="48MIRC deviation.PNG" alt="48MIRC deviation.PNG" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Q1. Is it correct to assume that the clock will deviate around 1% (approx. +/- 480000 clocks) between 0 to 85 degrees? Is there some kind of temperature distribution chart for the deviation?&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Q2. How will this clock deviation trickle down to the other clocks, bus clock and flash clock? We want to calculate&amp;nbsp; effect of clock deviation of each peripheral i.e., SPI, I2C, ADC and UART and in turn compare it with the tolerance given in the datasheet for these peripherals.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Any input will be very much appreciated.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you&lt;/P&gt;&lt;P&gt;Sachin&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 18 Feb 2020 09:26:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Clock-deviation/m-p/980051#M55437</guid>
      <dc:creator>smathad</dc:creator>
      <dc:date>2020-02-18T09:26:31Z</dc:date>
    </item>
    <item>
      <title>Re: Clock deviation</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Clock-deviation/m-p/980052#M55438</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Sachin,&lt;/P&gt;&lt;P&gt;1. yes,&amp;nbsp;clock will deviate around 1% (approx. +/- 480000 clocks) between 0 to 85 degrees. But there is no such a chart.&lt;/P&gt;&lt;P&gt;2. If you use IRC48 as system clock source, of course it will trickle down to whole system. The deviation is proportional.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Jing&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 19 Feb 2020 09:26:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Clock-deviation/m-p/980052#M55438</guid>
      <dc:creator>jingpan</dc:creator>
      <dc:date>2020-02-19T09:26:33Z</dc:date>
    </item>
    <item>
      <title>Re: Clock deviation</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Clock-deviation/m-p/1664596#M65149</link>
      <description>&lt;P&gt;Hi, anybody knows what is&amp;nbsp;IRC48 sensitivity to the MCU rail voltage VCC?&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 06 Jun 2023 20:23:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Clock-deviation/m-p/1664596#M65149</guid>
      <dc:creator>marktverskoy</dc:creator>
      <dc:date>2023-06-06T20:23:58Z</dc:date>
    </item>
  </channel>
</rss>