<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックKL82 VLLS low power modes</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL82-VLLS-low-power-modes/m-p/1658519#M65117</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I am trying to use VLLS mode 1 to implement a low power wakeup.&amp;nbsp; For my wakeup sources, I am using an input pin, and the LPTMR0 set for 15 seconds.&amp;nbsp; The device goes to sleep, and if I toggle the input pin, the device wakes up just fine, and eventually goes back to sleep.&amp;nbsp; If I wait 15s for the LPTMR0 to expire, the device wakes up (I can see a jump in current consumption) but the device is in an unknown state, and can only be restarted by cycling power.&lt;/P&gt;&lt;P&gt;Am I correct in assuming that the VLLS1 can support wake up on pin, and wake up on module together?&amp;nbsp; The provided example in the SDK(power mode switch) will only do one or the other.&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have modelled my code like the SDK example, except I have enabled 2 wakeup sources as mentioned above.&lt;/P&gt;&lt;P&gt;Any insight on this would be appreciated.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Fri, 26 May 2023 15:39:48 GMT</pubDate>
    <dc:creator>morrison232</dc:creator>
    <dc:date>2023-05-26T15:39:48Z</dc:date>
    <item>
      <title>KL82 VLLS low power modes</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL82-VLLS-low-power-modes/m-p/1658519#M65117</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I am trying to use VLLS mode 1 to implement a low power wakeup.&amp;nbsp; For my wakeup sources, I am using an input pin, and the LPTMR0 set for 15 seconds.&amp;nbsp; The device goes to sleep, and if I toggle the input pin, the device wakes up just fine, and eventually goes back to sleep.&amp;nbsp; If I wait 15s for the LPTMR0 to expire, the device wakes up (I can see a jump in current consumption) but the device is in an unknown state, and can only be restarted by cycling power.&lt;/P&gt;&lt;P&gt;Am I correct in assuming that the VLLS1 can support wake up on pin, and wake up on module together?&amp;nbsp; The provided example in the SDK(power mode switch) will only do one or the other.&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have modelled my code like the SDK example, except I have enabled 2 wakeup sources as mentioned above.&lt;/P&gt;&lt;P&gt;Any insight on this would be appreciated.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 26 May 2023 15:39:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL82-VLLS-low-power-modes/m-p/1658519#M65117</guid>
      <dc:creator>morrison232</dc:creator>
      <dc:date>2023-05-26T15:39:48Z</dc:date>
    </item>
  </channel>
</rss>