<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic MK80F25615 flash configuration, FSEC in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/MK80F25615-flash-configuration-FSEC/m-p/1657747#M65110</link>
    <description>&lt;P&gt;Would like to enable basic protection against cloning for an MK80F25615 CPU, so that it can be programmed or mass erased, but not read back. Development environment is MCUxpresso IDE.&lt;/P&gt;&lt;P&gt;From the information online it looks like this line in the startup_mk80f25615.c (created by the SDK) controls the flash configuration for these processors:&lt;/P&gt;&lt;P&gt;} Flash_Config = {0xFFFFFFFF, 0xFFFFFFFF, 0xFFFFFFFF, 0xFFFF3DFE};&lt;/P&gt;&lt;P&gt;However, I can't find any documentation describing where the FSEC bits appear in these values for this CPU. It doesn't appear to be in the CPU reference manual anywhere.&lt;/P&gt;&lt;P&gt;Would appreciate any help in finding where these bits are documented, or a better way to set up this feature in the IDE if there is one.&lt;/P&gt;</description>
    <pubDate>Thu, 25 May 2023 14:36:58 GMT</pubDate>
    <dc:creator>Anon00001</dc:creator>
    <dc:date>2023-05-25T14:36:58Z</dc:date>
    <item>
      <title>MK80F25615 flash configuration, FSEC</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/MK80F25615-flash-configuration-FSEC/m-p/1657747#M65110</link>
      <description>&lt;P&gt;Would like to enable basic protection against cloning for an MK80F25615 CPU, so that it can be programmed or mass erased, but not read back. Development environment is MCUxpresso IDE.&lt;/P&gt;&lt;P&gt;From the information online it looks like this line in the startup_mk80f25615.c (created by the SDK) controls the flash configuration for these processors:&lt;/P&gt;&lt;P&gt;} Flash_Config = {0xFFFFFFFF, 0xFFFFFFFF, 0xFFFFFFFF, 0xFFFF3DFE};&lt;/P&gt;&lt;P&gt;However, I can't find any documentation describing where the FSEC bits appear in these values for this CPU. It doesn't appear to be in the CPU reference manual anywhere.&lt;/P&gt;&lt;P&gt;Would appreciate any help in finding where these bits are documented, or a better way to set up this feature in the IDE if there is one.&lt;/P&gt;</description>
      <pubDate>Thu, 25 May 2023 14:36:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/MK80F25615-flash-configuration-FSEC/m-p/1657747#M65110</guid>
      <dc:creator>Anon00001</dc:creator>
      <dc:date>2023-05-25T14:36:58Z</dc:date>
    </item>
    <item>
      <title>Re: MK80F25615 flash configuration, FSEC</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/MK80F25615-flash-configuration-FSEC/m-p/1657866#M65112</link>
      <description>&lt;P&gt;Hello, my name is Pavel and I will be supporting your case, I found this information in the RM chapter&amp;nbsp;34.3.4.3 Flash Security Register (FTFA_FSEC), maybe that information that what you wanted.&lt;/P&gt;
&lt;P&gt;And the app note has more details about this register.&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com/docs/en/application-note/AN4835.pdf" target="_blank"&gt;Production Flash programming best practices for Kinetis K and L MCUs (nxp.com)&lt;/A&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Let me know if you have more doubts.&lt;/P&gt;
&lt;P&gt;Best regards,&lt;BR /&gt;Pavel&lt;/P&gt;</description>
      <pubDate>Thu, 25 May 2023 17:57:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/MK80F25615-flash-configuration-FSEC/m-p/1657866#M65112</guid>
      <dc:creator>Pavel_Hernandez</dc:creator>
      <dc:date>2023-05-25T17:57:41Z</dc:date>
    </item>
    <item>
      <title>Re: MK80F25615 flash configuration, FSEC</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/MK80F25615-flash-configuration-FSEC/m-p/1657874#M65113</link>
      <description>For the benefit of anyone reading this later, the relevant RM document number is:&lt;BR /&gt;K80P121M150SF5RM&lt;BR /&gt;In Rev. 4, 09/2015, the relevant page numbers are 803 and 811.&lt;BR /&gt;The 'SEC' field appears to be in the last two bits of the last byte, with default bit value b10 representing 'unsecured' and anything else representing 'secured'.</description>
      <pubDate>Thu, 25 May 2023 18:27:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/MK80F25615-flash-configuration-FSEC/m-p/1657874#M65113</guid>
      <dc:creator>Anon00001</dc:creator>
      <dc:date>2023-05-25T18:27:34Z</dc:date>
    </item>
  </channel>
</rss>