<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Microcontrollers中的主题 Re: KM35Z512 Three-Phase Power Meter</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KM35Z512-Three-Phase-Power-Meter/m-p/1653352#M65074</link>
    <description>&lt;P&gt;OK, I found that if you import the project, you can find the files.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Sorry.&lt;/P&gt;</description>
    <pubDate>Thu, 18 May 2023 22:13:43 GMT</pubDate>
    <dc:creator>dporada</dc:creator>
    <dc:date>2023-05-18T22:13:43Z</dc:date>
    <item>
      <title>KM35Z512 Three-Phase Power Meter</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KM35Z512-Three-Phase-Power-Meter/m-p/1193781#M59026</link>
      <description>&lt;P&gt;I am using TWR-KM35Z75M and working on building a 3-Phase Power Meter.&amp;nbsp;&lt;/P&gt;&lt;P&gt;When I looked all&amp;nbsp; Application Notes I just found&amp;nbsp;AN12837 (KM35Z512 based One-Phase Smart Power Meter Reference Design) as an example for KM35 series but I couldn't find 3-Phase Application Note.Also, I couldn't find the application software based on AN12837, which mentions about using&amp;nbsp;MKM35Z512 bare-metal software drivers but it seems MKM34Z256 bare metal software drivers (5. Referance of AN12837). The&amp;nbsp;MKM34Z256 bare metal software drivers is too old, is there any new bare metal software drivers?&lt;/P&gt;&lt;P&gt;Moreover, I couldn't understand that voltage signals are connected to 3 comparator channels (0, 2 and 5) but in their application software just 1 comparator channel is initialized&amp;nbsp;in the DRM162 and DRM147. And application softwares are using Filter-Based Algorithm, is there any 3-Phase power meter application software using FFT-Based Algorithm?&lt;/P&gt;&lt;P&gt;Thanks in advance.&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Mehmet.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 04 Dec 2020 08:12:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KM35Z512-Three-Phase-Power-Meter/m-p/1193781#M59026</guid>
      <dc:creator>MehmetKirgozoglu</dc:creator>
      <dc:date>2020-12-04T08:12:00Z</dc:date>
    </item>
    <item>
      <title>Re: KM35Z512 Three-Phase Power Meter</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KM35Z512-Three-Phase-Power-Meter/m-p/1196926#M59092</link>
      <description>&lt;P&gt;Hello&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;I suggest you use for reference the SDK examples. Here you can download the SDK for the TWR-KM35Z75M &lt;A href="https://mcuxpresso.nxp.com/en/welcome" target="_blank"&gt;https://mcuxpresso.nxp.com/en/welcome&lt;/A&gt;.&lt;/P&gt;
&lt;P&gt;There you can find examples of the use of the power metering library in different use cases that can be useful.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Let me know if this is helpful, if you have more questions do not hesitate to ask me.&lt;/P&gt;
&lt;P&gt;Best regards,&lt;/P&gt;
&lt;P&gt;Omar&lt;/P&gt;</description>
      <pubDate>Wed, 09 Dec 2020 21:26:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KM35Z512-Three-Phase-Power-Meter/m-p/1196926#M59092</guid>
      <dc:creator>Omar_Anguiano</dc:creator>
      <dc:date>2020-12-09T21:26:08Z</dc:date>
    </item>
    <item>
      <title>Re: KM35Z512 Three-Phase Power Meter</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KM35Z512-Three-Phase-Power-Meter/m-p/1198728#M59107</link>
      <description>&lt;P&gt;Hello Omar,&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you getting back to me. Well, there are useful metering library examples.&lt;/P&gt;&lt;P&gt;But, for the 3-Phase meter design, I couldn't see 3 comparator channels in application software where the 3 comparator channels connected to CMP0_IN0,&amp;nbsp;CMP0_IN2 and&amp;nbsp;CMP0_IN5 (DRM162). Also in my application I couldn't get any interrupt from comparator channels.&lt;/P&gt;&lt;P&gt;How should I use comparator channels (for the zero cross measurement) ?&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 14 Dec 2020 08:23:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KM35Z512-Three-Phase-Power-Meter/m-p/1198728#M59107</guid>
      <dc:creator>MehmetKirgozoglu</dc:creator>
      <dc:date>2020-12-14T08:23:04Z</dc:date>
    </item>
    <item>
      <title>Re: KM35Z512 Three-Phase Power Meter</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KM35Z512-Three-Phase-Power-Meter/m-p/1200675#M59129</link>
      <description>&lt;P&gt;Hello&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;CMP1 and CMP2 are used for zero-crossing detection. I suggest you refer to the cmp_interrupt example to integrate it into the 3-phase design.&lt;/P&gt;
&lt;P&gt;For more detailed information about the comparator, I suggest you check chapter 33 of the reference manual.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Let me know if this is helpful, if you have more questions do not hesitate to ask me.&lt;/P&gt;
&lt;P&gt;Best regards,&lt;/P&gt;
&lt;P&gt;Omar&lt;/P&gt;</description>
      <pubDate>Wed, 16 Dec 2020 20:17:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KM35Z512-Three-Phase-Power-Meter/m-p/1200675#M59129</guid>
      <dc:creator>Omar_Anguiano</dc:creator>
      <dc:date>2020-12-16T20:17:32Z</dc:date>
    </item>
    <item>
      <title>Re: KM35Z512 Three-Phase Power Meter</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KM35Z512-Three-Phase-Power-Meter/m-p/1377918#M61950</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;For 3 phase meter design with KM35Z512, you can also refer to AN13338&amp;nbsp;&lt;A href="https://www.nxp.com/docs/en/application-note/AN13338.pdf" target="_blank"&gt;https://www.nxp.com/docs/en/application-note/AN13338.pdf&lt;/A&gt;&amp;nbsp;and can find HW, SW details from&amp;nbsp;&lt;A href="https://www.nxp.com/products/processors-and-microcontrollers/arm-microcontrollers/general-purpose-mcus/km-series-cortex-m0-plus/5075-mhz-precision-metrology-mcus-with-segment-lcds-based-on-arm-cortex-m0-plus:KM3x?tab=Documentation_Tab" target="_blank"&gt;https://www.nxp.com/products/processors-and-microcontrollers/arm-microcontrollers/general-purpose-mcus/km-series-cortex-m0-plus/5075-mhz-precision-metrology-mcus-with-segment-lcds-based-on-arm-cortex-m0-plus:KM3x?tab=Documentation_Tab&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Biswanath&lt;/P&gt;</description>
      <pubDate>Mon, 29 Nov 2021 05:26:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KM35Z512-Three-Phase-Power-Meter/m-p/1377918#M61950</guid>
      <dc:creator>biswanath_bhowmick</dc:creator>
      <dc:date>2021-11-29T05:26:02Z</dc:date>
    </item>
    <item>
      <title>Re: KM35Z512 Three-Phase Power Meter</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KM35Z512-Three-Phase-Power-Meter/m-p/1652436#M65070</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I an also looking at AN13338 and I have downloaded the associated files&lt;SPAN class=""&gt;&amp;nbsp;AN13338SW.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;&lt;SPAN&gt;I am unable to open any code files for MCUXpresso. &amp;nbsp;I was able to open them for IAR, but I am only running a demo version. &amp;nbsp;How do I open the MCUXpresso files?&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 17 May 2023 20:06:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KM35Z512-Three-Phase-Power-Meter/m-p/1652436#M65070</guid>
      <dc:creator>dporada</dc:creator>
      <dc:date>2023-05-17T20:06:31Z</dc:date>
    </item>
    <item>
      <title>Re: KM35Z512 Three-Phase Power Meter</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KM35Z512-Three-Phase-Power-Meter/m-p/1653352#M65074</link>
      <description>&lt;P&gt;OK, I found that if you import the project, you can find the files.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Sorry.&lt;/P&gt;</description>
      <pubDate>Thu, 18 May 2023 22:13:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KM35Z512-Three-Phase-Power-Meter/m-p/1653352#M65074</guid>
      <dc:creator>dporada</dc:creator>
      <dc:date>2023-05-18T22:13:43Z</dc:date>
    </item>
    <item>
      <title>Re: KM35Z512 Three-Phase Power Meter</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KM35Z512-Three-Phase-Power-Meter/m-p/1673669#M65203</link>
      <description>&lt;P&gt;I have a question about AN13338SW. &amp;nbsp;I want to build the project km3x_3phase_meter_release. &amp;nbsp;When I import the files into MCUXpresso, I am unable to build the project. &amp;nbsp;It says that some of the files cannot be found. &amp;nbsp;I an unable to find them either. &amp;nbsp;Do you know how to fix this?&lt;/P&gt;</description>
      <pubDate>Wed, 21 Jun 2023 13:09:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KM35Z512-Three-Phase-Power-Meter/m-p/1673669#M65203</guid>
      <dc:creator>dporada</dc:creator>
      <dc:date>2023-06-21T13:09:18Z</dc:date>
    </item>
    <item>
      <title>Re: KM35Z512 Three-Phase Power Meter</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KM35Z512-Three-Phase-Power-Meter/m-p/1674180#M65205</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/43007"&gt;@dporada&lt;/a&gt;,&lt;/P&gt;&lt;P&gt;I am seeing the issue at my end. Instead of importing the archive .zip file, if you first unzip to to a folder and do "Import-&amp;gt;Existing Projects into Workspace-&amp;gt;Select root directory" and chose the unzipped folder and select the project(s) you want to build, does not get issues while building.&lt;/P&gt;&lt;P&gt;Let me know if this solved your issue.&lt;/P&gt;&lt;P&gt;The problem with archive import has been noted.&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Biswanath&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 22 Jun 2023 04:52:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KM35Z512-Three-Phase-Power-Meter/m-p/1674180#M65205</guid>
      <dc:creator>biswanath_bhowmick</dc:creator>
      <dc:date>2023-06-22T04:52:02Z</dc:date>
    </item>
    <item>
      <title>Re: KM35Z512 Three-Phase Power Meter</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KM35Z512-Three-Phase-Power-Meter/m-p/1675075#M65216</link>
      <description>&lt;P&gt;&lt;SPAN&gt;Biswanath,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thank you for your fast response.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;That kind of worked. &amp;nbsp;It still doesn’t work on the Macintosh version, but it worked on a windows version of MCUXpresso.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;On the Mac version I get the same errors. &amp;nbsp;I’m assuming that you were trying to run it on a windows machine?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Don&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Fri, 23 Jun 2023 17:40:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KM35Z512-Three-Phase-Power-Meter/m-p/1675075#M65216</guid>
      <dc:creator>dporada</dc:creator>
      <dc:date>2023-06-23T17:40:45Z</dc:date>
    </item>
  </channel>
</rss>