<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Can I use Cyclone Pro as a debugger for K60 tower? in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Can-I-use-Cyclone-Pro-as-a-debugger-for-K60-tower/m-p/147806#M65</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The Tower boards have an integrated OSJTAG debugger on the processor boards. This means that no external debugger is required.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;There is also a standard Cortex debug + ETM connector which can be used by external debuggers which conform to this standard. The Cyclone Pro from P+E doesn't support ARM processors as far as I know (only HC08 HCS08, HC(S)12 and Coldfire+/V1).&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Mark&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sat, 09 Jul 2011 16:20:11 GMT</pubDate>
    <dc:creator>mjbcswitzerland</dc:creator>
    <dc:date>2011-07-09T16:20:11Z</dc:date>
    <item>
      <title>Can I use Cyclone Pro as a debugger for K60 tower?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Can-I-use-Cyclone-Pro-as-a-debugger-for-K60-tower/m-p/147805#M64</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I would like to order K60 tower. &amp;nbsp;We have Cyclone Pro. Can I use it on tower for debugging with CW? Or Do I have to order BDM pod?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 09 Jul 2011 05:02:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Can-I-use-Cyclone-Pro-as-a-debugger-for-K60-tower/m-p/147805#M64</guid>
      <dc:creator>BasePointer</dc:creator>
      <dc:date>2011-07-09T05:02:16Z</dc:date>
    </item>
    <item>
      <title>Re: Can I use Cyclone Pro as a debugger for K60 tower?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Can-I-use-Cyclone-Pro-as-a-debugger-for-K60-tower/m-p/147806#M65</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The Tower boards have an integrated OSJTAG debugger on the processor boards. This means that no external debugger is required.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;There is also a standard Cortex debug + ETM connector which can be used by external debuggers which conform to this standard. The Cyclone Pro from P+E doesn't support ARM processors as far as I know (only HC08 HCS08, HC(S)12 and Coldfire+/V1).&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Mark&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 09 Jul 2011 16:20:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Can-I-use-Cyclone-Pro-as-a-debugger-for-K60-tower/m-p/147806#M65</guid>
      <dc:creator>mjbcswitzerland</dc:creator>
      <dc:date>2011-07-09T16:20:11Z</dc:date>
    </item>
    <item>
      <title>Re: Can I use Cyclone Pro as a debugger for K60 tower?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Can-I-use-Cyclone-Pro-as-a-debugger-for-K60-tower/m-p/147807#M66</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Yes you are right, we need Cyclone MAX instead of Pro.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 10 Jul 2011 00:56:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Can-I-use-Cyclone-Pro-as-a-debugger-for-K60-tower/m-p/147807#M66</guid>
      <dc:creator>BasePointer</dc:creator>
      <dc:date>2011-07-10T00:56:21Z</dc:date>
    </item>
  </channel>
</rss>