<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックRe: OpenSDAV2 MCU K20DX128Vxx5 not booting: mbed problem</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/OpenSDAV2-MCU-K20DX128Vxx5-not-booting-mbed-problem/m-p/1627172#M64918</link>
    <description>&lt;P&gt;You can update the bootloader on the board, (&lt;A href="https://www.nxp.com/webapp/Download?colCode=NXP_KINETIS_BOOTLOADER_2_0_0&amp;amp;appType=license" target="_blank"&gt;https://www.nxp.com/webapp/Download?colCode=NXP_KINETIS_BOOTLOADER_2_0_0&amp;amp;appType=license&lt;/A&gt;)&lt;/P&gt;</description>
    <pubDate>Tue, 04 Apr 2023 01:17:58 GMT</pubDate>
    <dc:creator>CarlosGarabito</dc:creator>
    <dc:date>2023-04-04T01:17:58Z</dc:date>
    <item>
      <title>OpenSDAV2 MCU K20DX128Vxx5 not booting: mbed problem</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/OpenSDAV2-MCU-K20DX128Vxx5-not-booting-mbed-problem/m-p/1626712#M64911</link>
      <description>&lt;P&gt;HI,&lt;/P&gt;&lt;P&gt;When plugging in the TWRK65F180M board, the MCU does not turn on. Only when I press the reset button does the D3 LCD start flashing. My computer then recognizes it as a device, pulls out the cperacceirosca vi olo ma po 10 seconds until the computer no longer recognizes it as a device The LCD of the D3 keeps flashing even though the MCU is not recognized by the computer.&lt;/P&gt;&lt;P&gt;To fix this, try these steps:&lt;/P&gt;&lt;P&gt;- Press and hold the RESET button (SW1).&lt;/P&gt;&lt;P&gt;- Connect the mini-USB port (J7) to power the board which should be numbered as a BOOTLOADER volume.&lt;/P&gt;&lt;P&gt;- Drag and drop the attached J-Link binary.&lt;/P&gt;&lt;P&gt;-Disconnect and connect the USB cable.&lt;/P&gt;&lt;P&gt;Then LEDs D3 and D5 light up but an MBED window opens and the MiniUSB port is not recognised. What can I do to fix the problem? Do I have to copy inside some specific file??&lt;/P&gt;</description>
      <pubDate>Mon, 03 Apr 2023 08:47:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/OpenSDAV2-MCU-K20DX128Vxx5-not-booting-mbed-problem/m-p/1626712#M64911</guid>
      <dc:creator>matteocrulli92</dc:creator>
      <dc:date>2023-04-03T08:47:20Z</dc:date>
    </item>
    <item>
      <title>Re: OpenSDAV2 MCU K20DX128Vxx5 not booting: mbed problem</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/OpenSDAV2-MCU-K20DX128Vxx5-not-booting-mbed-problem/m-p/1627171#M64917</link>
      <description>&lt;P style="margin: 0in; font-family: Montserrat; font-size: 12.0pt;" lang="es-MX"&gt;You can update the bootloader on the board, (&lt;A href="https://www.nxp.com/webapp/Download?colCode=NXP_KINETIS_BOOTLOADER_2_0_0&amp;amp;appType=license" target="_blank"&gt;https://www.nxp.com/webapp/Download?colCode=NXP_KINETIS_BOOTLOADER_2_0_0&amp;amp;appType=license&lt;/A&gt;)&lt;/P&gt;</description>
      <pubDate>Tue, 04 Apr 2023 01:17:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/OpenSDAV2-MCU-K20DX128Vxx5-not-booting-mbed-problem/m-p/1627171#M64917</guid>
      <dc:creator>CarlosGarabito</dc:creator>
      <dc:date>2023-04-04T01:17:49Z</dc:date>
    </item>
    <item>
      <title>Re: OpenSDAV2 MCU K20DX128Vxx5 not booting: mbed problem</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/OpenSDAV2-MCU-K20DX128Vxx5-not-booting-mbed-problem/m-p/1627172#M64918</link>
      <description>&lt;P&gt;You can update the bootloader on the board, (&lt;A href="https://www.nxp.com/webapp/Download?colCode=NXP_KINETIS_BOOTLOADER_2_0_0&amp;amp;appType=license" target="_blank"&gt;https://www.nxp.com/webapp/Download?colCode=NXP_KINETIS_BOOTLOADER_2_0_0&amp;amp;appType=license&lt;/A&gt;)&lt;/P&gt;</description>
      <pubDate>Tue, 04 Apr 2023 01:17:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/OpenSDAV2-MCU-K20DX128Vxx5-not-booting-mbed-problem/m-p/1627172#M64918</guid>
      <dc:creator>CarlosGarabito</dc:creator>
      <dc:date>2023-04-04T01:17:58Z</dc:date>
    </item>
  </channel>
</rss>