<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Microcontrollers中的主题 Problem flashing k24 jlink</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Problem-flashing-k24-jlink/m-p/1626827#M64913</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I'm trying to flash a k24 using the jlink segger tool. I execute the next commands, and after the loadbin I check if the image has been written correctly with verifybin and I get the error you see at the end. The verify is failing at 0x40C0 address. Do someone know why is this? Am I using the correct address? If I use 0x5000 the verify works ok but the program is not starting neither.&lt;/P&gt;&lt;P&gt;Thank you,&lt;/P&gt;&lt;LI-CODE lang="markup"&gt;J-Link&amp;gt;unlock kinetis
Found SWD-DP with ID 0x2BA01477
Unlocking device...O.K.
J-Link&amp;gt;speed 12000
Selecting 12000 kHz as target interface speed
J-Link&amp;gt;device MK24FN1M0xxx12
Disconnecting from J-Link...O.K.
Device "MK24FN1M0XXX12" selected.


Connecting to target via SWD
InitTarget()
Found SW-DP with ID 0x2BA01477
AP map detection skipped. Manually configured AP map found.
AP[0]: AHB-AP (IDR: Not set)
AP[0]: Core found
AP[0]: AHB-AP ROM base: 0xE00FF000
CPUID register: 0x410FC241. Implementer code: 0x41 (ARM)
Found Cortex-M4 r0p1, Little endian.
FPUnit: 6 code (BP) slots and 2 literal slots
CoreSight components:
ROMTbl[0] @ E00FF000
ROMTbl[0][0]: E000E000, CID: B105E00D, PID: 000BB00C SCS-M7
ROMTbl[0][1]: E0001000, CID: B105E00D, PID: 003BB002 DWT
ROMTbl[0][2]: E0002000, CID: B105E00D, PID: 002BB003 FPB
ROMTbl[0][3]: E0000000, CID: B105E00D, PID: 003BB001 ITM
ROMTbl[0][4]: E0040000, CID: B105900D, PID: 000BB9A1 TPIU
ROMTbl[0][5]: E0041000, CID: B105900D, PID: 000BB925 ETM
ROMTbl[0][6]: E0042000, CID: B105900D, PID: 003BB907 ETB
ROMTbl[0][7]: E0043000, CID: B105900D, PID: 001BB908 CSTF
Cortex-M4 identified.
J-Link&amp;gt;jtagconf -1, -1
J-Link&amp;gt;r
Reset delay: 0 ms
Reset type NORMAL: Resets core &amp;amp; peripherals via SYSRESETREQ &amp;amp; VECTRESET bit.
Reset: Halt core after reset via DEMCR.VC_CORERESET.
Reset: Reset device via AIRCR.SYSRESETREQ.
AfterResetTarget()
J-Link&amp;gt;loadbin zl_flash_dump.raw.bin 00000000
Downloading file [zl_flash_dump.raw.bin]...
Comparing flash   [100%] Done.
Erasing flash     [100%] Done.
Programming flash [100%] Done.
Verifying flash   [100%] Done.
J-Link: Flash download: Bank 0 @ 0x00000000: 1 range affected (77824 bytes)
J-Link: Flash download: Total time needed: 1.000s (Prepare: 0.032s, Compare: 0.009s, Erase: 0.007s, Program: 0.923s, Verify: 0.005s, Restore: 0.021s)
O.K.
J-Link&amp;gt;verifybin zl_flash_dump.raw.bin 00000000
Loading binary file zl_flash_dump.raw.bin
Reading 77192 bytes data from target memory @ 0x00000000.
Verify failed @ address 0x0000040C.
Expected 7B read 7A
ERROR: Verify failed.&lt;/LI-CODE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Mon, 03 Apr 2023 11:28:40 GMT</pubDate>
    <dc:creator>inakimartinez</dc:creator>
    <dc:date>2023-04-03T11:28:40Z</dc:date>
    <item>
      <title>Problem flashing k24 jlink</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Problem-flashing-k24-jlink/m-p/1626827#M64913</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I'm trying to flash a k24 using the jlink segger tool. I execute the next commands, and after the loadbin I check if the image has been written correctly with verifybin and I get the error you see at the end. The verify is failing at 0x40C0 address. Do someone know why is this? Am I using the correct address? If I use 0x5000 the verify works ok but the program is not starting neither.&lt;/P&gt;&lt;P&gt;Thank you,&lt;/P&gt;&lt;LI-CODE lang="markup"&gt;J-Link&amp;gt;unlock kinetis
Found SWD-DP with ID 0x2BA01477
Unlocking device...O.K.
J-Link&amp;gt;speed 12000
Selecting 12000 kHz as target interface speed
J-Link&amp;gt;device MK24FN1M0xxx12
Disconnecting from J-Link...O.K.
Device "MK24FN1M0XXX12" selected.


Connecting to target via SWD
InitTarget()
Found SW-DP with ID 0x2BA01477
AP map detection skipped. Manually configured AP map found.
AP[0]: AHB-AP (IDR: Not set)
AP[0]: Core found
AP[0]: AHB-AP ROM base: 0xE00FF000
CPUID register: 0x410FC241. Implementer code: 0x41 (ARM)
Found Cortex-M4 r0p1, Little endian.
FPUnit: 6 code (BP) slots and 2 literal slots
CoreSight components:
ROMTbl[0] @ E00FF000
ROMTbl[0][0]: E000E000, CID: B105E00D, PID: 000BB00C SCS-M7
ROMTbl[0][1]: E0001000, CID: B105E00D, PID: 003BB002 DWT
ROMTbl[0][2]: E0002000, CID: B105E00D, PID: 002BB003 FPB
ROMTbl[0][3]: E0000000, CID: B105E00D, PID: 003BB001 ITM
ROMTbl[0][4]: E0040000, CID: B105900D, PID: 000BB9A1 TPIU
ROMTbl[0][5]: E0041000, CID: B105900D, PID: 000BB925 ETM
ROMTbl[0][6]: E0042000, CID: B105900D, PID: 003BB907 ETB
ROMTbl[0][7]: E0043000, CID: B105900D, PID: 001BB908 CSTF
Cortex-M4 identified.
J-Link&amp;gt;jtagconf -1, -1
J-Link&amp;gt;r
Reset delay: 0 ms
Reset type NORMAL: Resets core &amp;amp; peripherals via SYSRESETREQ &amp;amp; VECTRESET bit.
Reset: Halt core after reset via DEMCR.VC_CORERESET.
Reset: Reset device via AIRCR.SYSRESETREQ.
AfterResetTarget()
J-Link&amp;gt;loadbin zl_flash_dump.raw.bin 00000000
Downloading file [zl_flash_dump.raw.bin]...
Comparing flash   [100%] Done.
Erasing flash     [100%] Done.
Programming flash [100%] Done.
Verifying flash   [100%] Done.
J-Link: Flash download: Bank 0 @ 0x00000000: 1 range affected (77824 bytes)
J-Link: Flash download: Total time needed: 1.000s (Prepare: 0.032s, Compare: 0.009s, Erase: 0.007s, Program: 0.923s, Verify: 0.005s, Restore: 0.021s)
O.K.
J-Link&amp;gt;verifybin zl_flash_dump.raw.bin 00000000
Loading binary file zl_flash_dump.raw.bin
Reading 77192 bytes data from target memory @ 0x00000000.
Verify failed @ address 0x0000040C.
Expected 7B read 7A
ERROR: Verify failed.&lt;/LI-CODE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 03 Apr 2023 11:28:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Problem-flashing-k24-jlink/m-p/1626827#M64913</guid>
      <dc:creator>inakimartinez</dc:creator>
      <dc:date>2023-04-03T11:28:40Z</dc:date>
    </item>
    <item>
      <title>Re: Problem flashing k24 jlink</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Problem-flashing-k24-jlink/m-p/1627275#M64923</link>
      <description>&lt;P&gt;Hello, my name is Pavel, and I will be supporting your case, I review your information, and could you tell me if you are using a custom bootloader? did you use another flash config? if yes, could you tell me about this config? did you try at first to erase all the MCU and then flash?&lt;/P&gt;&lt;P&gt;Best regards,&lt;BR /&gt;Pavel&lt;/P&gt;</description>
      <pubDate>Tue, 04 Apr 2023 04:04:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Problem-flashing-k24-jlink/m-p/1627275#M64923</guid>
      <dc:creator>Pavel_Hernandez</dc:creator>
      <dc:date>2023-04-04T04:04:36Z</dc:date>
    </item>
    <item>
      <title>Re: Problem flashing k24 jlink</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Problem-flashing-k24-jlink/m-p/1627456#M64925</link>
      <description>&lt;P&gt;Hello Pavel,&lt;/P&gt;&lt;P&gt;Yes Im using a custom bootloader.&lt;/P&gt;&lt;P&gt;I don't know what you mean by "flash config".&lt;/P&gt;&lt;P&gt;If it helps, I have tried to flash the .bin file using MCUXpresso IDE and I get the same result if I introduce a verifybin in the process.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;LI-CODE lang="markup"&gt;Executing flash operation 'Program' (Program executable into flash zl_flash_dump.raw.bin) - Tue Apr 04 09:53:26 CEST 2023
Checking MCU info...
Scanning for targets...
Executing flash action...
SEGGER J-Link Commander V7.86e (Compiled Mar 22 2023 16:27:49)
DLL version V7.86e, compiled Mar 22 2023 16:27:33
J-Link Command File read successfully.
Processing script file...
J-Link&amp;gt;ExitOnError 1
J-Link Commander will now exit on Error
J-Link&amp;gt;r
J-Link connection not established yet but required for command.
Connecting to J-Link via USB...O.K.
Firmware: J-Link V9 compiled May  7 2021 16:26:12
Hardware version: V9.30
J-Link uptime (since boot): N/A (Not supported by this model)
S/N: 59304712
License(s): GDB
VTref=3.314V
Target connection not established yet but required for command.
Device "MK24FN1M0XXX12" selected.
Connecting to target via SWD
InitTarget()
SWD selected. Executing JTAG -&amp;gt; SWD switching sequence.
Protection bytes in flash at addr. 0x400 - 0x40F indicate that readout protection is set.
For debugger connection the device needs to be unsecured.
Unsecuring will trigger a mass erase of the internal flash.
Executing default behavior previously saved in the registry.
Device will be unsecured now.
Found SW-DP with ID 0x2BA01477
DPIDR: 0x2BA01477
CoreSight SoC-400 or earlier
Scanning AP map to find all available APs
AP[2]: Stopped AP scan as end of AP map has been reached
AP[0]: AHB-AP (IDR: 0x24770011)
AP[1]: JTAG-AP (IDR: 0x001C0000)
Iterating through AP map to find AHB-AP to use
AP[0]: Core found
AP[0]: AHB-AP ROM base: 0xE00FF000
CPUID register: 0x410FC241. Implementer code: 0x41 (ARM)
Found Cortex-M4 r0p1, Little endian.
FPUnit: 6 code (BP) slots and 2 literal slots
CoreSight components:
ROMTbl[0] @ E00FF000
[0][0]: E000E000 CID B105E00D PID 000BB00C SCS-M7
[0][1]: E0001000 CID B105E00D PID 003BB002 DWT
[0][2]: E0002000 CID B105E00D PID 002BB003 FPB
[0][3]: E0000000 CID B105E00D PID 003BB001 ITM
[0][4]: E0040000 CID B105900D PID 000BB9A1 TPIU
[0][5]: E0041000 CID B105900D PID 000BB925 ETM
[0][6]: E0042000 CID B105900D PID 003BB907 ETB
[0][7]: E0043000 CID B105900D PID 001BB908 CSTF
Memory zones:
"Default" Description: Default access mode
Cortex-M4 identified.
Reset delay: 0 ms
Reset type NORMAL: Resets core &amp;amp; peripherals via SYSRESETREQ &amp;amp; VECTRESET bit.
Reset: Halt core after reset via DEMCR.VC_CORERESET.
Reset: Reset device via AIRCR.SYSRESETREQ.
AfterResetTarget()
J-Link&amp;gt;h
PC = FFFFFFFE, CycleCnt = 00000000
R0 = 00000000, R1 = 00000000, R2 = 00000000, R3 = 00000000
R4 = 00000000, R5 = 00000000, R6 = 00000000, R7 = 00000000
R8 = 00000000, R9 = 00000000, R10= 00000000, R11= 00000000
R12= 00000000
SP(R13)= FFFFFFFC, MSP= FFFFFFFC, PSP= 00000000, R14(LR) = FFFFFFFF
XPSR = 01000000: APSR = nzcvq, EPSR = 01000000, IPSR = 000 (NoException)
CFBP = 00000000, CONTROL = 00, FAULTMASK = 00, BASEPRI = 00, PRIMASK = 00
FPS0 = 00000000, FPS1 = 00000000, FPS2 = 00000000, FPS3 = 00000000
FPS4 = 00000000, FPS5 = 00000000, FPS6 = 00000000, FPS7 = 00000000
FPS8 = 00000000, FPS9 = 00000000, FPS10= 00000000, FPS11= 00000000
FPS12= 00000000, FPS13= 00000000, FPS14= 00000000, FPS15= 00000000
FPS16= 00000000, FPS17= 00000000, FPS18= 00000000, FPS19= 00000000
FPS20= 00000000, FPS21= 00000000, FPS22= 00000000, FPS23= 00000000
FPS24= 00000000, FPS25= 00000000, FPS26= 00000000, FPS27= 00000000
FPS28= 00000000, FPS29= 00000000, FPS30= 00000000, FPS31= 00000000
FPSCR= 00000000
J-Link&amp;gt;loadfile "/home/inaki/dev/zoslp/zoslp/output/current/build/libzl/zl_flash_dump.raw.bin" 0x0
'loadfile': Performing implicit reset &amp;amp; halt of MCU.
Reset: Halt core after reset via DEMCR.VC_CORERESET.
Reset: Reset device via AIRCR.SYSRESETREQ.
AfterResetTarget()
Downloading file [/home/inaki/dev/zoslp/zoslp/output/current/build/libzl/zl_flash_dump.raw.bin]...
J-Link: Flash download: Bank 0 @ 0x00000000: 1 range affected (77824 bytes)
J-Link: Flash download: Total: 3.598s (Prepare: 2.249s, Compare: 0.348s, Erase: 0.023s, Program &amp;amp; Verify: 0.942s, Restore: 0.034s)
J-Link: Flash download: Program &amp;amp; Verify speed: 80 KB/s
O.K.
J-Link&amp;gt;verifybin "/home/inaki/dev/zoslp/zoslp/output/current/build/libzl/zl_flash_dump.raw.bin" 0x0
Loading binary file /home/inaki/dev/zoslp/zoslp/output/current/build/libzl/zl_flash_dump.raw.bin
Reading 77252 bytes data from target memory @ 0x00000000.
Verify failed @ address 0x0000040C.
Expected 7B read 7A
ERROR: Verify failed.
Script processing completed.
Unable to perform operation!
Command failed with exit code 1&lt;/LI-CODE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Yes I have tried to execute an erase and the loadbin. It didn't work.&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;</description>
      <pubDate>Tue, 04 Apr 2023 07:55:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Problem-flashing-k24-jlink/m-p/1627456#M64925</guid>
      <dc:creator>inakimartinez</dc:creator>
      <dc:date>2023-04-04T07:55:42Z</dc:date>
    </item>
    <item>
      <title>Re: Problem flashing k24 jlink</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Problem-flashing-k24-jlink/m-p/1627979#M64927</link>
      <description>&lt;P&gt;Hello, I was referring to this section, about the Flash config.&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Pavel_Hernandez_0-1680655130916.png" style="width: 200px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/217780i8D5995C4ACC3A5FA/image-size/small?v=v2&amp;amp;px=200" role="button" title="Pavel_Hernandez_0-1680655130916.png" alt="Pavel_Hernandez_0-1680655130916.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;The code that you mentioned has some relation with this security section. Chapter&amp;nbsp;29.3.1 from the reference manual.&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Pavel_Hernandez_1-1680655221143.png" style="width: 200px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/217781i54FA8C6AF00AE4D8/image-size/small?v=v2&amp;amp;px=200" role="button" title="Pavel_Hernandez_1-1680655221143.png" alt="Pavel_Hernandez_1-1680655221143.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;if you are working with security this app note could help you.&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com/docs/en/application-note/AN4507.pdf" target="_blank"&gt;Using Kinetis Security and Flash Protection Features (nxp.com)&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Best regards,&lt;BR /&gt;Pavel&lt;/P&gt;</description>
      <pubDate>Wed, 05 Apr 2023 00:42:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Problem-flashing-k24-jlink/m-p/1627979#M64927</guid>
      <dc:creator>Pavel_Hernandez</dc:creator>
      <dc:date>2023-04-05T00:42:18Z</dc:date>
    </item>
  </channel>
</rss>