<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックRe: kl26z sanity check</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/kl26z-sanity-check/m-p/1626399#M64906</link>
    <description>&lt;P&gt;I tried the debug load again and it worked! Finally got the app I was wanting on there afterward, much thanks.&lt;/P&gt;</description>
    <pubDate>Sat, 01 Apr 2023 16:25:59 GMT</pubDate>
    <dc:creator>rickla</dc:creator>
    <dc:date>2023-04-01T16:25:59Z</dc:date>
    <item>
      <title>kl26z sanity check</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/kl26z-sanity-check/m-p/1626343#M64902</link>
      <description>&lt;P&gt;Got this board and am a novice (developer but not microcontrollers much) I went down the rabbit hole of windows and it stuck fast flashing got the boot loader to stop that on win 10.&lt;/P&gt;&lt;P&gt;But now I get it in bootloader mode, copy an elf file for the bubble demo, unplug, plug, and doesn't work. The file is gone but I have no idea if the file flashed, errored out or what.&lt;/P&gt;&lt;P&gt;So it may well be I built it wrong, does anyone have the binary for the bubble demo? I should just be able to copy it to the mounted drive, cycle power and it should work right?&lt;/P&gt;&lt;P&gt;I know the board is good because the demo was on it when I first powered it up and it worked. The board just stopped once I plugged into the other port.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Sat, 01 Apr 2023 03:42:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/kl26z-sanity-check/m-p/1626343#M64902</guid>
      <dc:creator>rickla</dc:creator>
      <dc:date>2023-04-01T03:42:53Z</dc:date>
    </item>
    <item>
      <title>Re: kl26z sanity check</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/kl26z-sanity-check/m-p/1626360#M64903</link>
      <description>&lt;P&gt;It seems that FRDM boards still get shipped with an outdated OpenSDA bootloader which does not work under Windows 10.&lt;/P&gt;&lt;P&gt;Copy demo a file to the 'bootloader mode' does not work, as it only accepts a debug (or bootloader) file.&lt;/P&gt;&lt;P&gt;What you need is to update the P&amp;amp;E OpenSDA bootloader on it to a newer version, capable to work with Windows 10. The ideal solution for this is to use a Windows 7 (not VM) machine, see or to deal with the registry, see &lt;A href="https://mcuoneclipse.com/2018/04/10/recovering-opensda-boards-with-windows-10/" target="_blank"&gt;https://mcuoneclipse.com/2018/04/10/recovering-opensda-boards-with-windows-10/&lt;/A&gt;&lt;/P&gt;&lt;P&gt;Then you can update the debug firmware too:&lt;/P&gt;&lt;P&gt;&lt;A href="https://mcuoneclipse.com/2014/11/01/illustrated-step-by-step-instructions-updating-the-freescale-freedom-board-firmware/" target="_blank"&gt;https://mcuoneclipse.com/2014/11/01/illustrated-step-by-step-instructions-updating-the-freescale-freedom-board-firmware/&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I hope this helps,&lt;/P&gt;&lt;P&gt;Erich&lt;/P&gt;</description>
      <pubDate>Sat, 01 Apr 2023 07:45:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/kl26z-sanity-check/m-p/1626360#M64903</guid>
      <dc:creator>ErichStyger</dc:creator>
      <dc:date>2023-04-01T07:45:38Z</dc:date>
    </item>
    <item>
      <title>Re: kl26z sanity check</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/kl26z-sanity-check/m-p/1626395#M64905</link>
      <description>&lt;P&gt;I did read this before and get it to 1.11, and debug. I don’t see the debug app showing so I’ll look at trying that again but I’m pretty I sure I did that correct.&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Sat, 01 Apr 2023 14:04:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/kl26z-sanity-check/m-p/1626395#M64905</guid>
      <dc:creator>rickla</dc:creator>
      <dc:date>2023-04-01T14:04:47Z</dc:date>
    </item>
    <item>
      <title>Re: kl26z sanity check</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/kl26z-sanity-check/m-p/1626399#M64906</link>
      <description>&lt;P&gt;I tried the debug load again and it worked! Finally got the app I was wanting on there afterward, much thanks.&lt;/P&gt;</description>
      <pubDate>Sat, 01 Apr 2023 16:25:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/kl26z-sanity-check/m-p/1626399#M64906</guid>
      <dc:creator>rickla</dc:creator>
      <dc:date>2023-04-01T16:25:59Z</dc:date>
    </item>
  </channel>
</rss>