<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Microcontrollers中的主题 Re: BLE Abstraction Layer</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/BLE-Abstraction-Layer/m-p/1624462#M64886</link>
    <description>&lt;P&gt;Hi,&amp;nbsp; &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/200888"&gt;@EduardoZamora&lt;/a&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Could you also suggest some documents to use other module like LEDs, Button and so, where developers can find a way to disable/change unwanted functionality like LED(using gLEDSupported_d). Similarly for other files as well.&lt;/P&gt;</description>
    <pubDate>Wed, 29 Mar 2023 20:45:13 GMT</pubDate>
    <dc:creator>pdnr7</dc:creator>
    <dc:date>2023-03-29T20:45:13Z</dc:date>
    <item>
      <title>BLE Abstraction Layer</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/BLE-Abstraction-Layer/m-p/1577927#M64538</link>
      <description>&lt;P&gt;What would be correct way to add BLE abstraction layer to a fresh new project and from where should be the abstraction to be downloaded from.&lt;/P&gt;</description>
      <pubDate>Thu, 05 Jan 2023 10:53:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/BLE-Abstraction-Layer/m-p/1577927#M64538</guid>
      <dc:creator>pdnr7</dc:creator>
      <dc:date>2023-01-05T10:53:06Z</dc:date>
    </item>
    <item>
      <title>Re: BLE Abstraction Layer</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/BLE-Abstraction-Layer/m-p/1578742#M64541</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/201743"&gt;@pdnr7&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;Since there are some memory and time constraints that need to be considered when developing BLE applications, I strongly recommend using any of the BLE example projects (compatible devices) from the corresponding &lt;A href="https://mcuxpresso.nxp.com/en/select" target="_blank"&gt;SDK&lt;/A&gt; as base for your application. This to avoid any memory or stack issue.&lt;/P&gt;
&lt;P&gt;Regards,&lt;BR /&gt;Eduardo.&lt;/P&gt;</description>
      <pubDate>Sat, 07 Jan 2023 01:29:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/BLE-Abstraction-Layer/m-p/1578742#M64541</guid>
      <dc:creator>EduardoZamora</dc:creator>
      <dc:date>2023-01-07T01:29:40Z</dc:date>
    </item>
    <item>
      <title>Re: BLE Abstraction Layer</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/BLE-Abstraction-Layer/m-p/1579316#M64544</link>
      <description>&lt;P&gt;&lt;SPAN class=""&gt;Hi &lt;/SPAN&gt;&lt;SPAN class=""&gt;EduardoZamora&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;Thanks for the response.&lt;/P&gt;&lt;P&gt;We are building the project on a custom board, which is mainly meant for CAN and other operations. The other part of the code is already ready.&lt;/P&gt;&lt;P&gt;If we use example code it is using debug(being used for some other operations),LED(being connected to some other pin),NVM memory which is not required in our case and we are also looking to add 2 different example projects in one code.&lt;/P&gt;&lt;P&gt;We are looking for fresh BLE stack/abstraction layer to be added into our code base.&lt;/P&gt;&lt;P&gt;Controller used: MKW36Z512.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 09 Jan 2023 12:34:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/BLE-Abstraction-Layer/m-p/1579316#M64544</guid>
      <dc:creator>pdnr7</dc:creator>
      <dc:date>2023-01-09T12:34:12Z</dc:date>
    </item>
    <item>
      <title>Re: BLE Abstraction Layer</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/BLE-Abstraction-Layer/m-p/1579564#M64549</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;I truly apologize for insisting, but please consider using an existing BLE project as base since custom implementation may cause stack issues and our support may be limited in these cases.&lt;/P&gt;
&lt;P&gt;Please, take a look at &lt;A href="https://www.nxp.com/docs/en/application-note/AN12273.pdf" target="_blank"&gt;Using MCUXpresso SDK CAN and LIN Drivers to Create a Bluetooth LE-CAN and Bluetooth LE-LIN Bridges on KW36&lt;/A&gt;. This Application Note describes how to create a new BLE project and add CAN and LIN drivers.&lt;/P&gt;
&lt;P&gt;Regards,&lt;BR /&gt;Eduardo.&lt;/P&gt;</description>
      <pubDate>Mon, 09 Jan 2023 21:32:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/BLE-Abstraction-Layer/m-p/1579564#M64549</guid>
      <dc:creator>EduardoZamora</dc:creator>
      <dc:date>2023-01-09T21:32:48Z</dc:date>
    </item>
    <item>
      <title>Re: BLE Abstraction Layer</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/BLE-Abstraction-Layer/m-p/1624462#M64886</link>
      <description>&lt;P&gt;Hi,&amp;nbsp; &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/200888"&gt;@EduardoZamora&lt;/a&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Could you also suggest some documents to use other module like LEDs, Button and so, where developers can find a way to disable/change unwanted functionality like LED(using gLEDSupported_d). Similarly for other files as well.&lt;/P&gt;</description>
      <pubDate>Wed, 29 Mar 2023 20:45:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/BLE-Abstraction-Layer/m-p/1624462#M64886</guid>
      <dc:creator>pdnr7</dc:creator>
      <dc:date>2023-03-29T20:45:13Z</dc:date>
    </item>
    <item>
      <title>Re: BLE Abstraction Layer</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/BLE-Abstraction-Layer/m-p/1625248#M64888</link>
      <description>&lt;P&gt;Also hierarchical architecture of the demo app mainly wireless uart&lt;/P&gt;</description>
      <pubDate>Thu, 30 Mar 2023 11:06:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/BLE-Abstraction-Layer/m-p/1625248#M64888</guid>
      <dc:creator>pdnr7</dc:creator>
      <dc:date>2023-03-30T11:06:04Z</dc:date>
    </item>
  </channel>
</rss>