<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Microcontrollers中的主题 Configure Flash Security</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Configure-Flash-Security/m-p/1613874#M64838</link>
    <description>&lt;P&gt;Hi All,&lt;/P&gt;&lt;P&gt;I'm working with the MK22FN1M0Axxx12, our solution is based on Bootloader + Custom Application.&lt;/P&gt;&lt;P&gt;Now, I should enable the Secure Mode and I'm able to enable it changing the definition of the&amp;nbsp;Flash_Config ( defined into the file startup_*.c ) of the Bootloader.&lt;/P&gt;&lt;P&gt;We have many device in field so I should enable the secure mode by our application, I have done the same steps changing the file startup_*.c of the Application's project but it seems that it doesn't work.&amp;nbsp;&lt;/P&gt;&lt;P&gt;So I have a doubs, is it possible enabling the secure mode from the application?&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Giampietro Pomponio&lt;/P&gt;</description>
    <pubDate>Mon, 13 Mar 2023 08:52:45 GMT</pubDate>
    <dc:creator>giampietropompo</dc:creator>
    <dc:date>2023-03-13T08:52:45Z</dc:date>
    <item>
      <title>Configure Flash Security</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Configure-Flash-Security/m-p/1613874#M64838</link>
      <description>&lt;P&gt;Hi All,&lt;/P&gt;&lt;P&gt;I'm working with the MK22FN1M0Axxx12, our solution is based on Bootloader + Custom Application.&lt;/P&gt;&lt;P&gt;Now, I should enable the Secure Mode and I'm able to enable it changing the definition of the&amp;nbsp;Flash_Config ( defined into the file startup_*.c ) of the Bootloader.&lt;/P&gt;&lt;P&gt;We have many device in field so I should enable the secure mode by our application, I have done the same steps changing the file startup_*.c of the Application's project but it seems that it doesn't work.&amp;nbsp;&lt;/P&gt;&lt;P&gt;So I have a doubs, is it possible enabling the secure mode from the application?&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Giampietro Pomponio&lt;/P&gt;</description>
      <pubDate>Mon, 13 Mar 2023 08:52:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Configure-Flash-Security/m-p/1613874#M64838</guid>
      <dc:creator>giampietropompo</dc:creator>
      <dc:date>2023-03-13T08:52:45Z</dc:date>
    </item>
  </channel>
</rss>