<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Microcontrollers中的主题 Which IDE/SDK to use?</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Which-IDE-SDK-to-use/m-p/1608712#M64800</link>
    <description>&lt;P&gt;I'm exploring options for a new design. I've never worked with NXP tools before. I'm currently looking at the KEA64 lineup as a good fit for my needs. But I can't get started with the software tools. The webpage for these processors lists MCUXpresso as an IDE/SDK for them - but I don't see them in the list. I tried downloading the "S32DS" package - I don't see where to get started with this either as it looks like an addon to another package.&lt;/P&gt;</description>
    <pubDate>Thu, 02 Mar 2023 20:06:22 GMT</pubDate>
    <dc:creator>Thumper_LV</dc:creator>
    <dc:date>2023-03-02T20:06:22Z</dc:date>
    <item>
      <title>Which IDE/SDK to use?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Which-IDE-SDK-to-use/m-p/1608712#M64800</link>
      <description>&lt;P&gt;I'm exploring options for a new design. I've never worked with NXP tools before. I'm currently looking at the KEA64 lineup as a good fit for my needs. But I can't get started with the software tools. The webpage for these processors lists MCUXpresso as an IDE/SDK for them - but I don't see them in the list. I tried downloading the "S32DS" package - I don't see where to get started with this either as it looks like an addon to another package.&lt;/P&gt;</description>
      <pubDate>Thu, 02 Mar 2023 20:06:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Which-IDE-SDK-to-use/m-p/1608712#M64800</guid>
      <dc:creator>Thumper_LV</dc:creator>
      <dc:date>2023-03-02T20:06:22Z</dc:date>
    </item>
    <item>
      <title>Re: Which IDE/SDK to use?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Which-IDE-SDK-to-use/m-p/1608783#M64802</link>
      <description>&lt;P&gt;Hi&lt;/P&gt;
&lt;P&gt;Since the KEA series is an automotive-grade MCU, its SDK and IDE are different from Kinetis MCU. That's why you can't find KEA in MCUXpresso.&lt;BR /&gt;&lt;SPAN&gt;You can download &lt;/SPAN&gt;&lt;A href="https://www.nxp.com/webapp/Download?colCode=FRDM-KEA-QSP" target="_self"&gt;&lt;STRONG&gt;FRDM-KEA Quick start package (REV 8 )&lt;/STRONG&gt;&lt;/A&gt;&lt;SPAN&gt;&amp;nbsp;or &lt;A href="https://www.nxp.com/webapp/Download?colCode=SAMPLE-DRIVER-FRDM-KEA-S32DS" target="_self"&gt;&lt;STRONG&gt;Sample Software Drivers for KEAZ64/128 using S32DS&lt;/STRONG&gt;&lt;/A&gt; from&amp;nbsp;&lt;/SPAN&gt;&lt;A href="https://www.nxp.com/design/development-boards/automotive-development-platforms/s32k-mcu-platforms/kea-freedom-evaluation-board:FRDM-KEAZ128" target="_blank" rel="nofollow noopener noreferrer"&gt;FRDM-KEAZ128: KEA Freedom Evaluation Board&amp;nbsp;&lt;/A&gt;&lt;SPAN&gt;website.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Those examples are developed with&amp;nbsp;&lt;/SPAN&gt;&lt;A href="https://www.nxp.com/webapp/swlicensing/sso/downloadSoftware.sp?catid=S32-DS-ARM_v2018" target="_blank" rel="nofollow noopener noreferrer"&gt;S32 Design Studio for Arm 2018.R1 – Windows/Linux(REV 2018-R1)&lt;/A&gt;&lt;SPAN&gt;.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;Best Regards,&lt;BR /&gt;Robin&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;
&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
      <pubDate>Fri, 03 Mar 2023 00:56:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Which-IDE-SDK-to-use/m-p/1608783#M64802</guid>
      <dc:creator>Robin_Shen</dc:creator>
      <dc:date>2023-03-03T00:56:35Z</dc:date>
    </item>
    <item>
      <title>Re: Which IDE/SDK to use?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Which-IDE-SDK-to-use/m-p/1611411#M64822</link>
      <description>&lt;P&gt;How do I start the IDE? I downloaded the zip file, extracted it, and all I see are various .jar files - none of which execute.&lt;/P&gt;&lt;P&gt;And is the KEA a product suitable for new designs?&lt;/P&gt;</description>
      <pubDate>Wed, 08 Mar 2023 07:17:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Which-IDE-SDK-to-use/m-p/1611411#M64822</guid>
      <dc:creator>Thumper_LV</dc:creator>
      <dc:date>2023-03-08T07:17:52Z</dc:date>
    </item>
    <item>
      <title>Re: Which IDE/SDK to use?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Which-IDE-SDK-to-use/m-p/1611421#M64823</link>
      <description>&lt;P&gt;Have you download and install S32DS?&amp;nbsp;&lt;A class="download-link" href="https://freescaleesd.flexnetoperations.com/337170/367/12472367/S32DS_ARM_Win32_v2018.R1_b180326.exe?ftpRequestID=9725036697&amp;amp;server=freescaleesd.flexnetoperations.com&amp;amp;dtm=DTM20230308072337NTU5ODMxOTU4&amp;amp;authparam=1678289018_e5b05f1c86211b5de20754b9d2608089&amp;amp;ext=.exe" target="_blank"&gt;S32DS_ARM_Win32_v2018.R1_b180326.exe&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;The SDK of KEA is not good as other MCUs. Do you consider using the &lt;A href="https://www.nxp.com/products/processors-and-microcontrollers/s32-automotive-platform/s32k-auto-general-purpose-mcus/s32k1-microcontrollers-for-automotive-general-purpose:S32K1" target="_self"&gt;S32K1 Microcontrollers for Automotive General Purpose?&lt;/A&gt;&lt;/P&gt;</description>
      <pubDate>Wed, 08 Mar 2023 07:32:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Which-IDE-SDK-to-use/m-p/1611421#M64823</guid>
      <dc:creator>Robin_Shen</dc:creator>
      <dc:date>2023-03-08T07:32:28Z</dc:date>
    </item>
    <item>
      <title>Re: Which IDE/SDK to use?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Which-IDE-SDK-to-use/m-p/1636842#M64970</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;SPAN&gt;Robin&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;Is there an SDK for S32DS that is compatible with S9KEAZN8?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Regards,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Johns&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Thu, 20 Apr 2023 03:04:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Which-IDE-SDK-to-use/m-p/1636842#M64970</guid>
      <dc:creator>johns_chuang</dc:creator>
      <dc:date>2023-04-20T03:04:05Z</dc:date>
    </item>
  </channel>
</rss>