<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: kea64 on board temperature sensor in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/kea64-on-board-temperature-sensor/m-p/1606725#M64783</link>
    <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/206759"&gt;@Miguel04&lt;/a&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I used AN3031 document for calculating the Vdd.&amp;nbsp; I am using 12 bit resolution and the typical Vbg value is 1.16 for KEA64.&amp;nbsp; I got the ADCR value of the bangap channel around 300. So by using the formula&lt;/P&gt;&lt;P&gt;Vdd = 4095 * 1.16 / 300 which equals to 15.8 . Maximum Value of Vdd is 6v but here im getting it as 15.8v.&lt;/P&gt;&lt;P&gt;Am I missing something here??&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Kiran.&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Tue, 28 Feb 2023 09:04:31 GMT</pubDate>
    <dc:creator>kiran5</dc:creator>
    <dc:date>2023-02-28T09:04:31Z</dc:date>
    <item>
      <title>kea64 on board temperature sensor</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/kea64-on-board-temperature-sensor/m-p/1605901#M64777</link>
      <description>&lt;P&gt;Hi,&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am trying to calculate the temperature value using the onboard temperature sensor. I am not able to find the exact calculation formula. Please provide the details needed for the calculation of the on board temperature value&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks and regards&amp;nbsp;&lt;/P&gt;&lt;P&gt;Kiran&lt;/P&gt;</description>
      <pubDate>Mon, 27 Feb 2023 07:27:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/kea64-on-board-temperature-sensor/m-p/1605901#M64777</guid>
      <dc:creator>kiran5</dc:creator>
      <dc:date>2023-02-27T07:27:56Z</dc:date>
    </item>
    <item>
      <title>Re: kea64 on board temperature sensor</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/kea64-on-board-temperature-sensor/m-p/1606374#M64780</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/211941"&gt;@kiran5&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;This is the formula of the temperature sensor:&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Miguel04_0-1677534099546.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/212542iBA79332079AD68DC/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Miguel04_0-1677534099546.png" alt="Miguel04_0-1677534099546.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;Miguel04_0-1677534099546.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P data-unlink="true"&gt;You can find more information in the &lt;A href="https://www.nxp.com/docs/en/application-note/AN3031.pdf" target="_self"&gt;AN3031&lt;/A&gt;&amp;nbsp;and the constant values are on the datasheet on table 12.&lt;/P&gt;
&lt;P data-unlink="true"&gt;Best Regards, Miguel.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 27 Feb 2023 21:43:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/kea64-on-board-temperature-sensor/m-p/1606374#M64780</guid>
      <dc:creator>Miguel04</dc:creator>
      <dc:date>2023-02-27T21:43:41Z</dc:date>
    </item>
    <item>
      <title>Re: kea64 on board temperature sensor</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/kea64-on-board-temperature-sensor/m-p/1606725#M64783</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/206759"&gt;@Miguel04&lt;/a&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I used AN3031 document for calculating the Vdd.&amp;nbsp; I am using 12 bit resolution and the typical Vbg value is 1.16 for KEA64.&amp;nbsp; I got the ADCR value of the bangap channel around 300. So by using the formula&lt;/P&gt;&lt;P&gt;Vdd = 4095 * 1.16 / 300 which equals to 15.8 . Maximum Value of Vdd is 6v but here im getting it as 15.8v.&lt;/P&gt;&lt;P&gt;Am I missing something here??&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Kiran.&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 28 Feb 2023 09:04:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/kea64-on-board-temperature-sensor/m-p/1606725#M64783</guid>
      <dc:creator>kiran5</dc:creator>
      <dc:date>2023-02-28T09:04:31Z</dc:date>
    </item>
    <item>
      <title>Re: kea64 on board temperature sensor</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/kea64-on-board-temperature-sensor/m-p/1607043#M64784</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/211941"&gt;@kiran5&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Can you tell me the number of resolution bits of the ADCR_BG value?&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best Regards, Miguel.&lt;/P&gt;</description>
      <pubDate>Tue, 28 Feb 2023 18:20:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/kea64-on-board-temperature-sensor/m-p/1607043#M64784</guid>
      <dc:creator>Miguel04</dc:creator>
      <dc:date>2023-02-28T18:20:30Z</dc:date>
    </item>
    <item>
      <title>Re: kea64 on board temperature sensor</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/kea64-on-board-temperature-sensor/m-p/1641304#M64983</link>
      <description>Hi Miguel04&lt;BR /&gt;The adc count from the ADCR register by enabling the temperature sensor is 1110. From this value I have calculated the Vtemp as 1110*5/4095 = 1.3431..&lt;BR /&gt;Here im using 5v reference voltage and 12 bit resolution.&lt;BR /&gt;The temperature is calculated from the formula&lt;BR /&gt;Temp = 25 - ((Vtemp-Vtemp@25)/Slope).&lt;BR /&gt;= 25 - ((1.3431-1.396)/0.003638)&lt;BR /&gt;=39.54&lt;BR /&gt;Here the temperature value i get is 39.54 Celcius.&lt;BR /&gt;We connected an external NTC resistor and calculated the temperature from that and the value observed was 34.&lt;BR /&gt;There is a difference of 5 celcius. Am i doing it the right way or should is do some changes.&lt;BR /&gt;Best Regards, Kiran</description>
      <pubDate>Thu, 27 Apr 2023 07:06:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/kea64-on-board-temperature-sensor/m-p/1641304#M64983</guid>
      <dc:creator>kiran5</dc:creator>
      <dc:date>2023-04-27T07:06:30Z</dc:date>
    </item>
  </channel>
</rss>