<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックApplication doesn.t run on FRDM-K22F</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Application-doesn-t-run-on-FRDM-K22F/m-p/1600761#M64716</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I use KDS 3.2.0 and FRDM-K22F. I create a new project and choose board&lt;BR /&gt;FRDM-K22F. Now I add to the project 3 BitIO components, set them as outputs&lt;BR /&gt;with initial value '1' and select required pins to control RGB LEDs.&lt;BR /&gt;Then, I generate Processor Expert code, compile it and flash the device.&lt;BR /&gt;Everything is OK, when I press the reset button, LEDs are ON and when I release&lt;BR /&gt;it LEDs go OFF. Everything as expected.&lt;/P&gt;&lt;P&gt;Now, I create a new project and choose processor instead of board (MK22FN512VLH12)&lt;BR /&gt;and I treate the board as my own custom project. I select maximal clock frequencys&lt;BR /&gt;(core 120MHz) and all the rest I do exactly as above. Unfortunately LEDs are always ON.&lt;/P&gt;&lt;P&gt;What am I missing?&lt;/P&gt;</description>
    <pubDate>Fri, 17 Feb 2023 01:13:21 GMT</pubDate>
    <dc:creator>Stachu</dc:creator>
    <dc:date>2023-02-17T01:13:21Z</dc:date>
    <item>
      <title>Application doesn.t run on FRDM-K22F</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Application-doesn-t-run-on-FRDM-K22F/m-p/1600761#M64716</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I use KDS 3.2.0 and FRDM-K22F. I create a new project and choose board&lt;BR /&gt;FRDM-K22F. Now I add to the project 3 BitIO components, set them as outputs&lt;BR /&gt;with initial value '1' and select required pins to control RGB LEDs.&lt;BR /&gt;Then, I generate Processor Expert code, compile it and flash the device.&lt;BR /&gt;Everything is OK, when I press the reset button, LEDs are ON and when I release&lt;BR /&gt;it LEDs go OFF. Everything as expected.&lt;/P&gt;&lt;P&gt;Now, I create a new project and choose processor instead of board (MK22FN512VLH12)&lt;BR /&gt;and I treate the board as my own custom project. I select maximal clock frequencys&lt;BR /&gt;(core 120MHz) and all the rest I do exactly as above. Unfortunately LEDs are always ON.&lt;/P&gt;&lt;P&gt;What am I missing?&lt;/P&gt;</description>
      <pubDate>Fri, 17 Feb 2023 01:13:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Application-doesn-t-run-on-FRDM-K22F/m-p/1600761#M64716</guid>
      <dc:creator>Stachu</dc:creator>
      <dc:date>2023-02-17T01:13:21Z</dc:date>
    </item>
    <item>
      <title>Re: Application doesn.t run on FRDM-K22F</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Application-doesn-t-run-on-FRDM-K22F/m-p/1600899#M64717</link>
      <description>&lt;P&gt;Have you looked into it with the debugger and checked that way that the program does what you want?&lt;/P&gt;</description>
      <pubDate>Fri, 17 Feb 2023 06:23:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Application-doesn-t-run-on-FRDM-K22F/m-p/1600899#M64717</guid>
      <dc:creator>ErichStyger</dc:creator>
      <dc:date>2023-02-17T06:23:52Z</dc:date>
    </item>
    <item>
      <title>Re: Application doesn.t run on FRDM-K22F</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Application-doesn-t-run-on-FRDM-K22F/m-p/1601360#M64719</link>
      <description>&lt;P&gt;Hi Erich,&lt;/P&gt;&lt;P&gt;No, I didn't . There is no single line of my own code. In both cases there is only Processor Expert code.&lt;/P&gt;&lt;P&gt;int main(void)&lt;BR /&gt;{&lt;BR /&gt;PE_low_level_init();&lt;BR /&gt;#ifdef PEX_RTOS_START&lt;BR /&gt;PEX_RTOS_START();&lt;BR /&gt;#endif&lt;BR /&gt;for(;;){}&lt;BR /&gt;}&lt;/P&gt;&lt;P&gt;Rgds, Stachu&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 17 Feb 2023 22:55:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Application-doesn-t-run-on-FRDM-K22F/m-p/1601360#M64719</guid>
      <dc:creator>Stachu</dc:creator>
      <dc:date>2023-02-17T22:55:13Z</dc:date>
    </item>
  </channel>
</rss>