<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: CAN0_RX pin on MKS20FN256VLL12 is 5V tolerant? in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/CAN0-RX-pin-on-MKS20FN256VLL12-is-5V-tolerant/m-p/1599943#M64707</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I review the information from the Datasheet, and this did not mention the tolerance for the 5v. I recommend using a level shifter.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best regards,&lt;BR /&gt;Pavel&lt;/P&gt;</description>
    <pubDate>Wed, 15 Feb 2023 21:23:34 GMT</pubDate>
    <dc:creator>Pavel_Hernandez</dc:creator>
    <dc:date>2023-02-15T21:23:34Z</dc:date>
    <item>
      <title>CAN0_RX pin on MKS20FN256VLL12 is 5V tolerant?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/CAN0-RX-pin-on-MKS20FN256VLL12-is-5V-tolerant/m-p/1599567#M64702</link>
      <description>&lt;P&gt;Hello all,&lt;/P&gt;&lt;P&gt;I'm using a 5V transceiver TJA1051T and the RX pin is 5V.&lt;/P&gt;&lt;P&gt;I tried to find the information if&amp;nbsp;MKS20FN256VLL12 is compatible with 5V for CAN0_RX pin but I couldn't.&lt;/P&gt;&lt;P&gt;Does someone knows if I can connect directly? If not, a simple voltage divider should be enought? Any suggestions?&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;</description>
      <pubDate>Wed, 15 Feb 2023 11:41:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/CAN0-RX-pin-on-MKS20FN256VLL12-is-5V-tolerant/m-p/1599567#M64702</guid>
      <dc:creator>Flaviohpo</dc:creator>
      <dc:date>2023-02-15T11:41:18Z</dc:date>
    </item>
    <item>
      <title>Re: CAN0_RX pin on MKS20FN256VLL12 is 5V tolerant?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/CAN0-RX-pin-on-MKS20FN256VLL12-is-5V-tolerant/m-p/1599943#M64707</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I review the information from the Datasheet, and this did not mention the tolerance for the 5v. I recommend using a level shifter.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best regards,&lt;BR /&gt;Pavel&lt;/P&gt;</description>
      <pubDate>Wed, 15 Feb 2023 21:23:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/CAN0-RX-pin-on-MKS20FN256VLL12-is-5V-tolerant/m-p/1599943#M64707</guid>
      <dc:creator>Pavel_Hernandez</dc:creator>
      <dc:date>2023-02-15T21:23:34Z</dc:date>
    </item>
  </channel>
</rss>