<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Flashing problem with MKL13Z32 in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Flashing-problem-with-MKL13Z32/m-p/1598880#M64693</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I have problem with ML13Z32 programming via SWD interface.&lt;/P&gt;&lt;P&gt;Using SEGGER J-Link probe with J-Flash software, every time I attempt to flash or erase the MCU, the probe connects correctly to MCU but after this it returns "Failed to download RAMCode" error.&lt;BR /&gt;I have checked power supply and signals and they are all OK.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="image002.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/210857i527DE31F12CC1EA0/image-size/medium?v=v2&amp;amp;px=400" role="button" title="image002.png" alt="image002.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;image002.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;I have tried to connect the MCU with KinetisFlashTool via UART (on PTA1 and PTA2 pins) and the MCU was flashed correctly.&lt;/P&gt;&lt;P&gt;J-Flash configuration is the same I use with other MCUs (e.g. MKL14Z64, MKE15Z64, MK34Z256, ...), maybe is it necessary another configuration?&lt;/P&gt;&lt;P&gt;Thank you in advance for the support&lt;/P&gt;</description>
    <pubDate>Tue, 14 Feb 2023 12:55:54 GMT</pubDate>
    <dc:creator>DanieleRossiFW</dc:creator>
    <dc:date>2023-02-14T12:55:54Z</dc:date>
    <item>
      <title>Flashing problem with MKL13Z32</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Flashing-problem-with-MKL13Z32/m-p/1598880#M64693</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I have problem with ML13Z32 programming via SWD interface.&lt;/P&gt;&lt;P&gt;Using SEGGER J-Link probe with J-Flash software, every time I attempt to flash or erase the MCU, the probe connects correctly to MCU but after this it returns "Failed to download RAMCode" error.&lt;BR /&gt;I have checked power supply and signals and they are all OK.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="image002.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/210857i527DE31F12CC1EA0/image-size/medium?v=v2&amp;amp;px=400" role="button" title="image002.png" alt="image002.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;image002.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;I have tried to connect the MCU with KinetisFlashTool via UART (on PTA1 and PTA2 pins) and the MCU was flashed correctly.&lt;/P&gt;&lt;P&gt;J-Flash configuration is the same I use with other MCUs (e.g. MKL14Z64, MKE15Z64, MK34Z256, ...), maybe is it necessary another configuration?&lt;/P&gt;&lt;P&gt;Thank you in advance for the support&lt;/P&gt;</description>
      <pubDate>Tue, 14 Feb 2023 12:55:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Flashing-problem-with-MKL13Z32/m-p/1598880#M64693</guid>
      <dc:creator>DanieleRossiFW</dc:creator>
      <dc:date>2023-02-14T12:55:54Z</dc:date>
    </item>
    <item>
      <title>Re: Flashing problem with MKL13Z32</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Flashing-problem-with-MKL13Z32/m-p/1692293#M65316</link>
      <description>&lt;P&gt;I am utilizing SEGGER J-Flash version 7.88m and encountering identical error outcomes.&lt;BR /&gt;I've noticed that the configuration file generated by the Jflash tool has set the RAM size to 16K, which is incorrect for my current situation.&lt;BR /&gt;I am currently utilizing the MKL13Z32VLH4 processor, which only has 4K of RAM. Additionally, the starting location of the RAM was incorrect.&lt;/P&gt;&lt;P&gt;To determine the precise location of your RAM start and its size, you can refer to your linker file. Afterwards, you need to ensure that the *.jflash file is correctly configured with this information. Once I completed these steps, I was able to establish a connection and successfully program the processor.&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 25 Jul 2023 13:01:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Flashing-problem-with-MKL13Z32/m-p/1692293#M65316</guid>
      <dc:creator>dave__</dc:creator>
      <dc:date>2023-07-25T13:01:50Z</dc:date>
    </item>
  </channel>
</rss>