<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: CAN demo with FRDM-KEAZ64 in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/CAN-demo-with-FRDM-KEAZ64/m-p/1588125#M64609</link>
    <description>I forgot to add that I am using S32DS 2.0</description>
    <pubDate>Thu, 26 Jan 2023 03:00:58 GMT</pubDate>
    <dc:creator>charleszimnicki</dc:creator>
    <dc:date>2023-01-26T03:00:58Z</dc:date>
    <item>
      <title>CAN demo with FRDM-KEAZ64</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/CAN-demo-with-FRDM-KEAZ64/m-p/1588123#M64608</link>
      <description>&lt;P&gt;I tried to run a CAN demo from FRDM_KEA128_MSCAN. I selected a default function:&lt;BR /&gt;&lt;BR /&gt;TEST_CASE_FUNC(Demo_Transmit_DataFrame);&lt;BR /&gt;&lt;BR /&gt;The program compiled, loaded and seems to run in the debugger mode but does not produce CAN data output on the PTC7 (as I think it should). My questions are:&lt;BR /&gt;- Is there a CAN demo specifically made for KEAZ64?&lt;BR /&gt;- If not, which build files I would need to replace to make it compatible with KEAZ64?&lt;BR /&gt;- Am I missing something, like perhaps some other pin dependencies?&lt;/P&gt;</description>
      <pubDate>Thu, 26 Jan 2023 02:59:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/CAN-demo-with-FRDM-KEAZ64/m-p/1588123#M64608</guid>
      <dc:creator>charleszimnicki</dc:creator>
      <dc:date>2023-01-26T02:59:54Z</dc:date>
    </item>
    <item>
      <title>Re: CAN demo with FRDM-KEAZ64</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/CAN-demo-with-FRDM-KEAZ64/m-p/1588125#M64609</link>
      <description>I forgot to add that I am using S32DS 2.0</description>
      <pubDate>Thu, 26 Jan 2023 03:00:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/CAN-demo-with-FRDM-KEAZ64/m-p/1588125#M64609</guid>
      <dc:creator>charleszimnicki</dc:creator>
      <dc:date>2023-01-26T03:00:58Z</dc:date>
    </item>
    <item>
      <title>Re: CAN demo with FRDM-KEAZ64</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/CAN-demo-with-FRDM-KEAZ64/m-p/1588598#M64617</link>
      <description>&lt;P&gt;Running MSCAN example proved not as simple as I originally thought. I found an answer to my own question (and some other ones) on another forum:&lt;BR /&gt;&lt;BR /&gt;&lt;A href="https://community.nxp.com/t5/S32-Design-Studio/S32-KEAZ-SDK-PEX-MSCAN-Missing-Help/m-p/660826" target="_blank"&gt;https://community.nxp.com/t5/S32-Design-Studio/S32-KEAZ-SDK-PEX-MSCAN-Missing-Help/m-p/660826&lt;/A&gt;&lt;/P&gt;</description>
      <pubDate>Fri, 27 Jan 2023 00:12:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/CAN-demo-with-FRDM-KEAZ64/m-p/1588598#M64617</guid>
      <dc:creator>charleszimnicki</dc:creator>
      <dc:date>2023-01-27T00:12:19Z</dc:date>
    </item>
  </channel>
</rss>