<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックHelp running QSPI_led_demo program on K82F Freedom board</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Help-running-QSPI-led-demo-program-on-K82F-Freedom-board/m-p/1588017#M64607</link>
    <description>&lt;P&gt;I am a new user of the K82F Freedom board. &amp;nbsp;My board and setup is working because I can load the blinky program to flash the LED (and Com3 shows up).&amp;nbsp;&amp;nbsp; However, I am trying to test out the QSPI flash. I am trying to get the led_demo_qspi_aooo or led_demo_qspi_alias_aooo demo working &amp;nbsp;using MCUExpresso IDE 11.6.1 under Windows 11.&lt;/P&gt;&lt;P&gt;The code compiles OK. When I try to run it for MCUExpresso it says it is running, but the LED does not light and it is not running.&lt;/P&gt;&lt;P&gt;After reading through the documentation again, it appears that I need to load this from the Bootloader.&amp;nbsp; I found a reference that says I can start the Booloader by holding Reset while plugging in the USB until the USB is registered. The Maintenance drive&amp;nbsp; D:MAINTAINANCE shows up. However, my Com Port (com3) does not show up. The blhost fails because it does not see a com port.&lt;/P&gt;&lt;P&gt;I tried running blhost. It said it could not connect.&lt;BR /&gt;I tried running the KinetisFlashTool.&amp;nbsp; It said it could not connect.&lt;/P&gt;&lt;P&gt;How do I get the bootloader running with the COM port?&lt;BR /&gt;Once the bootloader is running, do I need to&amp;nbsp; load the qspi_config.block.bin file and then load the application?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Wed, 25 Jan 2023 21:38:56 GMT</pubDate>
    <dc:creator>Bob99</dc:creator>
    <dc:date>2023-01-25T21:38:56Z</dc:date>
    <item>
      <title>Help running QSPI_led_demo program on K82F Freedom board</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Help-running-QSPI-led-demo-program-on-K82F-Freedom-board/m-p/1588017#M64607</link>
      <description>&lt;P&gt;I am a new user of the K82F Freedom board. &amp;nbsp;My board and setup is working because I can load the blinky program to flash the LED (and Com3 shows up).&amp;nbsp;&amp;nbsp; However, I am trying to test out the QSPI flash. I am trying to get the led_demo_qspi_aooo or led_demo_qspi_alias_aooo demo working &amp;nbsp;using MCUExpresso IDE 11.6.1 under Windows 11.&lt;/P&gt;&lt;P&gt;The code compiles OK. When I try to run it for MCUExpresso it says it is running, but the LED does not light and it is not running.&lt;/P&gt;&lt;P&gt;After reading through the documentation again, it appears that I need to load this from the Bootloader.&amp;nbsp; I found a reference that says I can start the Booloader by holding Reset while plugging in the USB until the USB is registered. The Maintenance drive&amp;nbsp; D:MAINTAINANCE shows up. However, my Com Port (com3) does not show up. The blhost fails because it does not see a com port.&lt;/P&gt;&lt;P&gt;I tried running blhost. It said it could not connect.&lt;BR /&gt;I tried running the KinetisFlashTool.&amp;nbsp; It said it could not connect.&lt;/P&gt;&lt;P&gt;How do I get the bootloader running with the COM port?&lt;BR /&gt;Once the bootloader is running, do I need to&amp;nbsp; load the qspi_config.block.bin file and then load the application?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 25 Jan 2023 21:38:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Help-running-QSPI-led-demo-program-on-K82F-Freedom-board/m-p/1588017#M64607</guid>
      <dc:creator>Bob99</dc:creator>
      <dc:date>2023-01-25T21:38:56Z</dc:date>
    </item>
    <item>
      <title>Re: Help running QSPI_led_demo program on K82F Freedom board</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Help-running-QSPI-led-demo-program-on-K82F-Freedom-board/m-p/1590754#M64633</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/211717"&gt;@Bob99&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;I'll prepare the steps to follow to run the demo.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;I'll be investigating more of your issue. Also, I've seen your other posts and I'm looking into them too.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Best Regards, Miguel.&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Tue, 31 Jan 2023 18:46:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Help-running-QSPI-led-demo-program-on-K82F-Freedom-board/m-p/1590754#M64633</guid>
      <dc:creator>Miguel04</dc:creator>
      <dc:date>2023-01-31T18:46:50Z</dc:date>
    </item>
  </channel>
</rss>