<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックMK10DX128VLH7 ADC issue</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/MK10DX128VLH7-ADC-issue/m-p/1588004#M64606</link>
    <description>&lt;P&gt;I have some code running on an MK10DX128VLH5 processor without issues.&amp;nbsp; We had supply chain&amp;nbsp;issues and swapped to MK10DX128VLH7.&amp;nbsp; I am having a problem with pin 12 (ADC0_DM3 adc channel 21).&amp;nbsp; The readings are all over the&amp;nbsp;place.&amp;nbsp; On the VLH5 all is good.&amp;nbsp; I am also using pins 11, 10, and 9 without an issue.&amp;nbsp; The VLH7 differs in that it has ADC1 as well.&amp;nbsp; On that particular pin (12) I used ADC1_DM3 (adc channel 19) and the readings are good.&amp;nbsp; So the same pin, just different ADC and channel.&amp;nbsp; Is there some errata that is not published or I didn't see.&lt;/P&gt;</description>
    <pubDate>Wed, 25 Jan 2023 21:13:32 GMT</pubDate>
    <dc:creator>marknorton</dc:creator>
    <dc:date>2023-01-25T21:13:32Z</dc:date>
    <item>
      <title>MK10DX128VLH7 ADC issue</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/MK10DX128VLH7-ADC-issue/m-p/1588004#M64606</link>
      <description>&lt;P&gt;I have some code running on an MK10DX128VLH5 processor without issues.&amp;nbsp; We had supply chain&amp;nbsp;issues and swapped to MK10DX128VLH7.&amp;nbsp; I am having a problem with pin 12 (ADC0_DM3 adc channel 21).&amp;nbsp; The readings are all over the&amp;nbsp;place.&amp;nbsp; On the VLH5 all is good.&amp;nbsp; I am also using pins 11, 10, and 9 without an issue.&amp;nbsp; The VLH7 differs in that it has ADC1 as well.&amp;nbsp; On that particular pin (12) I used ADC1_DM3 (adc channel 19) and the readings are good.&amp;nbsp; So the same pin, just different ADC and channel.&amp;nbsp; Is there some errata that is not published or I didn't see.&lt;/P&gt;</description>
      <pubDate>Wed, 25 Jan 2023 21:13:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/MK10DX128VLH7-ADC-issue/m-p/1588004#M64606</guid>
      <dc:creator>marknorton</dc:creator>
      <dc:date>2023-01-25T21:13:32Z</dc:date>
    </item>
    <item>
      <title>Re: MK10DX128VLH7 ADC issue</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/MK10DX128VLH7-ADC-issue/m-p/1589131#M64621</link>
      <description>&lt;P&gt;Hi&lt;/P&gt;
&lt;P&gt;there are some erratas on the next link&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com/products/processors-and-microcontrollers/arm-microcontrollers/general-purpose-mcus/k-series-arm-cortex-m4/k1x-mainstream/kinetis-k10-72-mhz-mixed-signal-integration-microcontrollers-mcus-based-on-arm-cortex-m4-core:K10_72?fpsp=1#documentation" target="_blank"&gt;https://www.nxp.com/products/processors-and-microcontrollers/arm-microcontrollers/general-purpose-mcus/k-series-arm-cortex-m4/k1x-mainstream/kinetis-k10-72-mhz-mixed-signal-integration-microcontrollers-mcus-based-on-arm-cortex-m4-core:K10_72?fpsp=1#documentation&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;and those are all of them&lt;/P&gt;
&lt;P&gt;what kind of problem do you have?&lt;/P&gt;
&lt;P&gt;what happens if you add some time between the measurements?&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Have a good day.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 27 Jan 2023 23:49:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/MK10DX128VLH7-ADC-issue/m-p/1589131#M64621</guid>
      <dc:creator>vicentegomez</dc:creator>
      <dc:date>2023-01-27T23:49:59Z</dc:date>
    </item>
  </channel>
</rss>