<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックS9KEAZN32ACLH</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/S9KEAZN32ACLH/m-p/1585989#M64597</link>
    <description>&lt;P&gt;Hi, i have a s9KEAZN32ACLH microcontroller but i'm not able to set 40MHz output clock in FEI mode.&lt;/P&gt;&lt;P&gt;This is my setup:&lt;/P&gt;&lt;P&gt;#define CPU_XTAL_CLK_HZ 0u /* Value of the external crystal or oscillator clock frequency in Hz */&lt;BR /&gt;#define CPU_INT_CLK_HZ 39062u /* Value of the slow internal oscillator clock frequency in Hz */&lt;/P&gt;&lt;P&gt;#if (CLOCK_SETUP == 6)&lt;BR /&gt;#define DEFAULT_SYSTEM_CLOCK 40000000u&amp;nbsp;&lt;/P&gt;&lt;P&gt;#define ICS_MODE ICS_MODE_FEI&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;#define ICS_C1_VALUE 0x04U&lt;/P&gt;&lt;P&gt;#define ICS_C2_VALUE 0x00U&amp;nbsp;&lt;BR /&gt;#define ICS_C4_VALUE 0x00U&amp;nbsp;&lt;BR /&gt;#define OSC_CR_VALUE 0x00U&amp;nbsp;&lt;BR /&gt;#define SIM_BUSDIV_VALUE 0x01U&amp;nbsp;&lt;/P&gt;&lt;P&gt;I set also&amp;nbsp;&lt;/P&gt;&lt;P&gt;SIM_SOPT |= SIM_SOPT_CLKOE_MASK;&lt;/P&gt;&lt;P&gt;to see bus clock frequency on PTH2, but now i see 16MHz instead of 20MHz.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I'have another question:&lt;/P&gt;&lt;P&gt;-what is the reference manual for this microcontroller? I don't see s9KEAZN32ACLH in any manuals.&lt;/P&gt;&lt;P&gt;Thank you!&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Fri, 20 Jan 2023 11:34:36 GMT</pubDate>
    <dc:creator>EmanueleP</dc:creator>
    <dc:date>2023-01-20T11:34:36Z</dc:date>
    <item>
      <title>S9KEAZN32ACLH</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/S9KEAZN32ACLH/m-p/1585989#M64597</link>
      <description>&lt;P&gt;Hi, i have a s9KEAZN32ACLH microcontroller but i'm not able to set 40MHz output clock in FEI mode.&lt;/P&gt;&lt;P&gt;This is my setup:&lt;/P&gt;&lt;P&gt;#define CPU_XTAL_CLK_HZ 0u /* Value of the external crystal or oscillator clock frequency in Hz */&lt;BR /&gt;#define CPU_INT_CLK_HZ 39062u /* Value of the slow internal oscillator clock frequency in Hz */&lt;/P&gt;&lt;P&gt;#if (CLOCK_SETUP == 6)&lt;BR /&gt;#define DEFAULT_SYSTEM_CLOCK 40000000u&amp;nbsp;&lt;/P&gt;&lt;P&gt;#define ICS_MODE ICS_MODE_FEI&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;#define ICS_C1_VALUE 0x04U&lt;/P&gt;&lt;P&gt;#define ICS_C2_VALUE 0x00U&amp;nbsp;&lt;BR /&gt;#define ICS_C4_VALUE 0x00U&amp;nbsp;&lt;BR /&gt;#define OSC_CR_VALUE 0x00U&amp;nbsp;&lt;BR /&gt;#define SIM_BUSDIV_VALUE 0x01U&amp;nbsp;&lt;/P&gt;&lt;P&gt;I set also&amp;nbsp;&lt;/P&gt;&lt;P&gt;SIM_SOPT |= SIM_SOPT_CLKOE_MASK;&lt;/P&gt;&lt;P&gt;to see bus clock frequency on PTH2, but now i see 16MHz instead of 20MHz.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I'have another question:&lt;/P&gt;&lt;P&gt;-what is the reference manual for this microcontroller? I don't see s9KEAZN32ACLH in any manuals.&lt;/P&gt;&lt;P&gt;Thank you!&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 20 Jan 2023 11:34:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/S9KEAZN32ACLH/m-p/1585989#M64597</guid>
      <dc:creator>EmanueleP</dc:creator>
      <dc:date>2023-01-20T11:34:36Z</dc:date>
    </item>
  </channel>
</rss>