<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックNXP Freemaster S32K144 board connection issue</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/NXP-Freemaster-S32K144-board-connection-issue/m-p/1585010#M64593</link>
    <description>&lt;P&gt;Hello everyone,&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am facing an issue with connecting my S32K144 board in the NXP Freemaster software. I am using 2.0 version. After I select the correct port in Project Options, and then proceed to Tools&amp;gt;Connection wizard&amp;gt;Next&amp;gt;Use direct connection to on-board USB port&amp;gt;Serial port to probe is selected (OpenSDA) and baud rate is 115200&amp;gt;Next After scanning all ports, I get an error message No board detected on any of specified UART communication ports.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Note that I checked in Device manager under Ports and correct port was getting displayed.&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Prathamesh&lt;/P&gt;</description>
    <pubDate>Wed, 18 Jan 2023 21:22:04 GMT</pubDate>
    <dc:creator>prkale</dc:creator>
    <dc:date>2023-01-18T21:22:04Z</dc:date>
    <item>
      <title>NXP Freemaster S32K144 board connection issue</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/NXP-Freemaster-S32K144-board-connection-issue/m-p/1585010#M64593</link>
      <description>&lt;P&gt;Hello everyone,&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am facing an issue with connecting my S32K144 board in the NXP Freemaster software. I am using 2.0 version. After I select the correct port in Project Options, and then proceed to Tools&amp;gt;Connection wizard&amp;gt;Next&amp;gt;Use direct connection to on-board USB port&amp;gt;Serial port to probe is selected (OpenSDA) and baud rate is 115200&amp;gt;Next After scanning all ports, I get an error message No board detected on any of specified UART communication ports.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Note that I checked in Device manager under Ports and correct port was getting displayed.&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Prathamesh&lt;/P&gt;</description>
      <pubDate>Wed, 18 Jan 2023 21:22:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/NXP-Freemaster-S32K144-board-connection-issue/m-p/1585010#M64593</guid>
      <dc:creator>prkale</dc:creator>
      <dc:date>2023-01-18T21:22:04Z</dc:date>
    </item>
    <item>
      <title>Re: NXP Freemaster S32K144 board connection issue</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/NXP-Freemaster-S32K144-board-connection-issue/m-p/1585100#M64594</link>
      <description>&lt;P&gt;Hi&amp;nbsp;Prathamesh,&lt;/P&gt;
&lt;P&gt;Have you refer to &lt;STRONG&gt;FreeMASTER Tutorial series&lt;/STRONG&gt;&lt;SPAN&gt;&amp;nbsp;&lt;A href="https://community.nxp.com/t5/FreeMASTER-Knowledge-Base/Communication-Driver-Application-Configuration/ta-p/1117797" target="_self"&gt;Communication Driver - Application Configuration&lt;/A&gt;&lt;/SPAN&gt;?&lt;/P&gt;
&lt;P&gt;Or have you tried to download the freemaster_s32k144 example in S32K SDK to S32K144EVB? That example configure the LPUART baud rate as 9600 in&amp;nbsp;freemaster_s32k144/board/peripherals_lpuart1.c&lt;BR /&gt;&lt;EM&gt;&lt;FONT color="#808080"&gt;The example documentation can be found in the S32 SDK documentation at Examples and Demos section. (&amp;lt;SDK_PATH&amp;gt;/doc/Start_Here.html)&lt;/FONT&gt;&amp;nbsp;&lt;/EM&gt;file:///C:/NXP/S32DS.3.4/S32DS/software/S32SDK_S32K1XX_RTM_4.0.3/doc/html_S32K144/freemaster_s32k144_group.html&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="freemaster_s32k144.png" style="width: 807px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/207843i6FDFEC414C4336F2/image-size/large?v=v2&amp;amp;px=999" role="button" title="freemaster_s32k144.png" alt="freemaster_s32k144.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&lt;BR /&gt;Best Regards,&lt;BR /&gt;Robin&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;
&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
      <pubDate>Thu, 19 Jan 2023 01:26:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/NXP-Freemaster-S32K144-board-connection-issue/m-p/1585100#M64594</guid>
      <dc:creator>Robin_Shen</dc:creator>
      <dc:date>2023-01-19T01:26:53Z</dc:date>
    </item>
    <item>
      <title>Re: NXP Freemaster S32K144 board connection issue</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/NXP-Freemaster-S32K144-board-connection-issue/m-p/1585661#M64596</link>
      <description>Thank you so much for that!&lt;BR /&gt;</description>
      <pubDate>Thu, 19 Jan 2023 18:00:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/NXP-Freemaster-S32K144-board-connection-issue/m-p/1585661#M64596</guid>
      <dc:creator>prkale</dc:creator>
      <dc:date>2023-01-19T18:00:48Z</dc:date>
    </item>
  </channel>
</rss>