<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic MIMXRT1064 RAM Application in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/MIMXRT1064-RAM-Application/m-p/1574914#M64515</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I'm working on a project with a MIMXRT1064 microcontroller. I need to load the application from External Flash to internal DTC RAM. I've followed &lt;A href="https://community.nxp.com/t5/i-MX-RT-Knowledge-Base/Generating-a-Bootable-Image-for-the-RT1050/ta-p/1123079" target="_self"&gt;this&lt;/A&gt; guide and everything works well, but I would like to create a bootable binary image from MCU Expresso or using a python script, so that I can load the application using Ozone or directly from MCUEspressoIDE. How can I do that?&lt;/P&gt;</description>
    <pubDate>Tue, 27 Dec 2022 12:08:42 GMT</pubDate>
    <dc:creator>GiulioDallaVecchia</dc:creator>
    <dc:date>2022-12-27T12:08:42Z</dc:date>
    <item>
      <title>MIMXRT1064 RAM Application</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/MIMXRT1064-RAM-Application/m-p/1574914#M64515</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I'm working on a project with a MIMXRT1064 microcontroller. I need to load the application from External Flash to internal DTC RAM. I've followed &lt;A href="https://community.nxp.com/t5/i-MX-RT-Knowledge-Base/Generating-a-Bootable-Image-for-the-RT1050/ta-p/1123079" target="_self"&gt;this&lt;/A&gt; guide and everything works well, but I would like to create a bootable binary image from MCU Expresso or using a python script, so that I can load the application using Ozone or directly from MCUEspressoIDE. How can I do that?&lt;/P&gt;</description>
      <pubDate>Tue, 27 Dec 2022 12:08:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/MIMXRT1064-RAM-Application/m-p/1574914#M64515</guid>
      <dc:creator>GiulioDallaVecchia</dc:creator>
      <dc:date>2022-12-27T12:08:42Z</dc:date>
    </item>
    <item>
      <title>Re: MIMXRT1064 RAM Application</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/MIMXRT1064-RAM-Application/m-p/1575310#M64520</link>
      <description>&lt;P&gt;These are the steps to execute the image from RAM:&lt;/P&gt;
&lt;P&gt;1. Select Project &amp;gt; Properties - C/C++ Build &amp;gt; Settings &amp;gt; Tool Settings &amp;gt; MCU Linker &amp;gt; Managed Linker Script and check Link application to RAM.&lt;/P&gt;
&lt;P&gt;2. In Project &amp;gt; Properties &amp;gt; C/C++ Build &amp;gt; MCU settings, delete Flash, and modify SRAM_ITC to start at (BASE + 0x3000) with size (SIZE - 0x3000).&lt;/P&gt;
&lt;P&gt;3. Move SRAM_ITC to the first position to make it default.&lt;/P&gt;
&lt;P&gt;4. Build the image.&lt;/P&gt;
&lt;P&gt;Best regards,&lt;BR /&gt;Omar&lt;/P&gt;</description>
      <pubDate>Wed, 28 Dec 2022 22:09:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/MIMXRT1064-RAM-Application/m-p/1575310#M64520</guid>
      <dc:creator>Omar_Anguiano</dc:creator>
      <dc:date>2022-12-28T22:09:42Z</dc:date>
    </item>
  </channel>
</rss>