<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックK10 watchdog slows with 100% interrupts</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K10-watchdog-slows-with-100-interrupts/m-p/1574834#M64514</link>
    <description>&lt;P&gt;Working with a K10 processor, configured with the Processor Expert and running on MQX. I set up the watch dog and did some some simple test, it seems to work fine. However, I have a bug in my CAN input that generates interrupts 100% of the time. The code I have that tickles the watchdog is starved out and not called. The CAN issue I can fix but I don't know why the watchdog is not kicking in. I can stop and look at the WD registers. I can see the counter is changing but real slow. So if I wait a LONG time, it might timeout. Any idea what can cause this?&amp;nbsp; Could this have something to do with the PEMicro hardware debugger attached?&lt;/P&gt;</description>
    <pubDate>Tue, 27 Dec 2022 16:48:59 GMT</pubDate>
    <dc:creator>bflorac</dc:creator>
    <dc:date>2022-12-27T16:48:59Z</dc:date>
    <item>
      <title>K10 watchdog slows with 100% interrupts</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K10-watchdog-slows-with-100-interrupts/m-p/1574834#M64514</link>
      <description>&lt;P&gt;Working with a K10 processor, configured with the Processor Expert and running on MQX. I set up the watch dog and did some some simple test, it seems to work fine. However, I have a bug in my CAN input that generates interrupts 100% of the time. The code I have that tickles the watchdog is starved out and not called. The CAN issue I can fix but I don't know why the watchdog is not kicking in. I can stop and look at the WD registers. I can see the counter is changing but real slow. So if I wait a LONG time, it might timeout. Any idea what can cause this?&amp;nbsp; Could this have something to do with the PEMicro hardware debugger attached?&lt;/P&gt;</description>
      <pubDate>Tue, 27 Dec 2022 16:48:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K10-watchdog-slows-with-100-interrupts/m-p/1574834#M64514</guid>
      <dc:creator>bflorac</dc:creator>
      <dc:date>2022-12-27T16:48:59Z</dc:date>
    </item>
  </channel>
</rss>