<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Microcontrollers中的主题 iseled SPI protocol</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/iseled-SPI-protocol/m-p/1573578#M64492</link>
    <description>&lt;P&gt;Dear NXP,&lt;/P&gt;&lt;P&gt;I need to build the application using MK22FN512 to control the iseled via&amp;nbsp;INLC10AQ by SPI protocol.&lt;/P&gt;&lt;P&gt;But there are no any document about the address to send the command for example&amp;nbsp;digLED_Init_Strip.&lt;/P&gt;&lt;P&gt;Is that possible to give me that kind of document .&lt;/P&gt;&lt;P&gt;Thanks you so much !&lt;/P&gt;</description>
    <pubDate>Thu, 22 Dec 2022 07:55:27 GMT</pubDate>
    <dc:creator>toxuandung</dc:creator>
    <dc:date>2022-12-22T07:55:27Z</dc:date>
    <item>
      <title>iseled SPI protocol</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/iseled-SPI-protocol/m-p/1573578#M64492</link>
      <description>&lt;P&gt;Dear NXP,&lt;/P&gt;&lt;P&gt;I need to build the application using MK22FN512 to control the iseled via&amp;nbsp;INLC10AQ by SPI protocol.&lt;/P&gt;&lt;P&gt;But there are no any document about the address to send the command for example&amp;nbsp;digLED_Init_Strip.&lt;/P&gt;&lt;P&gt;Is that possible to give me that kind of document .&lt;/P&gt;&lt;P&gt;Thanks you so much !&lt;/P&gt;</description>
      <pubDate>Thu, 22 Dec 2022 07:55:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/iseled-SPI-protocol/m-p/1573578#M64492</guid>
      <dc:creator>toxuandung</dc:creator>
      <dc:date>2022-12-22T07:55:27Z</dc:date>
    </item>
    <item>
      <title>Re: iseled SPI protocol</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/iseled-SPI-protocol/m-p/1573892#M64500</link>
      <description>&lt;P class="lia-align-justify"&gt;Hello &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/209726"&gt;@toxuandung&lt;/a&gt;,&lt;/P&gt;
&lt;P class="lia-align-justify"&gt;Unfortunately, we do not have a document to control ISELED INLC10AQ via SPI for the MK22FN512.&lt;/P&gt;
&lt;P class="lia-align-justify"&gt;Nonetheless, might be useful to take a look to the following documentation for your application:&lt;/P&gt;
&lt;UL class="lia-align-justify" type="disc"&gt;
&lt;LI&gt;&lt;A href="https://www.nxp.com/webapp/Download?colCode=S32K1XXISELEDUG" target="_blank"&gt;ISELED User Guide with S32K1XX&lt;/A&gt;&lt;/LI&gt;
&lt;LI&gt;&lt;A href="https://www.nxp.com/webapp/Download?colCode=K22P121M120SF8RM" target="_blank"&gt;Kinetis K22: 120MHz Cortex-M4F 256KB Flash (64-121 pin)&lt;/A&gt; Reference Manual&lt;/LI&gt;
&lt;LI&gt;The next application note related with QUADSPI: &lt;A href="https://www.nxp.com/docs/en/application-note/AN5244.pdf" target="_blank"&gt;https://www.nxp.com/docs/en/application-note/AN5244.pdf&lt;/A&gt;&lt;/LI&gt;
&lt;/UL&gt;
&lt;P class="lia-align-justify"&gt;Hope any of the information may work for you.&lt;/P&gt;
&lt;P class="lia-align-justify"&gt;Regards, Raul.&lt;/P&gt;</description>
      <pubDate>Thu, 22 Dec 2022 20:39:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/iseled-SPI-protocol/m-p/1573892#M64500</guid>
      <dc:creator>RaRo</dc:creator>
      <dc:date>2022-12-22T20:39:45Z</dc:date>
    </item>
  </channel>
</rss>