<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックFlexcan Tx/Rx - MK64FX512</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Flexcan-Tx-Rx-MK64FX512/m-p/1569171#M64445</link>
    <description>&lt;P&gt;&lt;SPAN&gt;Hello, Community,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;I am having a problem with getting the Flexcan tx/rx functioning. I am using the latest version of MCUXpresso (11.6.1), with the SDK_2_11_0_MK64FX512xxx12 loaded and a target board using the MK64FX512VLL12 micro. I am running in debugger mode using the OpenSDA Link Services.&amp;nbsp; I have set the tx/rx to use both loopback transfer examples with ISR and the callback function method from the examples, and set up the initializations to happen in the generated periferals.c file. I am working on classic CAN Extended ID priject and conducting my testing using a CAN network with a CANalyzer. testing at 250K bitrate - I verified the timing is correct on the scope and keep getting a stuff bit or Rx error.&amp;nbsp; When tracing the code,the execution is returning a 5310 status error on the transmit callback, and it appears that the interrupts are not working - I am using the routines in the flexcan_loopback_transfer example.c that uses the non blocking transfer functions. I even tried a hypbrid using the callback method for the tx and the ISR method from the flexcan_loopback.c routines for the ISR based rx. &lt;/SPAN&gt;&lt;SPAN&gt;In my configuration I have tx set up as mb0 and rx mb1 to 11 set up for extended ID as I am building a J1939 framework example ID 0x18FFA080. My recent testing - I also noticed that upon starting the debugger session and stepping through the first tx attempt it appears to go through then after that the tx message buffer allways returns status = kStatus_FLEXCAN_TxBusy; from the status_t FLEXCAN_TransferSendNonBlocking function in fsl_flexcan.c . I have even tried to clear the mb interrup flag, diasable the mb interrupt and try a standard id message but always returns the busy status. another opservation is that it apperas that the extended id masking macros may be corrupting the .id in the frame structure.&amp;nbsp; I have submitted a help ticket and still have gotten no response, so maybe my friends in the community may be able to offer some insight.&amp;nbsp; Thank you in advance...&lt;/SPAN&gt;&lt;/P&gt;</description>
    <pubDate>Tue, 13 Dec 2022 21:04:38 GMT</pubDate>
    <dc:creator>jrozsnaki</dc:creator>
    <dc:date>2022-12-13T21:04:38Z</dc:date>
    <item>
      <title>Flexcan Tx/Rx - MK64FX512</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Flexcan-Tx-Rx-MK64FX512/m-p/1569171#M64445</link>
      <description>&lt;P&gt;&lt;SPAN&gt;Hello, Community,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;I am having a problem with getting the Flexcan tx/rx functioning. I am using the latest version of MCUXpresso (11.6.1), with the SDK_2_11_0_MK64FX512xxx12 loaded and a target board using the MK64FX512VLL12 micro. I am running in debugger mode using the OpenSDA Link Services.&amp;nbsp; I have set the tx/rx to use both loopback transfer examples with ISR and the callback function method from the examples, and set up the initializations to happen in the generated periferals.c file. I am working on classic CAN Extended ID priject and conducting my testing using a CAN network with a CANalyzer. testing at 250K bitrate - I verified the timing is correct on the scope and keep getting a stuff bit or Rx error.&amp;nbsp; When tracing the code,the execution is returning a 5310 status error on the transmit callback, and it appears that the interrupts are not working - I am using the routines in the flexcan_loopback_transfer example.c that uses the non blocking transfer functions. I even tried a hypbrid using the callback method for the tx and the ISR method from the flexcan_loopback.c routines for the ISR based rx. &lt;/SPAN&gt;&lt;SPAN&gt;In my configuration I have tx set up as mb0 and rx mb1 to 11 set up for extended ID as I am building a J1939 framework example ID 0x18FFA080. My recent testing - I also noticed that upon starting the debugger session and stepping through the first tx attempt it appears to go through then after that the tx message buffer allways returns status = kStatus_FLEXCAN_TxBusy; from the status_t FLEXCAN_TransferSendNonBlocking function in fsl_flexcan.c . I have even tried to clear the mb interrup flag, diasable the mb interrupt and try a standard id message but always returns the busy status. another opservation is that it apperas that the extended id masking macros may be corrupting the .id in the frame structure.&amp;nbsp; I have submitted a help ticket and still have gotten no response, so maybe my friends in the community may be able to offer some insight.&amp;nbsp; Thank you in advance...&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Tue, 13 Dec 2022 21:04:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Flexcan-Tx-Rx-MK64FX512/m-p/1569171#M64445</guid>
      <dc:creator>jrozsnaki</dc:creator>
      <dc:date>2022-12-13T21:04:38Z</dc:date>
    </item>
    <item>
      <title>Re: Flexcan Tx/Rx - MK64FX512</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Flexcan-Tx-Rx-MK64FX512/m-p/1570134#M64464</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;This case is a clone, and I will be following your case in the other, if you have any questions, please redirect to that.&lt;/P&gt;
&lt;P&gt;Best regards,&lt;BR /&gt;Pavel&lt;/P&gt;</description>
      <pubDate>Thu, 15 Dec 2022 03:52:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Flexcan-Tx-Rx-MK64FX512/m-p/1570134#M64464</guid>
      <dc:creator>Pavel_Hernandez</dc:creator>
      <dc:date>2022-12-15T03:52:33Z</dc:date>
    </item>
  </channel>
</rss>