<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Microcontrollers中的主题 Watchdog for S9KEAZN8</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Watchdog-for-S9KEAZN8/m-p/1568912#M64442</link>
    <description>&lt;P&gt;&lt;SPAN&gt;Hello,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;Does the Watchdog of S9KEAZN8 have the following features?&lt;/P&gt;&lt;P&gt;1. No dependence between watchdog time base and controller time base.&lt;BR /&gt;2. The watchdog is activated automatically.&lt;BR /&gt;3. It must not be possible to stop or reconfigure the watchdog outside the&lt;BR /&gt;4. Initialization phase of the watchdog.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks for your help.&lt;/P&gt;&lt;P&gt;Johns&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Tue, 13 Dec 2022 09:24:17 GMT</pubDate>
    <dc:creator>johns_chuang</dc:creator>
    <dc:date>2022-12-13T09:24:17Z</dc:date>
    <item>
      <title>Watchdog for S9KEAZN8</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Watchdog-for-S9KEAZN8/m-p/1568912#M64442</link>
      <description>&lt;P&gt;&lt;SPAN&gt;Hello,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;Does the Watchdog of S9KEAZN8 have the following features?&lt;/P&gt;&lt;P&gt;1. No dependence between watchdog time base and controller time base.&lt;BR /&gt;2. The watchdog is activated automatically.&lt;BR /&gt;3. It must not be possible to stop or reconfigure the watchdog outside the&lt;BR /&gt;4. Initialization phase of the watchdog.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks for your help.&lt;/P&gt;&lt;P&gt;Johns&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 13 Dec 2022 09:24:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Watchdog-for-S9KEAZN8/m-p/1568912#M64442</guid>
      <dc:creator>johns_chuang</dc:creator>
      <dc:date>2022-12-13T09:24:17Z</dc:date>
    </item>
    <item>
      <title>Re: Watchdog for S9KEAZN8</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Watchdog-for-S9KEAZN8/m-p/1569924#M64458</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/81923"&gt;@johns_chuang&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;1. Watchdog timer works independently, it has an independent 1kHz oscillator.&lt;/P&gt;
&lt;P&gt;2. Yes, Watchdog timer is inabled immediatley but it is disbaled during debug mode.&lt;/P&gt;
&lt;P&gt;3 &amp;amp; 4? WDOG_CS1[UPDATE] could allow updates on the configuration without forcing a reset on the mcu.&lt;/P&gt;
&lt;P&gt;You can find more information on chapter 16 of the reference manual.&lt;/P&gt;
&lt;P&gt;Let me know if this answers your questions.&lt;/P&gt;
&lt;P&gt;Best Regards, Miguel.&lt;/P&gt;</description>
      <pubDate>Wed, 14 Dec 2022 18:22:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Watchdog-for-S9KEAZN8/m-p/1569924#M64458</guid>
      <dc:creator>Miguel04</dc:creator>
      <dc:date>2022-12-14T18:22:17Z</dc:date>
    </item>
    <item>
      <title>Re: Watchdog for S9KEAZN8</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Watchdog-for-S9KEAZN8/m-p/1570075#M64463</link>
      <description>&lt;P&gt;Hi Miguel&lt;/P&gt;&lt;P&gt;Thanks for your reply, it's very helpful for me.&lt;/P&gt;&lt;P&gt;Johns&lt;/P&gt;</description>
      <pubDate>Thu, 15 Dec 2022 02:00:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Watchdog-for-S9KEAZN8/m-p/1570075#M64463</guid>
      <dc:creator>johns_chuang</dc:creator>
      <dc:date>2022-12-15T02:00:49Z</dc:date>
    </item>
  </channel>
</rss>