<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックWhat should be the reason for getting timeout error while pinging in MQX 4.1?</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/What-should-be-the-reason-for-getting-timeout-error-while/m-p/1562747#M64380</link>
    <description>&lt;P&gt;We are using the&amp;nbsp;&lt;SPAN&gt;TWR-K70F12M dev board with MQX 4.1 where we are developing an application in which we are giving two options to the user as follows,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;1)SNMP&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;2) Webpage&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;For the implementation of the same, we referred to the below link&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;U&gt;&lt;STRONG&gt;&lt;A href="https://community.nxp.com/t5/MQX-Software-Solutions/MQX-RTCS/m-p/1009894" target="_blank" rel="noopener"&gt;https://community.nxp.com/t5/MQX-Software-Solutions/MQX-RTCS/m-p/1009894&lt;/A&gt;&lt;/STRONG&gt;&lt;/U&gt;&lt;/P&gt;&lt;P&gt;We followed the procedure mentioned in the above link. But, after implementation, we observed that whenever we try to ping the board timeout errors are coming frequently.&lt;/P&gt;&lt;P&gt;As in our application webpage is playing the main role we cannot afford this pinging issue.&lt;BR /&gt;&lt;BR /&gt;How we can solve this issue? any help will be really appreciated.&lt;/P&gt;</description>
    <pubDate>Thu, 01 Dec 2022 10:03:19 GMT</pubDate>
    <dc:creator>omkardixit</dc:creator>
    <dc:date>2022-12-01T10:03:19Z</dc:date>
    <item>
      <title>What should be the reason for getting timeout error while pinging in MQX 4.1?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/What-should-be-the-reason-for-getting-timeout-error-while/m-p/1562747#M64380</link>
      <description>&lt;P&gt;We are using the&amp;nbsp;&lt;SPAN&gt;TWR-K70F12M dev board with MQX 4.1 where we are developing an application in which we are giving two options to the user as follows,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;1)SNMP&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;2) Webpage&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;For the implementation of the same, we referred to the below link&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;U&gt;&lt;STRONG&gt;&lt;A href="https://community.nxp.com/t5/MQX-Software-Solutions/MQX-RTCS/m-p/1009894" target="_blank" rel="noopener"&gt;https://community.nxp.com/t5/MQX-Software-Solutions/MQX-RTCS/m-p/1009894&lt;/A&gt;&lt;/STRONG&gt;&lt;/U&gt;&lt;/P&gt;&lt;P&gt;We followed the procedure mentioned in the above link. But, after implementation, we observed that whenever we try to ping the board timeout errors are coming frequently.&lt;/P&gt;&lt;P&gt;As in our application webpage is playing the main role we cannot afford this pinging issue.&lt;BR /&gt;&lt;BR /&gt;How we can solve this issue? any help will be really appreciated.&lt;/P&gt;</description>
      <pubDate>Thu, 01 Dec 2022 10:03:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/What-should-be-the-reason-for-getting-timeout-error-while/m-p/1562747#M64380</guid>
      <dc:creator>omkardixit</dc:creator>
      <dc:date>2022-12-01T10:03:19Z</dc:date>
    </item>
    <item>
      <title>Re: What should be the reason for getting timeout error while pinging in MQX 4.1?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/What-should-be-the-reason-for-getting-timeout-error-while/m-p/1565649#M64400</link>
      <description>&lt;P&gt;Hi Omkardixit:&lt;/P&gt;
&lt;P&gt;Not sure your problem, but for TWR-K70120M board, it is important to know that plug both the processor and the serial board (TWR-SER) into the TOWER.&amp;nbsp; The processor should&amp;nbsp; use the external clock from the Ethernet PHY on the serial board . If not, there is a possibility to loose eth packets.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;
&lt;P&gt;Daniel&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;
&lt;P&gt;Daniel&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 07 Dec 2022 06:39:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/What-should-be-the-reason-for-getting-timeout-error-while/m-p/1565649#M64400</guid>
      <dc:creator>danielchen</dc:creator>
      <dc:date>2022-12-07T06:39:10Z</dc:date>
    </item>
    <item>
      <title>Re: What should be the reason for getting timeout error while pinging in MQX 4.1?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/What-should-be-the-reason-for-getting-timeout-error-while/m-p/1568015#M64428</link>
      <description>&lt;P&gt;Hello danielchen&lt;/P&gt;&lt;P&gt;Thanks for the reply. Basically, we have made our own custom board where we are using&amp;nbsp;&lt;SPAN&gt;Ethernet PHY. Also, we have confirmed that the external clock is getting received.&amp;nbsp;&lt;BR /&gt;&lt;BR /&gt;Is there anything we need to change at the code level? for example in HTTP 1.0, the server always closes the connection after sending the response unless the client sent a &lt;EM&gt;&lt;STRONG&gt;Connection: keep-alive&lt;/STRONG&gt;&amp;nbsp;&lt;/EM&gt;request header and the server sent a&amp;nbsp;&lt;STRONG&gt;&lt;EM&gt;Connection: keep-alive.&amp;nbsp;&lt;/EM&gt;&lt;/STRONG&gt;So, if no such response header exists, the client must close its end of the connection after receiving a response.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;I'm guessing here because of this header, I'm facing a ping issue.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;So Is my understanding correct here? If so, then how we can implement the same header in the current MQX4.1 version?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Any help will be really appreciated!&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Omkar Dixit&lt;/P&gt;</description>
      <pubDate>Mon, 12 Dec 2022 07:06:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/What-should-be-the-reason-for-getting-timeout-error-while/m-p/1568015#M64428</guid>
      <dc:creator>omkardixit</dc:creator>
      <dc:date>2022-12-12T07:06:48Z</dc:date>
    </item>
  </channel>
</rss>