<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Missing FlexBus pins in MK53DX256CMD10 in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Missing-FlexBus-pins-in-MK53DX256CMD10/m-p/1556646#M64326</link>
    <description>&lt;P class="lia-align-justify"&gt;Hello &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/208878"&gt;@msmrecza&lt;/a&gt;,&lt;/P&gt;
&lt;P class="lia-align-justify"&gt;You can find the available signals to use for the FlexBus for the MK53DX256CMD10 in the User Manual, Datasheet and ConfigTools Pins.&lt;/P&gt;
&lt;P class="lia-align-justify"&gt;I would recommend you to try the following Application Note: &lt;A href="https://www.nxp.com/docs/en/application-note/AN4393.pdf" target="_blank"&gt;Using FlexBus Interface for Kinetis Microcontrollers&lt;/A&gt;, and verify if this works for your needs. Even though they are not using the K53, perhaps you might find it useful considering that it shows a couple of examples that don't use the FB_AD[23:21] signals.&lt;/P&gt;
&lt;P class="lia-align-justify"&gt;Best regards, Raul.&lt;/P&gt;</description>
    <pubDate>Fri, 18 Nov 2022 20:55:01 GMT</pubDate>
    <dc:creator>RaRo</dc:creator>
    <dc:date>2022-11-18T20:55:01Z</dc:date>
    <item>
      <title>Missing FlexBus pins in MK53DX256CMD10</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Missing-FlexBus-pins-in-MK53DX256CMD10/m-p/1555012#M64308</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I planned to use MK53DX256CMD10 and FlexBus communication with 32 AD lines (i.e. FB_AD[31:0]). The reference manual of the microcontroller describes everything as if the communication using 32 lines was possible. However, for some reason, the pinout is missing the signals FB_AD[23:21]. The package is 144-pin and pins PB6-PB8 are available (normally the FB lines should be at ALT5). Could you tell me if there is a mistake in the reference manual or if I am missing something?&lt;/P&gt;&lt;P&gt;Thank you in advance,&lt;/P&gt;&lt;P&gt;M.&lt;/P&gt;</description>
      <pubDate>Wed, 16 Nov 2022 15:37:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Missing-FlexBus-pins-in-MK53DX256CMD10/m-p/1555012#M64308</guid>
      <dc:creator>msmrecza</dc:creator>
      <dc:date>2022-11-16T15:37:42Z</dc:date>
    </item>
    <item>
      <title>Re: Missing FlexBus pins in MK53DX256CMD10</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Missing-FlexBus-pins-in-MK53DX256CMD10/m-p/1556646#M64326</link>
      <description>&lt;P class="lia-align-justify"&gt;Hello &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/208878"&gt;@msmrecza&lt;/a&gt;,&lt;/P&gt;
&lt;P class="lia-align-justify"&gt;You can find the available signals to use for the FlexBus for the MK53DX256CMD10 in the User Manual, Datasheet and ConfigTools Pins.&lt;/P&gt;
&lt;P class="lia-align-justify"&gt;I would recommend you to try the following Application Note: &lt;A href="https://www.nxp.com/docs/en/application-note/AN4393.pdf" target="_blank"&gt;Using FlexBus Interface for Kinetis Microcontrollers&lt;/A&gt;, and verify if this works for your needs. Even though they are not using the K53, perhaps you might find it useful considering that it shows a couple of examples that don't use the FB_AD[23:21] signals.&lt;/P&gt;
&lt;P class="lia-align-justify"&gt;Best regards, Raul.&lt;/P&gt;</description>
      <pubDate>Fri, 18 Nov 2022 20:55:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Missing-FlexBus-pins-in-MK53DX256CMD10/m-p/1556646#M64326</guid>
      <dc:creator>RaRo</dc:creator>
      <dc:date>2022-11-18T20:55:01Z</dc:date>
    </item>
    <item>
      <title>Re: Missing FlexBus pins in MK53DX256CMD10</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Missing-FlexBus-pins-in-MK53DX256CMD10/m-p/1556751#M64328</link>
      <description>&lt;P&gt;Hello &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/206649"&gt;@RaRo&lt;/a&gt;&amp;nbsp; and thank you for your answer.&lt;/P&gt;&lt;P&gt;In my case I am constrained by the application and I must use all 32 lines. Does it mean it is certain that the MK53DX256CMD10 doesn't have the 3 mentioned signals? I find it inconsistent with the rest of the documentation and some of your documents describing FlexBus in 144-pin packages though... Do you know if there is any particular reason for that?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;M.&lt;/P&gt;</description>
      <pubDate>Sun, 20 Nov 2022 21:04:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Missing-FlexBus-pins-in-MK53DX256CMD10/m-p/1556751#M64328</guid>
      <dc:creator>msmrecza</dc:creator>
      <dc:date>2022-11-20T21:04:45Z</dc:date>
    </item>
  </channel>
</rss>