<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: FRDM-K66F, Creating composite device of Audio Input Device (Plug and Play) and MSD (SD Card) in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-K66F-Creating-composite-device-of-Audio-Input-Device-Plug/m-p/1552260#M64290</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;In the SDK you can find examples for this but there is not a specific example with both, that is a solution you may to development combine the examples.&lt;/P&gt;
&lt;P&gt;Best regards,&lt;BR /&gt;Pavel&lt;/P&gt;</description>
    <pubDate>Thu, 10 Nov 2022 22:53:47 GMT</pubDate>
    <dc:creator>Pavel_Hernandez</dc:creator>
    <dc:date>2022-11-10T22:53:47Z</dc:date>
    <item>
      <title>FRDM-K66F, Creating composite device of Audio Input Device (Plug and Play) and MSD (SD Card)</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-K66F-Creating-composite-device-of-Audio-Input-Device-Plug/m-p/1549224#M64272</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I have a very high-level design question.&lt;/P&gt;&lt;P&gt;I would like to use the FRDM-K66F board in any one of the following options&lt;/P&gt;&lt;P&gt;1. User would be able to switch between one of the two functionalities of "audio input device" or "MSD Device" for SD Card with a (for eg.) press of a button&amp;nbsp;&lt;/P&gt;&lt;P&gt;2. Creating a composite device with both "audio input device" and "MSD device". I am afraid that having these two functionalities would affect the throughput in USB as one is Isochronout transfer and the other is bulk transfer.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Personally, I think the first method is very efficient and the user will be happy with the device's performance. However, I am wondering which is the quickest way to implement it with the available resources.&lt;/P&gt;&lt;P&gt;If anyone can please suggest which is the preferred or right method, and quickest method to implement?&lt;/P&gt;&lt;P&gt;I have gone through USB documentation that was available with the lastest SDK for FRDM-K66F board, but I am not sure where to start and how to proceed.&lt;/P&gt;&lt;P&gt;Please guide me in the direction to achieve both functionalities.&lt;/P&gt;&lt;P&gt;best regards,&lt;/P&gt;&lt;P&gt;Mahendran&lt;/P&gt;</description>
      <pubDate>Sun, 06 Nov 2022 11:25:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-K66F-Creating-composite-device-of-Audio-Input-Device-Plug/m-p/1549224#M64272</guid>
      <dc:creator>mahendranmanoha</dc:creator>
      <dc:date>2022-11-06T11:25:47Z</dc:date>
    </item>
    <item>
      <title>Re: FRDM-K66F, Creating composite device of Audio Input Device (Plug and Play) and MSD (SD Card)</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-K66F-Creating-composite-device-of-Audio-Input-Device-Plug/m-p/1552260#M64290</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;In the SDK you can find examples for this but there is not a specific example with both, that is a solution you may to development combine the examples.&lt;/P&gt;
&lt;P&gt;Best regards,&lt;BR /&gt;Pavel&lt;/P&gt;</description>
      <pubDate>Thu, 10 Nov 2022 22:53:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-K66F-Creating-composite-device-of-Audio-Input-Device-Plug/m-p/1552260#M64290</guid>
      <dc:creator>Pavel_Hernandez</dc:creator>
      <dc:date>2022-11-10T22:53:47Z</dc:date>
    </item>
    <item>
      <title>Re: FRDM-K66F, Creating composite device of Audio Input Device (Plug and Play) and MSD (SD Card)</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-K66F-Creating-composite-device-of-Audio-Input-Device-Plug/m-p/1552728#M64294</link>
      <description>&lt;P&gt;Thank you Pavel,&lt;/P&gt;&lt;P&gt;Earlier, I have gone through the code examples and assumed that my requirement needs to be developed. I want to thank you for confirming it.&amp;nbsp;&lt;/P&gt;&lt;P&gt;best regards,&lt;/P&gt;&lt;P&gt;Mahendran&lt;/P&gt;</description>
      <pubDate>Fri, 11 Nov 2022 20:46:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-K66F-Creating-composite-device-of-Audio-Input-Device-Plug/m-p/1552728#M64294</guid>
      <dc:creator>mahendranmanoha</dc:creator>
      <dc:date>2022-11-11T20:46:44Z</dc:date>
    </item>
  </channel>
</rss>