<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Microcontrollers中的主题 Re: FRDM-KL25Z not working anymore</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-KL25Z-not-working-anymore/m-p/245442#M6423</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Did you have the USB connected at the same time as the 4.8V? Is it possible that the USB was trying to supply power to the 4.8V supply?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Was the 4.8V connected to the 5-9V in (J9p16) or the 5V USB out (J9p10)? If to J9p10, I would expect smoke because the USB 5V would be trying to drive the 4.8 V power supply which would likely be clamping (shorting) the 5 V to ground to get it back to 4.8V.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;OR, even though you had connected both sources previously without incident, it is quite possible that previously you had connected the 4.8 V first and then the USB which would cause the FRDM to run on the 4.8V. But the last time you connected the USB then the 4.8V which would cause the USB to supply the FRDM and perhaps then try to drive the 4.8V PS higher. (Or visa versa.)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt; If that is not the problem, make sure you know how your 3.3 V supply is being used.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I got smoke from a FRDM-KL25Z once when I connected an external switch incorrectly and, evidently, shorted 3V3 to ground. Believe it or not, after connecting things correctly, the board still worked.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Another time, after an interface board redesign, the device I was building worked for a few minutes, then D2 on the KL25Z board blew up. That is the diode that supplies 3V3. Evidently, the interface board drew too much current, or the 3V3 was unhappy about something else (perhaps those durn switches again). ;-(&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Another possibility, might be that you had two USB cables connected from two different devices and they did not have a common ground. That might also allow current to turn to smoke and escape the board forever. ;-)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Obviously, you were drawing too much current somehow. Is it easier to try to solve that problem or move on to a better design?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;G'luck.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 13 Aug 2013 17:11:12 GMT</pubDate>
    <dc:creator>injunear1</dc:creator>
    <dc:date>2013-08-13T17:11:12Z</dc:date>
    <item>
      <title>FRDM-KL25Z not working anymore</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-KL25Z-not-working-anymore/m-p/245441#M6422</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN lang="en"&gt;&lt;SPAN class="hps"&gt;Hello&lt;/SPAN&gt;!&lt;BR /&gt;&lt;SPAN class="hps"&gt;So today&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;I&lt;/SPAN&gt; turn on &lt;SPAN class="hps"&gt;my&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;freedom&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;board&lt;/SPAN&gt; via vin/gnd pins with 4,8V &lt;SPAN class="hps"&gt;and noticed a&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;smoke coming out&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;near the&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;reset button&lt;/SPAN&gt;, I &lt;SPAN class="hps"&gt;immediately&lt;/SPAN&gt; turned off &lt;SPAN class="hps"&gt;and tried&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;turn on again,&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;this time&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;via USB&lt;/SPAN&gt;, &lt;SPAN class="hps"&gt;but without success.&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;Any tips&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;on which component&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;may have been damaged&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;and how can I&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;verify this&lt;/SPAN&gt;&lt;SPAN&gt;?&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN lang="en"&gt;&lt;SPAN&gt;&lt;SPAN class="short_text" lang="en"&gt;&lt;SPAN class="hps"&gt;I've done that&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;before and&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;it worked&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;well&lt;/SPAN&gt;.&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN lang="en"&gt;&lt;SPAN&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN lang="en"&gt;&lt;SPAN&gt;Thanks.&lt;BR /&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 07 Aug 2013 23:26:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-KL25Z-not-working-anymore/m-p/245441#M6422</guid>
      <dc:creator>cardoso</dc:creator>
      <dc:date>2013-08-07T23:26:03Z</dc:date>
    </item>
    <item>
      <title>Re: FRDM-KL25Z not working anymore</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-KL25Z-not-working-anymore/m-p/245442#M6423</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Did you have the USB connected at the same time as the 4.8V? Is it possible that the USB was trying to supply power to the 4.8V supply?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Was the 4.8V connected to the 5-9V in (J9p16) or the 5V USB out (J9p10)? If to J9p10, I would expect smoke because the USB 5V would be trying to drive the 4.8 V power supply which would likely be clamping (shorting) the 5 V to ground to get it back to 4.8V.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;OR, even though you had connected both sources previously without incident, it is quite possible that previously you had connected the 4.8 V first and then the USB which would cause the FRDM to run on the 4.8V. But the last time you connected the USB then the 4.8V which would cause the USB to supply the FRDM and perhaps then try to drive the 4.8V PS higher. (Or visa versa.)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt; If that is not the problem, make sure you know how your 3.3 V supply is being used.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I got smoke from a FRDM-KL25Z once when I connected an external switch incorrectly and, evidently, shorted 3V3 to ground. Believe it or not, after connecting things correctly, the board still worked.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Another time, after an interface board redesign, the device I was building worked for a few minutes, then D2 on the KL25Z board blew up. That is the diode that supplies 3V3. Evidently, the interface board drew too much current, or the 3V3 was unhappy about something else (perhaps those durn switches again). ;-(&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Another possibility, might be that you had two USB cables connected from two different devices and they did not have a common ground. That might also allow current to turn to smoke and escape the board forever. ;-)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Obviously, you were drawing too much current somehow. Is it easier to try to solve that problem or move on to a better design?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;G'luck.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 13 Aug 2013 17:11:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-KL25Z-not-working-anymore/m-p/245442#M6423</guid>
      <dc:creator>injunear1</dc:creator>
      <dc:date>2013-08-13T17:11:12Z</dc:date>
    </item>
    <item>
      <title>Re: FRDM-KL25Z not working anymore</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-KL25Z-not-working-anymore/m-p/245443#M6424</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, &lt;/P&gt;&lt;P&gt;The USB was not connected at same time. The 4.8V was connected to the 5-9V in J9p16. I believe that some short occurred when I turn it on.&lt;/P&gt;&lt;P&gt;I'll check some components and do a better design!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 14 Aug 2013 15:54:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-KL25Z-not-working-anymore/m-p/245443#M6424</guid>
      <dc:creator>cardoso</dc:creator>
      <dc:date>2013-08-14T15:54:08Z</dc:date>
    </item>
    <item>
      <title>Re: FRDM-KL25Z not working anymore</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-KL25Z-not-working-anymore/m-p/245444#M6425</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Ok, after a long time I found that D2 is open between 1(anode) to 3(cathode), bypassing it I get the frdm working again, but I know this is not safe. Any suggestion on how to fix this? Replacing this component it's not trivial for me, or can I replace by non SMD component?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;&lt;P class="page" title="Page 6"&gt;&amp;nbsp; &lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/40337i17CE3E91EB688E1E/image-size/large?v=v2&amp;amp;px=999" title="diodes.png" alt="diodes.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 06 Sep 2013 16:29:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-KL25Z-not-working-anymore/m-p/245444#M6425</guid>
      <dc:creator>cardoso</dc:creator>
      <dc:date>2013-09-06T16:29:58Z</dc:date>
    </item>
  </channel>
</rss>