<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic K60F120M (120MHz) controller in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K60F120M-120MHz-controller/m-p/245398#M6420</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm using &lt;STRONG&gt;K60F120M (120MHz)&lt;/STRONG&gt; controller, a sram device is connected to the spi1 interface. I use the spi driver example code to access to the sram via dma. But I don't see at all a clock or data on the pins.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Has somebody tried the spi driver?&lt;/P&gt;&lt;P&gt;What could be the reason for that?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;regards&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 05 Dec 2013 11:06:11 GMT</pubDate>
    <dc:creator>pet</dc:creator>
    <dc:date>2013-12-05T11:06:11Z</dc:date>
    <item>
      <title>K60F120M (120MHz) controller</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K60F120M-120MHz-controller/m-p/245398#M6420</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm using &lt;STRONG&gt;K60F120M (120MHz)&lt;/STRONG&gt; controller, a sram device is connected to the spi1 interface. I use the spi driver example code to access to the sram via dma. But I don't see at all a clock or data on the pins.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Has somebody tried the spi driver?&lt;/P&gt;&lt;P&gt;What could be the reason for that?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;regards&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 05 Dec 2013 11:06:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K60F120M-120MHz-controller/m-p/245398#M6420</guid>
      <dc:creator>pet</dc:creator>
      <dc:date>2013-12-05T11:06:11Z</dc:date>
    </item>
    <item>
      <title>Re: K60F120M (120MHz) controller</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K60F120M-120MHz-controller/m-p/245399#M6421</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Please refer Kinetis 120MHz example code with below link, which provides DSPI example code.&lt;/P&gt;&lt;P&gt;KINETIS_120MHZ_SC&amp;nbsp; (Kinetis 120MHz bare metal sample code) : &lt;/P&gt;&lt;P&gt;&lt;A href="http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=TWR-K70F120M&amp;amp;fpsp=1&amp;amp;tab=Design_Tools_Tab" title="http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=TWR-K70F120M&amp;amp;fpsp=1&amp;amp;tab=Design_Tools_Tab"&gt;TWR-K70F120M: Kinetis K70 120 MHz Tower System Module&lt;/A&gt;&lt;/P&gt;&lt;P&gt;Wish it helps.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 09 Dec 2013 08:02:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K60F120M-120MHz-controller/m-p/245399#M6421</guid>
      <dc:creator>Hui_Ma</dc:creator>
      <dc:date>2013-12-09T08:02:16Z</dc:date>
    </item>
  </channel>
</rss>