<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックRe: KL17 RTC high drift</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL17-RTC-high-drift/m-p/1512637#M63899</link>
    <description>&lt;P&gt;I must admit that I can't think of another clue that could cause the drift that isn't mentioned in the aforementioned application note and the recommendations in section &lt;EM&gt;28.6 External Crystal / Resonator Connections&lt;/EM&gt; of the &lt;A href="https://www.nxp.com/webapp/Download?colCode=KL17P64M48SF6RM" target="_blank" rel="noopener"&gt;reference manual&lt;/A&gt;.&lt;/P&gt;
&lt;P&gt;Now, if you can no longer optimize the oscillator design, you could try to increase reliability through software, for more information about this, please refer to section &lt;EM&gt;32.4.3 Compensation&lt;/EM&gt; of the reference manual. Also application note &lt;A href="https://www.nxp.com/docs/en/application-note/AN4949.pdf" target="_blank" rel="noopener"&gt;AN4949&lt;/A&gt; can serve as a reference.&lt;/P&gt;</description>
    <pubDate>Fri, 26 Aug 2022 22:34:04 GMT</pubDate>
    <dc:creator>_Leo_</dc:creator>
    <dc:date>2022-08-26T22:34:04Z</dc:date>
    <item>
      <title>KL17 RTC high drift</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL17-RTC-high-drift/m-p/1507690#M63840</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I have a 32,768kHz +/-20ppm 12pF load cap crystal in my two custom boards. In both PCB the RTC drifts aproximatelly +120s/week. That yields +200ppm if I am not mistaken, which is quite high.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;SC8P and SC4P fields of the OSC_CR register are enable using the Clocks Config tool on MCUXpresso.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="AndreVB_0-1660759807775.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/190523iA8DFD6F4748A81F9/image-size/medium?v=v2&amp;amp;px=400" role="button" title="AndreVB_0-1660759807775.png" alt="AndreVB_0-1660759807775.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;I noticed RTC_CR is disable. Is that correct?&lt;/P&gt;&lt;P&gt;I understand that enabling&amp;nbsp;&lt;SPAN&gt;SC8P and SC4P the oscillator block will add 24pF on EXTAL and 24pF on XTAL pins, correct? Besides, the crystal is 1mm far from the XTAL/EXTAL pins of the MCU (see next).&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="AndreVB_1-1660762020044.png" style="width: 233px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/190526i18F6FFDB4F41BB2E/image-dimensions/233x189?v=v2" width="233" height="189" role="button" title="AndreVB_1-1660762020044.png" alt="AndreVB_1-1660762020044.png" /&gt;&lt;/span&gt;&amp;nbsp;below and to the right of the crystal is GND, above is RESET pin.&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;PCB is at room temperature all the time. That said, if the&amp;nbsp;OSC_CR setup is correct, any idea what could be causing such high drift?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Thank you very in advance.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Best regards,&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;Andre VB&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 17 Aug 2022 18:57:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL17-RTC-high-drift/m-p/1507690#M63840</guid>
      <dc:creator>AndreVB</dc:creator>
      <dc:date>2022-08-17T18:57:09Z</dc:date>
    </item>
    <item>
      <title>Re: KL17 RTC high drift</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL17-RTC-high-drift/m-p/1510336#M63874</link>
      <description>&lt;P&gt;Thank you so much for your interest in our products and for using our community.&lt;/P&gt;
&lt;P&gt;For that we have an application note that could help you. Please refer to "Crystal Oscillator Troubleshooting Guide" (&lt;A href="https://www.nxp.com/docs/en/application-note/AN3208.pdf" target="_blank" rel="noopener"&gt;AN3208&lt;/A&gt;).&lt;/P&gt;
&lt;P&gt;Hope it helps you. Please let me know if you have more questions about it.&lt;/P&gt;
&lt;P&gt;Have a nice day!&lt;/P&gt;</description>
      <pubDate>Tue, 23 Aug 2022 17:31:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL17-RTC-high-drift/m-p/1510336#M63874</guid>
      <dc:creator>_Leo_</dc:creator>
      <dc:date>2022-08-23T17:31:34Z</dc:date>
    </item>
    <item>
      <title>Re: KL17 RTC high drift</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL17-RTC-high-drift/m-p/1511738#M63884</link>
      <description>&lt;P&gt;Thank you for your reply. The AN describes many potential problems but for Kinetics KL devices, as log as the low frequency crystal is close to the I/Os, the load capacitance is correct, and the crystal far from other noisy signals, it seems there is not much to do about it. I was also very careful in soldering the crystal.&amp;nbsp;&lt;/P&gt;&lt;P&gt;The drift is very high. I have used a RTL code example from KL27 as starting point.&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;If you have any clue of what could cause the drift, please share.&lt;/P&gt;&lt;P&gt;Thank you,&lt;/P&gt;&lt;P&gt;Andre&lt;/P&gt;</description>
      <pubDate>Thu, 25 Aug 2022 12:06:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL17-RTC-high-drift/m-p/1511738#M63884</guid>
      <dc:creator>AndreVB</dc:creator>
      <dc:date>2022-08-25T12:06:55Z</dc:date>
    </item>
    <item>
      <title>Re: KL17 RTC high drift</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL17-RTC-high-drift/m-p/1512637#M63899</link>
      <description>&lt;P&gt;I must admit that I can't think of another clue that could cause the drift that isn't mentioned in the aforementioned application note and the recommendations in section &lt;EM&gt;28.6 External Crystal / Resonator Connections&lt;/EM&gt; of the &lt;A href="https://www.nxp.com/webapp/Download?colCode=KL17P64M48SF6RM" target="_blank" rel="noopener"&gt;reference manual&lt;/A&gt;.&lt;/P&gt;
&lt;P&gt;Now, if you can no longer optimize the oscillator design, you could try to increase reliability through software, for more information about this, please refer to section &lt;EM&gt;32.4.3 Compensation&lt;/EM&gt; of the reference manual. Also application note &lt;A href="https://www.nxp.com/docs/en/application-note/AN4949.pdf" target="_blank" rel="noopener"&gt;AN4949&lt;/A&gt; can serve as a reference.&lt;/P&gt;</description>
      <pubDate>Fri, 26 Aug 2022 22:34:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL17-RTC-high-drift/m-p/1512637#M63899</guid>
      <dc:creator>_Leo_</dc:creator>
      <dc:date>2022-08-26T22:34:04Z</dc:date>
    </item>
  </channel>
</rss>