<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic FRDM-K22F to K22FX512VLH12 USB Support in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-K22F-to-K22FX512VLH12-USB-Support/m-p/1509040#M63861</link>
    <description>&lt;P&gt;I have run a few sample applications on the FRDM-K22F with success, now I"m moving to my custom board using a MK22FX512VLH12 (has CAN which I need)&lt;/P&gt;&lt;P&gt;I copied code from the Blinky LED sample for the K22F and moved it to my fresh project, edited the code to use my ports PTB0-2 for my boards LED's. flashed the image and played with it for a bit. it worked great.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;For my next test, I loaded the K22F Host USB keyboard and mouse demo to the K22F and got it working on the K22F board. I then changed the target MCU to the K22FX512VLH12,&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;What is the best way to get the USB demo working on my board?&lt;/P&gt;&lt;P&gt;I can't seem to find documentation on the USB operation using the SDK. Any help would be appreciated.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Sun, 21 Aug 2022 16:42:56 GMT</pubDate>
    <dc:creator>stevenlutz</dc:creator>
    <dc:date>2022-08-21T16:42:56Z</dc:date>
    <item>
      <title>FRDM-K22F to K22FX512VLH12 USB Support</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-K22F-to-K22FX512VLH12-USB-Support/m-p/1509040#M63861</link>
      <description>&lt;P&gt;I have run a few sample applications on the FRDM-K22F with success, now I"m moving to my custom board using a MK22FX512VLH12 (has CAN which I need)&lt;/P&gt;&lt;P&gt;I copied code from the Blinky LED sample for the K22F and moved it to my fresh project, edited the code to use my ports PTB0-2 for my boards LED's. flashed the image and played with it for a bit. it worked great.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;For my next test, I loaded the K22F Host USB keyboard and mouse demo to the K22F and got it working on the K22F board. I then changed the target MCU to the K22FX512VLH12,&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;What is the best way to get the USB demo working on my board?&lt;/P&gt;&lt;P&gt;I can't seem to find documentation on the USB operation using the SDK. Any help would be appreciated.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Sun, 21 Aug 2022 16:42:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-K22F-to-K22FX512VLH12-USB-Support/m-p/1509040#M63861</guid>
      <dc:creator>stevenlutz</dc:creator>
      <dc:date>2022-08-21T16:42:56Z</dc:date>
    </item>
  </channel>
</rss>