<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Microcontrollers中的主题 Re: KV11z-DAC</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KV11z-DAC/m-p/1496506#M63670</link>
    <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/204016"&gt;@CMooN&lt;/a&gt;,&lt;/P&gt;&lt;P&gt;In the SDK example, there is a toggle function called "LED_TOGGLE" under the interrupt "LPTMR_LED_HANDLER", this is what controls the LED in each interrupt. In your case, you would need to implement the application you want to do with PTE30 inside this interrupt handler.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best regards, Julian&lt;/P&gt;</description>
    <pubDate>Wed, 27 Jul 2022 15:54:12 GMT</pubDate>
    <dc:creator>Julián_AragónM</dc:creator>
    <dc:date>2022-07-27T15:54:12Z</dc:date>
    <item>
      <title>KV11z-DAC</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KV11z-DAC/m-p/1494876#M63631</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;Can someone help me about how can I create a periodic interrupt timer for KV11z ? I am using dac_basic.c. I want to increase a voltage from 0V to 3.3V with 100mV increase for each 100ms.&lt;/P&gt;</description>
      <pubDate>Mon, 25 Jul 2022 14:02:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KV11z-DAC/m-p/1494876#M63631</guid>
      <dc:creator>CMooN</dc:creator>
      <dc:date>2022-07-25T14:02:04Z</dc:date>
    </item>
    <item>
      <title>Re: KV11z-DAC</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KV11z-DAC/m-p/1495672#M63647</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/204016"&gt;@CMooN&lt;/a&gt;,&lt;/P&gt;&lt;P&gt;There is an application of the Low-Power Timer in the KV11Z SDK called "lptmr" under "driver_examples", which show how to use the timer. I hope you find that example useful.&lt;/P&gt;&lt;P&gt;For the specific time interval, I suggest you also take a look at this guide for the PIT modules:&amp;nbsp;&lt;A href="https://www.nxp.com/docs/en/supporting-information/Periodic-Interrupt-Timer-Training.pdf" target="_blank"&gt;https://www.nxp.com/docs/en/supporting-information/Periodic-Interrupt-Timer-Training.pdf&lt;/A&gt;&lt;/P&gt;</description>
      <pubDate>Tue, 26 Jul 2022 14:45:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KV11z-DAC/m-p/1495672#M63647</guid>
      <dc:creator>Julián_AragónM</dc:creator>
      <dc:date>2022-07-26T14:45:22Z</dc:date>
    </item>
    <item>
      <title>Re: KV11z-DAC</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KV11z-DAC/m-p/1496144#M63660</link>
      <description>&lt;P&gt;Hi Julian,&lt;/P&gt;&lt;P&gt;Thanks for your answer. In lptmr, the LED is controlled. But, in my project, I want to control different pin which is PTE30. Can you help me how can I built the configuration ?&lt;/P&gt;</description>
      <pubDate>Wed, 27 Jul 2022 07:04:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KV11z-DAC/m-p/1496144#M63660</guid>
      <dc:creator>CMooN</dc:creator>
      <dc:date>2022-07-27T07:04:28Z</dc:date>
    </item>
    <item>
      <title>Re: KV11z-DAC</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KV11z-DAC/m-p/1496506#M63670</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/204016"&gt;@CMooN&lt;/a&gt;,&lt;/P&gt;&lt;P&gt;In the SDK example, there is a toggle function called "LED_TOGGLE" under the interrupt "LPTMR_LED_HANDLER", this is what controls the LED in each interrupt. In your case, you would need to implement the application you want to do with PTE30 inside this interrupt handler.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best regards, Julian&lt;/P&gt;</description>
      <pubDate>Wed, 27 Jul 2022 15:54:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KV11z-DAC/m-p/1496506#M63670</guid>
      <dc:creator>Julián_AragónM</dc:creator>
      <dc:date>2022-07-27T15:54:12Z</dc:date>
    </item>
  </channel>
</rss>