<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックCannot connect to  via FRDM-KL27using blhost</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Cannot-connect-to-via-FRDM-KL27using-blhost/m-p/1496358#M63664</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;My understanding is that the built in ROM contains an image of KBOOT on the FRDM-KL27Z.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;My overall goal is to configure the KL27 on the FRDM-KL27Z to boot and UART/I2C flash on the dev board. I am following and adapting the steps listed in &lt;STRONG&gt;MCUBLHOSTUG&lt;/STRONG&gt; (blhost User's Guide) and&amp;nbsp;&lt;STRONG&gt;Getting Started with the MCU Flashloader&lt;/STRONG&gt; to the KL27 however all attempts to have the KL27 communicate with blhost is unsuccessful.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;My procedure is as follows:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;1. FRDM-KL27Z is powered thru the SDA USB port (next to SW1) and running an LED color cycling app from internal flash). FOPT is configured via the FlashConfigBlock to:&lt;/P&gt;&lt;P&gt;2. Press and hold SW2 (NMI), then press SW1 (Reset)&lt;/P&gt;&lt;P&gt;3. Release SW1, then release SW2&lt;/P&gt;&lt;P&gt;4. Attempt to connect to the board via blhost.exe. I downloaded the version included with NXP Kinetis Bootloader 2.0.0&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;syntax:&lt;/P&gt;&lt;P&gt;blhost.exe -p com19 -- get-property 1&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Error: Initial ping failure: No response received for ping command.&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Any suggestions on what else I can try to connect, or perhaps an explanation as to what I'm missing from my setup would be greatly appreciated.&lt;/P&gt;</description>
    <pubDate>Wed, 27 Jul 2022 12:06:13 GMT</pubDate>
    <dc:creator>Ravikumar1</dc:creator>
    <dc:date>2022-07-27T12:06:13Z</dc:date>
    <item>
      <title>Cannot connect to  via FRDM-KL27using blhost</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Cannot-connect-to-via-FRDM-KL27using-blhost/m-p/1496358#M63664</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;My understanding is that the built in ROM contains an image of KBOOT on the FRDM-KL27Z.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;My overall goal is to configure the KL27 on the FRDM-KL27Z to boot and UART/I2C flash on the dev board. I am following and adapting the steps listed in &lt;STRONG&gt;MCUBLHOSTUG&lt;/STRONG&gt; (blhost User's Guide) and&amp;nbsp;&lt;STRONG&gt;Getting Started with the MCU Flashloader&lt;/STRONG&gt; to the KL27 however all attempts to have the KL27 communicate with blhost is unsuccessful.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;My procedure is as follows:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;1. FRDM-KL27Z is powered thru the SDA USB port (next to SW1) and running an LED color cycling app from internal flash). FOPT is configured via the FlashConfigBlock to:&lt;/P&gt;&lt;P&gt;2. Press and hold SW2 (NMI), then press SW1 (Reset)&lt;/P&gt;&lt;P&gt;3. Release SW1, then release SW2&lt;/P&gt;&lt;P&gt;4. Attempt to connect to the board via blhost.exe. I downloaded the version included with NXP Kinetis Bootloader 2.0.0&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;syntax:&lt;/P&gt;&lt;P&gt;blhost.exe -p com19 -- get-property 1&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Error: Initial ping failure: No response received for ping command.&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Any suggestions on what else I can try to connect, or perhaps an explanation as to what I'm missing from my setup would be greatly appreciated.&lt;/P&gt;</description>
      <pubDate>Wed, 27 Jul 2022 12:06:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Cannot-connect-to-via-FRDM-KL27using-blhost/m-p/1496358#M63664</guid>
      <dc:creator>Ravikumar1</dc:creator>
      <dc:date>2022-07-27T12:06:13Z</dc:date>
    </item>
    <item>
      <title>Re: Cannot connect to  via FRDM-KL27using blhost</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Cannot-connect-to-via-FRDM-KL27using-blhost/m-p/1497569#M63690</link>
      <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/200204"&gt;@Ravikumar1&lt;/a&gt; , you can check this excellent blog &lt;A href="https://mcuoneclipse.com/2018/03/05/tutorial-crc32-checksum-with-the-kboot-bootloader/" target="_blank"&gt;https://mcuoneclipse.com/2018/03/05/tutorial-crc32-checksum-with-the-kboot-bootloader/&amp;nbsp;&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&lt;A href="https://mcuoneclipse.com/2017/07/12/getting-started-rom-bootloader-on-the-nxp-frdm-kl03z-board/" target="_blank"&gt;https://mcuoneclipse.com/2017/07/12/getting-started-rom-bootloader-on-the-nxp-frdm-kl03z-board/&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Have a good day&lt;/P&gt;</description>
      <pubDate>Thu, 28 Jul 2022 23:40:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Cannot-connect-to-via-FRDM-KL27using-blhost/m-p/1497569#M63690</guid>
      <dc:creator>CarlosGarabito</dc:creator>
      <dc:date>2022-07-28T23:40:50Z</dc:date>
    </item>
    <item>
      <title>Re: Cannot connect to  via FRDM-KL27using blhost</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Cannot-connect-to-via-FRDM-KL27using-blhost/m-p/1500753#M63737</link>
      <description>&lt;P&gt;Thank you,&lt;/P&gt;&lt;P&gt;Its resolved my problem&lt;/P&gt;</description>
      <pubDate>Thu, 04 Aug 2022 04:25:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Cannot-connect-to-via-FRDM-KL27using-blhost/m-p/1500753#M63737</guid>
      <dc:creator>Ravikumar1</dc:creator>
      <dc:date>2022-08-04T04:25:08Z</dc:date>
    </item>
  </channel>
</rss>