<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックKV58 CANBUS Communication</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KV58-CANBUS-Communication/m-p/1496356#M63663</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I am using KV58&amp;nbsp; CANBUS to communicate the ESP32 CANBUS(Support ISO 11898-1).&lt;/P&gt;&lt;P&gt;1) When I try the communication between ESP32 board, it works fine.&lt;/P&gt;&lt;P&gt;2) When I try KV58 with K64F CANBUS, it works fine as well.&lt;/P&gt;&lt;P&gt;3) Then, I try KV58 CANBUS with ESP32, I cannot get it work. The difference between K64F CANBUS and ESP32 CANBUS is just MCU, all others(tranceiver, connection, and etc) are exactly same. I am wondering if it is related to timing settings?&lt;/P&gt;&lt;P&gt;Can anybody tell me how to fix this problem? Any suggestion?&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Christie&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Wed, 27 Jul 2022 12:03:41 GMT</pubDate>
    <dc:creator>a8Chcx</dc:creator>
    <dc:date>2022-07-27T12:03:41Z</dc:date>
    <item>
      <title>KV58 CANBUS Communication</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KV58-CANBUS-Communication/m-p/1496356#M63663</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I am using KV58&amp;nbsp; CANBUS to communicate the ESP32 CANBUS(Support ISO 11898-1).&lt;/P&gt;&lt;P&gt;1) When I try the communication between ESP32 board, it works fine.&lt;/P&gt;&lt;P&gt;2) When I try KV58 with K64F CANBUS, it works fine as well.&lt;/P&gt;&lt;P&gt;3) Then, I try KV58 CANBUS with ESP32, I cannot get it work. The difference between K64F CANBUS and ESP32 CANBUS is just MCU, all others(tranceiver, connection, and etc) are exactly same. I am wondering if it is related to timing settings?&lt;/P&gt;&lt;P&gt;Can anybody tell me how to fix this problem? Any suggestion?&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Christie&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 27 Jul 2022 12:03:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KV58-CANBUS-Communication/m-p/1496356#M63663</guid>
      <dc:creator>a8Chcx</dc:creator>
      <dc:date>2022-07-27T12:03:41Z</dc:date>
    </item>
    <item>
      <title>Re: KV58 CANBUS Communication</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KV58-CANBUS-Communication/m-p/1500522#M63735</link>
      <description>&lt;P&gt;Hi Christie,&lt;/P&gt;&lt;P&gt;Thank you so much for your interest in our products and for using our community.&lt;/P&gt;&lt;P&gt;I think you are correct. It is related to timing settings. If you are using the SDK examples of KV58 and K64, both bit rates are set to 1 Mb/s. Then it is only to check how the ESP32 is configured.&lt;/P&gt;&lt;P&gt;Hope it helps you.&amp;nbsp;Please let me know if you have more questions about it.&lt;/P&gt;&lt;P&gt;Have a nice day!&lt;/P&gt;</description>
      <pubDate>Wed, 03 Aug 2022 22:09:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KV58-CANBUS-Communication/m-p/1500522#M63735</guid>
      <dc:creator>_Leo_</dc:creator>
      <dc:date>2022-08-03T22:09:31Z</dc:date>
    </item>
  </channel>
</rss>