<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックRe: CAN communication at KV5x</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/CAN-communication-at-KV5x/m-p/1488914#M63563</link>
    <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/190527"&gt;@CauTran&lt;/a&gt;,&lt;/P&gt;&lt;P&gt;I see that you have another case with the same question, I will follow up on this last one that I mention.&lt;/P&gt;</description>
    <pubDate>Wed, 13 Jul 2022 16:09:47 GMT</pubDate>
    <dc:creator>_Leo_</dc:creator>
    <dc:date>2022-07-13T16:09:47Z</dc:date>
    <item>
      <title>CAN communication at KV5x</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/CAN-communication-at-KV5x/m-p/1487923#M63560</link>
      <description>&lt;P&gt;Hi everyone,&amp;nbsp;&lt;/P&gt;&lt;P&gt;I had a problem when I am used CAN communication.&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am using CAN1 for communication. I have three node ID. Two node is a slave, they have 0x039, 0x010 for send, respectively. And received id is 0x0D3, 0x09C respectively.&amp;nbsp; And one node is a master.&amp;nbsp;&lt;/P&gt;&lt;P&gt;There is okay when the slaves transfer data to master or master transfer data for slaves.&amp;nbsp;&lt;/P&gt;&lt;P&gt;But when slaves and master transfer data &lt;STRONG&gt;concurrently, I see problem.&amp;nbsp;&lt;/STRONG&gt;My program see the packet lost at both directions.&amp;nbsp; when I use candump in linux, I see that&amp;nbsp;problems found when receiving and transmitting meet.&lt;/P&gt;&lt;P&gt;This is my project for can testing. Please focus on rcp_can.c and rcp_can.h on utilities folder.&lt;/P&gt;</description>
      <pubDate>Tue, 12 Jul 2022 07:51:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/CAN-communication-at-KV5x/m-p/1487923#M63560</guid>
      <dc:creator>CauTran</dc:creator>
      <dc:date>2022-07-12T07:51:46Z</dc:date>
    </item>
    <item>
      <title>Re: CAN communication at KV5x</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/CAN-communication-at-KV5x/m-p/1488914#M63563</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/190527"&gt;@CauTran&lt;/a&gt;,&lt;/P&gt;&lt;P&gt;I see that you have another case with the same question, I will follow up on this last one that I mention.&lt;/P&gt;</description>
      <pubDate>Wed, 13 Jul 2022 16:09:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/CAN-communication-at-KV5x/m-p/1488914#M63563</guid>
      <dc:creator>_Leo_</dc:creator>
      <dc:date>2022-07-13T16:09:47Z</dc:date>
    </item>
  </channel>
</rss>