<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: MK22FX512AVLK12 - 5V tolerant input? in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/MK22FX512AVLK12-5V-tolerant-input/m-p/1486206#M63529</link>
    <description>&lt;P&gt;The second link is for the MKL26 not the 22.&amp;nbsp; The 26 is not 5V tolerant.&lt;BR /&gt;First link for the 22 gives the answer.&lt;BR /&gt;They could have made the data sheet clearer.&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Thu, 07 Jul 2022 11:49:59 GMT</pubDate>
    <dc:creator>bobpaddock</dc:creator>
    <dc:date>2022-07-07T11:49:59Z</dc:date>
    <item>
      <title>MK22FX512AVLK12 - 5V tolerant input?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/MK22FX512AVLK12-5V-tolerant-input/m-p/1486059#M63525</link>
      <description>&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;LI-SPOILER&gt;MK22FX512AVLK12 - 5V tolerant input?&lt;/LI-SPOILER&gt;&lt;P&gt;I'm using&amp;nbsp;MK22FX512AVLK12 operated in 3.3V.&lt;/P&gt;&lt;P&gt;I want to connect the uart port to another board that id operated with 5V - hence the uart_rx will get 5V (and not the recommended 3.3v) - are those pins tolerant to 5V?&lt;/P&gt;&lt;P&gt;Of course, about the Vih of the other board, i will need to check that he "understand" the "3.3V" from the MK22 as "1".&lt;/P&gt;&lt;P&gt;I could not find in the DS clear info about it.&lt;/P&gt;&lt;P&gt;I saw some other post about it but one says its not tolerant and another one says it is.&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/t5/Kinetis-Microcontrollers/K22-controller-pin-TXD-and-RXD-uart-pins-operated-on-5V-external/m-p/643418" target="_blank" rel="noopener"&gt;https://community.nxp.com/t5/Kinetis-Microcontrollers/K22-controller-pin-TXD-and-RXD-uart-pins-operated-on-5V-external/m-p/643418&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/t5/Kinetis-Microcontrollers/Are-the-MK2-UART-RX-pins-5V-tolerant/m-p/1402141/highlight/true#M62279" target="_blank" rel="noopener"&gt;https://community.nxp.com/t5/Kinetis-Microcontrollers/Are-the-MK2-UART-RX-pins-5V-tolerant/m-p/1402141/highlight/true#M62279&lt;/A&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;Uzi&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 07 Jul 2022 08:07:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/MK22FX512AVLK12-5V-tolerant-input/m-p/1486059#M63525</guid>
      <dc:creator>Uzi</dc:creator>
      <dc:date>2022-07-07T08:07:54Z</dc:date>
    </item>
    <item>
      <title>Re: MK22FX512AVLK12 - 5V tolerant input?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/MK22FX512AVLK12-5V-tolerant-input/m-p/1486206#M63529</link>
      <description>&lt;P&gt;The second link is for the MKL26 not the 22.&amp;nbsp; The 26 is not 5V tolerant.&lt;BR /&gt;First link for the 22 gives the answer.&lt;BR /&gt;They could have made the data sheet clearer.&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 07 Jul 2022 11:49:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/MK22FX512AVLK12-5V-tolerant-input/m-p/1486206#M63529</guid>
      <dc:creator>bobpaddock</dc:creator>
      <dc:date>2022-07-07T11:49:59Z</dc:date>
    </item>
  </channel>
</rss>